Recycle & Retrofit
  • Challenges & Projects
  • Project14
  • Recycle & Retrofit
  • More
  • Cancel
Recycle & Retrofit
Blog Retrofited Alarm Clock with New Brains and stuff
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Recycle & Retrofit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: hugohu
  • Date Created: 8 Dec 2020 1:41 PM Date Created
  • Views 3171 views
  • Likes 7 likes
  • Comments 12 comments
  • recycleretrofitch
Related
Recommended

Retrofited Alarm Clock with New Brains and stuff

hugohu
hugohu
8 Dec 2020
image

Recycle & Retrofit

Enter Your Electronics & Design Project for a chance to win a $200 shopping cart!

Submit an EntrySubmit an Entry  Back to homepage image
Project14 Home
Monthly Themes
Monthly Theme Poll

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I have this old Sony alarm clock. Took it apart a few months ago, powered solely by ICs.

 

It's not too powerful.

 

I'm adding a Pi 4 to it- to run the Google Assistant SDK, so it could be a google assistant enabled alarm clock.

 

Well, what's my progress?

 

Welp. I've been procrastinating a bit since I thought the due date was 1/14.

 

Turns out it was 12/14

 

Ouch.

 

Anyway. I have a first-gen AIY kit I got from microcenter for 3 dollars. I plopped it onto the Pi 4 4GB Tariq sent me(thank you!)

I set up the SDK, API, and stuff like that yesterday.
https://aiyprojects.withgoogle.com/voice-v1/

 

I can't find the microphone! I'll find the speaker I took from this alarm clock, reinstall it, and connect.

 

When done, I'll install it into the chassis.

 

For the screen- I'll have to reverse engineer the LCD module.... ouch....

 

Multimeter should come in handy.

 

Yay. I opened up the chassis. Looks like I'll need significantly more effort to modify the case than i expected.

 

Ouch.

 

Ouch.

 

Ouch...

 

Yipee. The API didn't work. I have to redo it. WHIPEE.

 

Hey, I did finid that mic.

 

12/9/2020

 

Ralph, you were right! Just finished the major portion for this.

 

image

 

3A+(sorry Tariq but space was limited)

 

This also has one of those AIY hats.

 

The AIY hat is basically just an audio amp, mic breakout, and servo drivers.

 

Suits me.

 

The original speaker's wires are too old and I decided to swap them for new ones. Hi-quality 22AWG, here we come!

 

Soldered on some new wire, and it's as good as new.

 

The sound quality isn't the best, but it IS over a decade old.

image

 

Trust me- it really is the original speaker.

 

Look how much it fits to the original chassis. Had to tape it on since I couldn't find my glue gun.

 

image

 

And lastly a poorly shot image

 

That plastic, is to prevent the terminal block leads from touching the HDMI port which causes a short circuit which isn't fatal but make a buzzing noise.

 

That's it.

 

(Or is it)

 

I have to add a video for proof!

 

Here's a short video, showing myself asking the current time and temperature.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Time to figure out the timing part. Ouch....

 

Now that hurts. Time to dig up some dev modules.

 

12/11

 

I did make the clock!

 

With an arduino Uno, but I realized it wouldn't fit. In my attempt to use a digispark I managed to kill the digispark and also the screen and RTC.

 

*Trying but failing not to cry*

 

*sniffs*

 

Sacrficed, I suppose.

 

Time to find something else.

 

A bit of "how to"

 

First, you have to follow the instructions in the link I posted above. However, don't connect the speaker nor put it in a case.

 

Then, see how to fit this into your case. I had to snap some plastic support structures to do so.

 

Then, I had to figure out the power issue. I basically took the power cable and then fit it through the hole that the power cable used to be.

 

Since I already enclosed the board, I use SSH to connect to it, and run the scripts.

 

I have no idea if I can add a screen- I fried the smallest dev board I had, the small ones that I have now are incompatible with libraries.

 

I still have a cool SHARP monochrome 2.7" screen, but that requires a large memory size and I don't have small boards with more powerful chips that support libraries.

 

Installed a LCD, 12/17

thanks for the extension!

  • Sign in to reply

Top Comments

  • hugohu
    hugohu over 5 years ago in reply to ralphjy +3
    Ha. Tariq sent me this pi for this project14 and i don't want to be a traitor and not submit anything. Hehe. Short deadlines? You bet. I'm also.. *considering* builidng onto this for the making time one…
  • mp2100
    mp2100 over 5 years ago +3
    Huh, I bought one of those google AIY kits at microcenter too. It was cheap because is was a few generations old. For the G company, anything from 2019 is ancient history, no support, libraries not available…
  • ralphjy
    ralphjy over 5 years ago +2
    The Making Time Competition ends 1/14. You could switch to that and give yourself more time for the project. Or maybe short deadlines help cure your procrastination .
  • hugohu
    hugohu over 5 years ago in reply to ralphjy

    Ha. Tariq sent me this pi for this project14 and i don't want to be a traitor and not submit anything.

     

    Hehe.

     

    Short deadlines? You bet.

     

    I'm also.. *considering* builidng onto this for the making time one.

     

    And also something else.

     

    And then, also something else...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago

    The Making Time Competition ends 1/14.  You could switch to that and give yourself more time for the project.  Or maybe short deadlines help cure your procrastination image.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<