Recycle & Retrofit
  • Challenges & Projects
  • Project14
  • Recycle & Retrofit
  • More
  • Cancel
Recycle & Retrofit
Blog Virucidal Oven
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Recycle & Retrofit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sunnyiut
  • Date Created: 14 Dec 2020 8:58 PM Date Created
  • Views 1513 views
  • Likes 5 likes
  • Comments 3 comments
  • recycleretrofitch
Related
Recommended

Virucidal Oven

sunnyiut
sunnyiut
14 Dec 2020

Virucidal means - having the capacity to or tending to destroy or inactivate viruses. In this project, I am using an out of order old microwave oven to make a very simple DIY ‘disinfector’ device to destroy or inactivate viruses, intended mostly for the CORONA virus. The main weapon is the UVC germicidal light which is used instead of the Magnetron of the Microwave Oven.

 

image

 

What’s the difference?? Nothing special!!!! Well – the answer is ‘simplicity’

 

There are lots of examples and designs of disinfector ovens using UVC light to destroy the virus. I am not going into the detail of the mechanism of how UVC [258 nm] light can effectively act as a disinfector in this blog.

 

Here, My goal is to make a very simplified version of the device where I can make it easier DIY so that anyone can do it with basic electrical knowledge without taking the headache of designing complex circuitry for exposure time control and safety lock etc.

 

 

So, it has to be a solution which is -

Efficient

Low cost

Easy to setup

And SAFE

 

And the automatic choice for me is a MICROWAVE OVEN!!!

I used my old microwave oven which has a burned out magnetron. It was from a local brand ‘RANGS’. They are the official dealer of SONY in Bangladesh. The build quality of the microwave oven is superb. I just placed a germicidal UVC light from PHILIPS at the terminals of the magnetron.

 

Advantage: it almost has all the basic requirements –

  • The basic timing circuits are built-in
  • There are safety locks for doors
  • The turn table helps to distribute the UVC exposure evenly
  • Stainless steel inner body to avoid any degradation
  • Glass on the front door gives the visibility but prevents UVC to pass through
  • Only a germicidal UVC tube and ready-made driver circuit is needed

 

Assembly:

Step01- I removed the magnetron and other unnecessary parts from the chassis. I removed the top cover and drilled two holes to mount the T8 tube holders.

imageimage

Step02- I placed the wires with heat shrink tubes. Because the insulation of the wires can be degraded due to UVC exposure for a long time. However, the tube holders are also made of plastic, but the intensity of the UVC light is almost nill at the edges. It is highest at the middle for the lamp tube.

imageimage

Step03- I connected a driver for the UVC lamp at the terminals of the magnetron. I had to drill some holes and placed connectors for a neat assembly of the cables. The general purpose bulb was missing!! I can’t remember where it had gone. So, I had to mount another bulb separately so that I can see the internal staffs while it’s operating.

imageimage

 

Interior:

 

 

{gallery} Interior setup

image

Internal SS body: UVC exposure degrades plastic and even paints. It was an advantage for me that the body of the oven is made of bare SS.

image

UVC lamp: Philips TUV 15W 258nm germicidal T8 tube provides the required UVC light for disinfection

image

Turntable: Turntable provides a better UVC light distribution

image

Front door: The glass of the front door gives visibility but blocks the UVC light to come out during operation. Safety lock turns off the UVC lamp automatically when the door is opened.

 

Operation:

Just like a traditional microwave oven, the exposure time can be varied accordingly. However, other options are disabled and there is no control over the power or intensity of the exposure. Once the door is locked and time is fixed, the UVC lamp turns on with pressing the start button. A fading blue light is visible from outside through the glass front door.

imageimage

 

There are two limitations of this simple design. The UVC is exposed only from the top. Several other lamps can be placed on the side walls too to overcome this limitation.

The turntable side does not get any exposure, as UVC does not reflects back from the metal body with much energy. So, the stuffs placed inside need to be flipped manually after the first session of exposure.

 

**there is an interesting observation. I have a screen cover attached on the display of my phone. It had a crack previously. After a month of UVC exposure on regular basis, I noticed several cracks on the cover and the paints on the plastic body at the back became more brittle.

 

Overall, this is a very low cost solution. Easy to build and quite effective. I am using it from July 2020. It was fun to utilize the old oven and recycle it for some other purpose. As it goes with this project14 theme, I thought better to share it with you all.

Hope you all enjoyed it.

Thanks.

  • Sign in to reply

Top Comments

  • neuromodulator
    neuromodulator over 5 years ago +1
    This is an interesting project, but UVC is quite dangerous...the damage to the plastic is not surprising, you are dealing with ionizing radiation. This UV light is even more energetic than what you get…
  • DAB
    DAB over 5 years ago +1
    You should put a UV block filter on the door so you do not blind anyone looking in. Good project though. DAB
Parents
  • neuromodulator
    neuromodulator over 5 years ago

    This is an interesting project, but UVC is quite dangerous...the damage to the plastic is not surprising, you are dealing with ionizing radiation. This UV light is even more energetic than what you get from the sun (since UVC gets filtered out by the ozone layer). UVC light can damage lots of materials (pretty much the same materials that get damaged by sunlight), so you have to be careful on what you put in that machine.

     

    I wouldn't say that working with a high power UVC light is safe... you could get skin burns, cancer or cataracts if you are not careful enough... Eventually photolysis of some materials could release toxic fumes.

     

    Why do you say that the door prevents UVC light to leak out? If you can see the light from the outside, its just getting through (probably much less but still).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • neuromodulator
    neuromodulator over 5 years ago

    This is an interesting project, but UVC is quite dangerous...the damage to the plastic is not surprising, you are dealing with ionizing radiation. This UV light is even more energetic than what you get from the sun (since UVC gets filtered out by the ozone layer). UVC light can damage lots of materials (pretty much the same materials that get damaged by sunlight), so you have to be careful on what you put in that machine.

     

    I wouldn't say that working with a high power UVC light is safe... you could get skin burns, cancer or cataracts if you are not careful enough... Eventually photolysis of some materials could release toxic fumes.

     

    Why do you say that the door prevents UVC light to leak out? If you can see the light from the outside, its just getting through (probably much less but still).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • sunnyiut
    sunnyiut over 5 years ago in reply to neuromodulator

    Hi, thanks for your comment.

    Yes, you are right, UVC is dangerous and that's why it has the germicidal capability. It's a common practice to use UVC for disinfection.

    You can find an overview from International Ultraviolet Association : https://www.iuva.org/resources/covid-19/UV%20101%20-%20Overview%20of%20Ultraviolet%20Disinfection%20-%20White%20Paper.pd…

     

    Working with UVC light is not safe. That's why I used the microwave oven chassis which has a metal [SS] body and the glass front door has safety lock mechanism. Glass does not allow UVC to pass through. Only UVA can pass and the lamp produce mostly ~258nm [UVC] wavelength output. It produces very low energy at UVA band and that also gets blocked partially by the glass. Normal glass (as used in windows) is transparent [almost 70%] to UV radiation to a wavelength of about 330 nm (UV-A). Below 330 nm (UV-B and UV-C), almost 100% is blocked by normal glass."

    link: https://www.iuva.org/UV-FAQs

     

    Therefore, i thought that the glass will be safe enough. However, the blue light that we see from outside is within the visible rage and it is not harmful i believe.