Solar Powered Yard Gadget
  • Challenges & Projects
  • Project14
  • Solar Powered Yard Gadget
  • More
  • Cancel
Solar Powered Yard Gadget
Blog Building a Solar Charger
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Solar Powered Yard Gadget to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 14 Oct 2017 9:57 PM Date Created
  • Views 6671 views
  • Likes 14 likes
  • Comments 17 comments
  • solaryardgadgetch
  • solar-cell
  • battery charging
  • battery charger
  • solar panel
  • energyharvestingch
  • bq24650
  • solar-energy
  • conservation_projects
  • texas_instruments
  • solarpwrdevicesch
  • project14
  • project 14
  • texas instruments
  • solar
Related
Recommended

Building a Solar Charger

shabaz
shabaz
14 Oct 2017
image

Electronics & Design Projects

Monthly project competitions, chances to earn prizes, you decide project themes, your ideas, your projects, turn ideas into projects.

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Introduction

There is lots of scope for outdoor electronics. A solar charger is useful for this : ) The 90-second video here describes it.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I wanted to have a general purpose outdoor solar charger that could be used for (say) powering outdoor speakers, or for evening lighting. I wanted something that could easily charge some tens of Watt-hours energy capacity batteries, so that there is lots of power available, but small enough that it doesn’t need a massive panel.

 

I have several compact solar panels and a few rechargeable batteries to test with for now, but I hope to find slightly larger panels and batteries too.

image

 

A charge current of a few amps was the ballpark I was looking for, and the ability to charge a cell or 2- or 3-cell battery, perhaps up to 12V.

 

It needed to have some flexibility, so that I could try out different panels and batteries. I didn’t want a microcontroller to be mandatory, so I wanted to be able to set the solar panel MPPT (maximum peak power tracking) value using a resistor.

 

The perfect IC for this seemed to be the BQ24650BQ24650. It can accept a reasonably wide power range for small panels (5V to 28V) and can handle different battery types and different numbers of cells.

 

Schematic

The circuit is fairly straightforward; it is based on the datasheet, with some external control to be able to switch it on/off using an optional microcontroller. The two main connectors J1 and J2 are used for the solar panel input and the battery to be charged. There is a third connector which carries the same connections plus a few more that are useful for connecting up a microcontroller or LEDs for status information.

image

 

PCB Layout

The CAD layout here shows the current state of the board; it still needs to be routed! It will be fairly compact, around 100x50mm.

image

 

Circuit Calculations

In order to determine precise component values, there is an excellent BQ24650 spreadsheet. I used it to experiment with what values will be required. These will be selected once a battery is chosen. Initially I may use a couple of D sized NiMH batteries, to build an outdoor lamp or speaker : )

image

 

Summary

There is still lots to do (PCB layout, battery selection, component value adjustment) but I’m happy that soon there could be a compact, general-purpose solar charger for small to mid-powered outdoor projects!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +2
    I seem to recall you posted what the panel was, but I'm not sure where (and you add so much content the search engine would die ) I'm interested in what you've decided on, since I have several projects…
  • jw0752
    jw0752 over 8 years ago +2
    This is a good project and I am glad you are sharing your research with us. I see that they are commercially using a lot of the small panels for powering signs and other applications. I wonder if they…
  • shabaz
    shabaz over 8 years ago in reply to jw0752 +2
    Hi John, That's an excellent idea! I will ask a local councillor what they do with all the electrical stuff they scrap. It would also be useful to take one apart, to see how they construct it.
Parents
  • ka_ru
    ka_ru over 8 years ago

    Hi,

    do you definitely want to always have a connected output divider to the battery?
    Do you have two layer PCB? Are you sure that you do not need resistance in the line BTSR?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to ka_ru

    Hi ka,

     

    Thanks for examining the circuit! I think it is ok to have the divider, it is very high impedance, the current through it is the order of 10-20uA depending on the selected battery voltage. The circuit is intended for several tens of Wh battery capacity. It could be possible to reduce the leakage with a MOSFET to switch on/off the connection to the battery though, it is a good point.

    It will be a 2-layer board, but I wasn't sure what you meant by BTSR and resistance in the line. Do you mean BTST? or something else? Could you explain what you mean about having resistance?

    By the way, there is an error in the schematic in the blog post currently, there should be a wire link from the pin 'PH' to the junction common to the two MOSFETs (i.e. where the Q2A source and Q2B drain connect together). I've corrected the error locally but have not updated the diagram yet, I'll do that soon, and will finish the PCB layout soon too. If you spot anything else that concerns you, do let me know.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ka_ru
    ka_ru over 8 years ago in reply to shabaz

    I highly recommend putting serial resistance in the line BTST(<10R) and in the gate of the MOSFETs. If this is not done, there may be a large surge on VREF.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to ka_ru

    Hi Ka,

     

    Thanks for the information. The reference board and data sheet doesn't mention this, although the reference board does have a resistor in the BTST line. I will add this and the gate resistors.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 8 years ago in reply to ka_ru

    Hi Ka,

     

    Thanks for the information. The reference board and data sheet doesn't mention this, although the reference board does have a resistor in the BTST line. I will add this and the gate resistors.