Spring Clean!
  • Challenges & Projects
  • Project14
  • Spring Clean!
  • More
  • Cancel
Spring Clean!
Spring Clean Projects 2026 Spring cleaning... gone wrong!
  • News and Projects
  • Forum
  • Members
  • More
  • Cancel
  • New
Join Spring Clean! to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: strb
  • Date Created: 24 May 2026 1:57 PM Date Created
  • Views 298 views
  • Likes 7 likes
  • Comments 9 comments
  • Spring Clean 2026
Related
Recommended

Spring cleaning... gone wrong!

strb
strb
24 May 2026

Last year I partecipated to the Spring Clean competition and I enjoyed it a lot. It gave me the push to complete what I had left over at the time, freeing up some bench and mental space. This year, when I discovered that the Spring Clean challenge was up and running again, I was ready to participate. But it didn't go according to plan.

The beginning

This year's competition started on March 18th, but I discovered it only one week later (thanks JoRatcliffe  for the tag in a comment!). I had an old radio from a family friend sitting on the shelf waiting to be repaired. To me this was the perfect occasion to work on it, while having fun and participating in the e14 community. Still, I was able to start working on it only during April.

imageThe radio, ready to be repaired. I brought with me a little helper!

The radio is a Major RS2020L, apparently from the 1980s. This thing is almost 15 years older than I am, but it looks pretty well maintained, especially the front panel, which is clean and shiny. This radio was handed to me with no more information than "It doesn't work, please check if you can fix it". After checking the fuse (which was fine), I decided to plug it in to see if there was something obviously wrong. To my surprise, the front panel lit up as supposed and nothing else happened. Looking from outside, the radio seemed fine. Time to dig deeper!

image

The radio turned on and lit up correctly. In the photo looks dimmer compared to real life.

Opening it up

After removing four screw and lifting up the wooden cover, the inner work of the radio showed to me. At first glance all components seemed fine: no burn marks, no smell, hardly any dust deposit.
I took a moment to observe some particulars I'm not used to in modern electronics. I like the variable capacitor and all the mechanisms used to tune it. They apparently also added some weight on the knob shaft supposibly to give a different feeling (I'm not going to remove that to see how the feeling changes, not at the moment, at least Slight smile ).

image

I then turned it upside down and... oh! Somebody had fun with cable management!

image

One of the boards (the amplifier board) had some strange white residue on it, but it came off easily with just a bit of IPA.

{gallery}Board cleanup

image

image

Let's start debugging

As very first step, I set up a quick measure to check the current/voltage at the transformer output. The "big cap" sits at 40V and the current waveform is exactly what one would expect from a full bridge rectifier + capacitor. From now on, I'm going to provide the supply with my bench power supply, so I don't need to worry about being plugged into mains voltage. 

image

Input current. Supply circuits seems fine. 

After fiddling a little around, I managed to set the RS2020L in "radio mode", while observing speaker outputs with my oscilloscope. Moving the tuning knob back and forth seemed like that one channel had some activity, while the other was silent. Knowing that, I decided to exclude the radio board from my initial investigation (as it seemed fine) and concentrate my effort on the rest of the circuitry.
Starting from the back aux connector, I managed to trace the signal path from that connector through the boards up to the outputs.

image

I then proceeded by injecting a small signal in the L/R aux channels, measuring it at different points to see where it disappears. Turned out that the probable cause of the fault is the last stage: the amplifier board. Signals arrives to it correctly but on one channel nothing comes out.

image

Input and output signal on the working channel.

I searched the internet for some schematics but had no luck in finding anything. I then proceeded by desoldering all active components and checking them for damage. All transistors (a mixture of npn and pnp bjts) in the "bad" channel seemed fine after testing them with a multimeter.
I wasn't particularly keen on desoldering and checking every single component on the board, so I decided to change my approach. Having a functional channel, I started measuring bias points on every transistor on the working side and then checking the same transistor on the bad side. The layout of the second channel is pretty much the mirrored copy of the first one, so I was able to complete this operation even without the board schematic.

And then...

... I got stuck again! It has been almost three weeks since last time I worked on the radio due to personal and work commitments.

But wait, there's more! While working on it, I received other requests for repair! I started with the radio but I ended up with the radio, a small UPS and an electronic speed controller to repair. These are not "my faults", but I have to take the blame for another reason: just a couple of days ago I got back from work with a bag full of old unused equipment that was going to be thrown away. How could I possibly have resisted taking them back home with me?

image

Before and after Spring Cleaning. Clearly something has gone wrong in the process!

And this is how my story ends for this year's Spring Clean competition. Time is running out and the next week is already fully scheduled, so no chance to get back on the radio before the competition ends.

Thanks a lot to the e14 staff that organizes this kind of events and thanks to the members who tried helping me here.
Happy life to you all and enjoy this last Spring Clean week!

  • Sign in to reply

Top Comments

  • colporteur
    colporteur 4 months ago +1
    I wouldn't say wrong, just not complete.
  • strb
    strb 4 months ago in reply to kmikemoo +1
    I mean, both of us have probably achieved two victories: we are now closer to the completion of our initial projects we are already set up for next year's Spring Clean competition
Parents
  • kmikemoo
    kmikemoo 4 months ago

    strb Ah... a kindred soul.  The pile on the floor by the workbench is larger and I will only have two days left in the cometition by the time I return home.  Short of a miracle... I won't get my project done - but I have advanced it - sort of. Laughing  Your project is less incomplete now than it was at the start of the competition.  Even small victories are victories. Thumbsup

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kmikemoo
    kmikemoo 4 months ago

    strb Ah... a kindred soul.  The pile on the floor by the workbench is larger and I will only have two days left in the cometition by the time I return home.  Short of a miracle... I won't get my project done - but I have advanced it - sort of. Laughing  Your project is less incomplete now than it was at the start of the competition.  Even small victories are victories. Thumbsup

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • strb
    strb 4 months ago in reply to kmikemoo

    I mean, both of us have probably achieved two victories:

    • we are now closer to the completion of our initial projects
    • we are already set up for next year's Spring Clean competition Rofl