Test Instrumentation
  • Challenges & Projects
  • Project14
  • Test Instrumentation
  • More
  • Cancel
Test Instrumentation
Blog Micro:bit VI Curve Tracer Implementation
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 21 Nov 2018 11:44 PM Date Created
  • Views 2892 views
  • Likes 6 likes
  • Comments 6 comments
  • advanced micro:bit projects
  • microbit
  • micro bit
  • advanced_microbit_projects
  • test instrumentation
  • project 14
  • diytestinstruch
Related
Recommended

Micro:bit VI Curve Tracer Implementation

ralphjy
ralphjy
21 Nov 2018
image

Test Instrumentation

Enter Your Electronics & Design Project for a chance to win a Grand Prize for Originality, a Tool Set, and a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

Since I'm late to the party, I'm just going to do a quick proof of concept implementation rather than a fully developed tool.  I'll continue to develop the tool to fit future requirements.

 

Hardware:

I decided to make the tool modular to make it more flexible.  The first module will incorporate the Micro:bit and the display shield.  The second module will include the I2C DAC and programmable current sink.  The modular approach allows me to add other functionality later.

 

The first step was to print a case to house the Micro:bit and display.

 

Case:

image

 

The second step was to provide the interface for the second module.  The second module needs the I2C pins to program the DAC and an Analog pin to read the current sink voltage plus power pins.

 

Micro:bit pinFunction
19SCL I2C clock
20SDA I2C data
0Analog In 0
3V33.3V power
GNDGround

 

Unfortunately, the LCD shield that I'm using only provides the breakout of the pins that the shield uses so I needed to solder wires directly to the shield connector pins.

image

 

For now, I've decided to implement the second module on a breadboard so I won't print a case for it yet.

 

Software:

As I was searching for the right software development environment to use, I came across a great tutorial by Adafruit on programming the Micro:bit using the Arduino IDE: https://learn.adafruit.com/use-micro-bit-with-arduino/overview.

 

Since I am very familiar with the Arduino IDE, this allowed me to get the software working quickly.  I used the SPI library and and a Waveshare library for a compatible Arduino LCD shield.  After adjusting the pins and fixing the screen orientation I was able to use the library functions without additional modification.  I used the Wire library for the I2C and since the Board Manager maps the Micro:bit default pins; I didn't need to specify them.

 

Here is the code for my example program: Microbit_VI_Monitor.ino:

 

 

 

Hardware setup:

image

 

 

Video of Curve Trace:  Linear trace of current through a fixed resistor

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Summary:

I basically just verified that I could get the hardware and software interface working for a Micro:bit Curve Tracer.  It still needs some work to get it functioning as I'd like.  I would like to add remote logging via Bluetooth in addition to just using the LCD display for output.  Remote control via Bluetooth would be nice also.  I need to add some configuration code to allow scaling for different voltage and current values.  I also need to add calibration values to allow running with different power sources (I am using the 3.3V supply as my DAC and ADC references and the supply value changes with power source - i.e. USB vs battery).  And I need to package the second module.  But all that will have to wait for another day....

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 7 years ago in reply to dougw +3
    dougw wrote: That tip on using the arduino IDE could be very useful .... yes! I have tried to use the Mbed project in various IDEs by using the online Mbed editor’s export functionality. That has kept…
  • three-phase
    three-phase over 7 years ago +3
    Good useful project. That would be great to connect up to an insulation tester output to automatically record a polarisation index curve. Monitoring the curve of a 4 wire AC impedance or 4 wire DC resistance…
  • dougw
    dougw over 7 years ago +2
    That tip on using the arduino IDE could be very useful ....
Parents
  • tariq.ahmad
    tariq.ahmad over 7 years ago

    Hi ralphjy ,

     

    You never have to worry about if its too late to work on a project.  This is great content and seeing this creativity turned to life is well worth the journey irrespective of the prize.

     

    The community was interested in more micro:bit projects so this was the Project14 program's way of contributing and we got another great one here!

     

    Hope everything is well with you and we're grateful for your latest contribution to the community. image  Would love to see if this evolves as your Solar Power Devices  project was quite impressive!

     

    Tariq

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • tariq.ahmad
    tariq.ahmad over 7 years ago

    Hi ralphjy ,

     

    You never have to worry about if its too late to work on a project.  This is great content and seeing this creativity turned to life is well worth the journey irrespective of the prize.

     

    The community was interested in more micro:bit projects so this was the Project14 program's way of contributing and we got another great one here!

     

    Hope everything is well with you and we're grateful for your latest contribution to the community. image  Would love to see if this evolves as your Solar Power Devices  project was quite impressive!

     

    Tariq