Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Beaglebone Ai Heating Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 124 replies
  • Subscribers 18 subscribers
  • Views 21897 views
  • Users 0 members are here
  • beagleboneai
  • beaglebone ai
  • BeagleBone
  • ai
  • beagleboard
Related

Beaglebone Ai Heating Issues

ipv1
ipv1 over 7 years ago

While experimenting with the device, I found that the board would shutdown without warning. The reasons is...

 

image

 

Now I tried a number of combos like us the USB tether, connect with display(yes I have the cursed microHDMI cable) and use standalone but every time, it just overheats if I do anything.

 

Idle temps are high too. Was wondering if I got a bad board or is it everyone?

  • Sign in to reply
  • Cancel

Top Replies

  • mudz
    mudz over 7 years ago +7
    After seeing all of you in so much trouble I decided - Why you should have all the fun so iI bought this kit too, to get into the same trouble pool.. After all, we all are community members. Cheers to…
  • tariq.ahmad
    tariq.ahmad over 7 years ago +6
    Hi ipv1 , I looked into this and this is a known issue: BeagleBone AI - Frequently Asked Questions (FAQ) They recommend adding a larger heat sink and cooling via fan.
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb +6
    Hi shabaz - I've made a first prototype which seems to fit quite well. Packing out the top spacing by one extra washer was enough to get it to grip the existing heatsink fins. I'll make a bracket over…
Parents
  • tariq.ahmad
    tariq.ahmad over 7 years ago

    Hi ipv1 ,

     

    I  looked into this and this is a known issue:

     

    BeagleBoneRegistered AI - Frequently Asked Questions (FAQ)

     

    They recommend adding a larger heat sink and cooling via fan.   

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to tariq.ahmad

    My investigations showed much the same. My questions are:

     

    1. How was this not caught during testing ? Some minor overheating might be missed but shutting down as described on many of the comments makes it obvious that there is a serious problem.

    2. This is happening when you are only running the OS on the ARM Cortex-A15 cores.  What happens to the temperature when you start using some mixture or all of the ARM Cortex-M4s cores,

          DSPs, EVEs and PRUs too?

    3. If it needs a bigger heat sink and fan just running the OS why doesn't it HAVE a bigger heat sink and fan (see 2.).

     

    After reading the earlier comments in this discussion and checking for other comments on the web I hopped over to Ebay and bought a couple of 25mm fans. The heat sink on the AI is 25mm and

    it looks like there are threaded holes to attach the fan with. I'm not sure how you mount a larger heat sink  other than a adhesive thermal pad or thermal epoxy. There is an adhesive thermal pad

    between the heat sink and SoC but I'm not a big fan of thermal pads and in this case I would much rather have a heat sink that uses mount points on the PCB and a wafer thin layer of quality thermal

    paste.

     

    It also looks like it could use some serious thermal management on the OS side. I'll give them the benefit of the doubt and hope that somebody is looking into this.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to gdstew

    gdstew  wrote:

     

    I've got a couple of 40mm fans but what I found was they have large motor hubs and very small blades which puts the blades too far away from

    most of the heat sink for my liking

    That's a good point.. subconsciously that must have been bothering me too, so I've been thinking of trying to make the area larger (with an aluminium plate). The height of the heatsink that comes attached to the BB-AI clears the height of the USB connector too, so quite a large plate could be glued on top. It might be inefficient though.. I'll try it anyway, and if it doesn't cool sufficiently, I'll switch to the 25mm fan.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz

    The actual location that the blades are pointing to is not very critical. The goal is to keep the air flow going so that the hot air gets evacuated and replaced by cold air. The air volume plays the bigger role here.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to gdstew

    > And again, so far this is not even close to running it under full load

     

    Apparently the GUI environment runs by default on the BeagleBone AI, and disabling this helps the temperatures to subside somewhat.

     

     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to jomoenginer

    > The trick is to find that Cape Fan.  I have not been able to locate it.

     

    The official one is a couple of months away, so I'm told.

     

    Until then, mayermakes has been designing an add-on board image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to gdstew

    > luckily it will be a very small banshee.

     

    Seems appropriate for Halloween - Projects and Videos

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to cstanton

    I was thinking of making one, when board arrives >>>

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to shabaz

    > without the active cooling, it would throttle more, especially if it detects no cooling is attached

     

    I wish I could get my head around cpufreq a bit more to get a system service package to handle this, I would've perhaps hoped that one existed in debian to manage this for us already but I'm not certain/conviced, I think laptop-utils would/used to do something like this but perhaps not for ARM based controllers?

     

    This seems to be something which other boards manage to do, but I'm not sure of the intricacies of how. If anyone knows I think it'd be pretty useful for this board to work on it at least - or point me in the right direction, dabbling with linux is fun.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to cstanton

    I'm convinced that this is a powerful processor with DSP cores similar to pc processor but smaller version (Didn't got hands on board yet). Surely it will heat up and demands similar active cooling like in pc's/laptops. You can try copper pipes and fan to transfer heat, setup will be bulky but you will be able to use Caps.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to mudz

    Yes, it is basically a tweaked BeagleBoard X15 chip mounted on a smaller board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to cstanton

    Hi Christopher,

     

    It's something new to me too, I'm not really sure how it is done in Linux with ARM.

    There's this web page that is for BBB discussing cpufreq, and it mentions how some parameters of the policy can be changed by writing to different devices in a cpufreq/ondemand path. But I've never seen a good explanation of how to create a custom policy, because it would be nice to have a couple of defined ones, and swap between them if heatsink/fans are attached or not.

    It's an important topic, because some may prefer no throttling, and just run the device slower, whereas others may prefer to have more dynamic behaviour.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago in reply to cstanton

    Hi Christopher,

     

    It's something new to me too, I'm not really sure how it is done in Linux with ARM.

    There's this web page that is for BBB discussing cpufreq, and it mentions how some parameters of the policy can be changed by writing to different devices in a cpufreq/ondemand path. But I've never seen a good explanation of how to create a custom policy, because it would be nice to have a couple of defined ones, and swap between them if heatsink/fans are attached or not.

    It's an important topic, because some may prefer no throttling, and just run the device slower, whereas others may prefer to have more dynamic behaviour.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cstanton
    cstanton over 7 years ago in reply to shabaz

    That's right, it's sparked a memory, basically a configuration of the governor needs to be setup in the configuration files, and then the governor profiles can be switched between, I think it then calls the necessary scripts depending on the parameters and automagically handles them? probably requires some time with the man pages.

     

    My fallback tends to be to rely on Arch linux documentation because it's cutting edge / up to date, though apparently there's some kernel documentation so it's probably managed there for the BeagleBone

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to shabaz

    shabaz & cstanton I am going to tackle this problem over the weekend. If I get good results, I will publish on Monday. Fingers crossed...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to cstanton

    Surely you can change its frequency and governer to low and power saver respectively, but beaware in low power mode it might shut down few peripherals. Also it surely needs active cooling source, read thermal considerations for AM57xx http://www.ti.com/lit/an/sprac53a/sprac53a.pdf 
    Better get proper cooling method to test it at full efficiency.
    Caution don't let it get too hot, there are chances of EOS damage.  >> http://www.ti.com/lit/an/sprace7/sprace7.pdf