Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Beaglebone Ai Heating Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 124 replies
  • Subscribers 18 subscribers
  • Views 21919 views
  • Users 0 members are here
  • beagleboneai
  • beaglebone ai
  • BeagleBone
  • ai
  • beagleboard
Related

Beaglebone Ai Heating Issues

ipv1
ipv1 over 7 years ago

While experimenting with the device, I found that the board would shutdown without warning. The reasons is...

 

image

 

Now I tried a number of combos like us the USB tether, connect with display(yes I have the cursed microHDMI cable) and use standalone but every time, it just overheats if I do anything.

 

Idle temps are high too. Was wondering if I got a bad board or is it everyone?

  • Sign in to reply
  • Cancel

Top Replies

  • mudz
    mudz over 7 years ago +7
    After seeing all of you in so much trouble I decided - Why you should have all the fun so iI bought this kit too, to get into the same trouble pool.. After all, we all are community members. Cheers to…
  • tariq.ahmad
    tariq.ahmad over 7 years ago +6
    Hi ipv1 , I looked into this and this is a known issue: BeagleBone AI - Frequently Asked Questions (FAQ) They recommend adding a larger heat sink and cooling via fan.
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb +6
    Hi shabaz - I've made a first prototype which seems to fit quite well. Packing out the top spacing by one extra washer was enough to get it to grip the existing heatsink fins. I'll make a bracket over…
Parents
  • tariq.ahmad
    tariq.ahmad over 7 years ago

    Hi ipv1 ,

     

    I  looked into this and this is a known issue:

     

    BeagleBoneRegistered AI - Frequently Asked Questions (FAQ)

     

    They recommend adding a larger heat sink and cooling via fan.   

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to tariq.ahmad

    My investigations showed much the same. My questions are:

     

    1. How was this not caught during testing ? Some minor overheating might be missed but shutting down as described on many of the comments makes it obvious that there is a serious problem.

    2. This is happening when you are only running the OS on the ARM Cortex-A15 cores.  What happens to the temperature when you start using some mixture or all of the ARM Cortex-M4s cores,

          DSPs, EVEs and PRUs too?

    3. If it needs a bigger heat sink and fan just running the OS why doesn't it HAVE a bigger heat sink and fan (see 2.).

     

    After reading the earlier comments in this discussion and checking for other comments on the web I hopped over to Ebay and bought a couple of 25mm fans. The heat sink on the AI is 25mm and

    it looks like there are threaded holes to attach the fan with. I'm not sure how you mount a larger heat sink  other than a adhesive thermal pad or thermal epoxy. There is an adhesive thermal pad

    between the heat sink and SoC but I'm not a big fan of thermal pads and in this case I would much rather have a heat sink that uses mount points on the PCB and a wafer thin layer of quality thermal

    paste.

     

    It also looks like it could use some serious thermal management on the OS side. I'll give them the benefit of the doubt and hope that somebody is looking into this.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to shabaz

    I believe development kits are basically to test processor functionality, to learn about new things - How it performs, its features usability, How to code them, most importantly to find mistakes/errors before using it for applications.. But the main thing is, they are made to be used for specific applications. They went good with previous boards similar to other board designer, but this is one mischievous processor. They just need to design the board properly.
    This is just board designing gone bad.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to cstanton

    I don't know how useful it is, but there's some Sitara Bootcamp, with Power Management training ppt : )

    https://training.ti.com/sitara-arm-processors-boot-camp-linux-power-management-overview-and-hands

     

    It's for AX335x, but the concepts mentioned in there are supported in the BB-AI/X15 (AM572x) chip too.

    There's some Linux power management training link here:

    Sitara Linux Training: Power Management - Texas Instruments Wiki

    But it's using TI's Linux image, I don't know if the same drivers are integrated in the normal BB-AI Linux image yet, and if not, what the plan for that is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to mudz

    The BeagleBoards are a bit more than development kits though.. there's some serious commitment to supporting them with software images and driver code, and supporting customers to create their own variants, or to integrate onto custom PCBs in their own designs, i.e. BeagleBone in appliances effectively, and these would be a large task if the Linux code/drivers/platform stuff needed to be maintained by the company creating their own design.

    It's a known processor, it was the same chip on an earlier BeagleBone design, the X15. So they have several years of experience with this chip. It doesn't make sense to assume they had no idea it would get hot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to shabaz

    Both the BB AI and the Jetson Nano were released to target folks looking to get involved in AI and ML, so I am not seeing a diff in target market here.

     

    Also, the Jetson Nano is Production ready.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to shabaz

    Oh, please. I've been working with the BB for some time now and comparing the support from the NVIDIA site to the now BB Google forums, the NVIDIA support and community far outshines anything the BeagleBoard folks are doing.  If you can get a response from the BeagleBoard you are lucky.

     

    And the fact the BB AI is using the same SoC as the X15 goes back to one of my original issues; its 6+ year old technology.  It was not designed for any of the newer AI and ML aps or workloads of today.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    I've had great experiences with the BB team-members for years. They're human, everyone has their off days.

    jomoenginer  wrote:

     

    It was not designed for any of the newer AI and ML aps or workloads of today.

     

    Ok, so what? There's new orgs being formed all the time, dealing with compute and AI at the edge. That's a growing deployment scenario, and even Cortex-M is being deployed for that role. The raw performance isn't the only criteria.. device longevity, industrial temp spec, hard real-time engines, are all things that the TI chips are good at.

    It sounds like you expected BB-AI to be something different from what it is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    It's good that the Nano is guaranteed for sale until 2025.. I hadn't realized that.

    https://developer.nvidia.com/embedded/community/lifecycle

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to jomoenginer

    the fan listed in the bom here: BB AI cooling Addon board available
    is the one that fits on the heatsink that is mounted on the BBAI as default.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to shabaz

    Nope. I just expect the board to perform as advertised.  The "AI" in the name seems to imply it is designed for AI, meaning Artificial Intelligence.  Or, are you saying it stands for something else?  Chip longevity is only valid for currently produced products and for a specific support lifestyle, or in cases where a mature device is mandatory by spec;  not typically for new products in this particular space. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    jomoenginer  wrote:

     

    ...I just expect the board to perform as advertised.  The "AI" in the name seems to imply it is designed for AI, meaning Artificial Intelligence.  Or, are you saying it stands for something else?

    I think the board will work for AI applications..

    It's predecessor was the BB-X15, powered by some high-powered rocket : )

     

    Back at school, we were taught there used to be some cheerios commercial about feeling groovy, and one person sued the manufacturer because they didn't make him feel groovy in the mornings. The product is different but the concept feels the same : )

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    jomoenginer  wrote:

     

    ...I just expect the board to perform as advertised.  The "AI" in the name seems to imply it is designed for AI, meaning Artificial Intelligence.  Or, are you saying it stands for something else?

    I think the board will work for AI applications..

    It's predecessor was the BB-X15, powered by some high-powered rocket : )

     

    Back at school, we were taught there used to be some cheerios commercial about feeling groovy, and one person sued the manufacturer because they didn't make him feel groovy in the mornings. The product is different but the concept feels the same : )