Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Beaglebone Ai Heating Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 124 replies
  • Subscribers 18 subscribers
  • Views 21897 views
  • Users 0 members are here
  • beagleboneai
  • beaglebone ai
  • BeagleBone
  • ai
  • beagleboard
Related

Beaglebone Ai Heating Issues

ipv1
ipv1 over 7 years ago

While experimenting with the device, I found that the board would shutdown without warning. The reasons is...

 

image

 

Now I tried a number of combos like us the USB tether, connect with display(yes I have the cursed microHDMI cable) and use standalone but every time, it just overheats if I do anything.

 

Idle temps are high too. Was wondering if I got a bad board or is it everyone?

  • Sign in to reply
  • Cancel

Top Replies

  • mudz
    mudz over 7 years ago +7
    After seeing all of you in so much trouble I decided - Why you should have all the fun so iI bought this kit too, to get into the same trouble pool.. After all, we all are community members. Cheers to…
  • tariq.ahmad
    tariq.ahmad over 7 years ago +6
    Hi ipv1 , I looked into this and this is a known issue: BeagleBone AI - Frequently Asked Questions (FAQ) They recommend adding a larger heat sink and cooling via fan.
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb +6
    Hi shabaz - I've made a first prototype which seems to fit quite well. Packing out the top spacing by one extra washer was enough to get it to grip the existing heatsink fins. I'll make a bracket over…
Parents
  • tariq.ahmad
    tariq.ahmad over 7 years ago

    Hi ipv1 ,

     

    I  looked into this and this is a known issue:

     

    BeagleBoneRegistered AI - Frequently Asked Questions (FAQ)

     

    They recommend adding a larger heat sink and cooling via fan.   

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to tariq.ahmad

    My investigations showed much the same. My questions are:

     

    1. How was this not caught during testing ? Some minor overheating might be missed but shutting down as described on many of the comments makes it obvious that there is a serious problem.

    2. This is happening when you are only running the OS on the ARM Cortex-A15 cores.  What happens to the temperature when you start using some mixture or all of the ARM Cortex-M4s cores,

          DSPs, EVEs and PRUs too?

    3. If it needs a bigger heat sink and fan just running the OS why doesn't it HAVE a bigger heat sink and fan (see 2.).

     

    After reading the earlier comments in this discussion and checking for other comments on the web I hopped over to Ebay and bought a couple of 25mm fans. The heat sink on the AI is 25mm and

    it looks like there are threaded holes to attach the fan with. I'm not sure how you mount a larger heat sink  other than a adhesive thermal pad or thermal epoxy. There is an adhesive thermal pad

    between the heat sink and SoC but I'm not a big fan of thermal pads and in this case I would much rather have a heat sink that uses mount points on the PCB and a wafer thin layer of quality thermal

    paste.

     

    It also looks like it could use some serious thermal management on the OS side. I'll give them the benefit of the doubt and hope that somebody is looking into this.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to jomoenginer

    f you can't wait to get a fan-addon for the Beaglebone AI : here is the link to order the pcb right away https://aisler.net/p/HUQFWYRM

    it takes the recommended Fan and allows to control it with pwm from a Pin on the Beaglebone (compatible with AI, Balck, Green, Blue and Indutrial Beaglebones)
    Here is the BOM:

    1x https://at.farnell.com/multicomp/mcmf0w8ff1002a20/metal-film-resistor-10kohm-125mw/dp/1127017?st=resistor%2010k

    1x https://at.farnell.com/infineon/irlz44npbf/mosfet-n-kanal-55v-41a-to-220/dp/8651418?st=IRLZ44N

    1xhttps://at.farnell.com/nidec-copal/f251r-05llc/axiall-fter-25mm-5v-dc-1-412cfm/dp/2856031?st=fan%205V%2025mm

    + some generic 2,54mm pitch headers you may already have at home.

     

    this was planned to be released alongside some content, but I see the need for people to use it so please try out this prototype at your own risk.

    the first 0 batch has not yet arrived in my workshop so I can't promise it works perfectly right now

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to shabaz

    shabaz & cstanton I am going to tackle this problem over the weekend. If I get good results, I will publish on Monday. Fingers crossed...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to cstanton

    Surely you can change its frequency and governer to low and power saver respectively, but beaware in low power mode it might shut down few peripherals. Also it surely needs active cooling source, read thermal considerations for AM57xx http://www.ti.com/lit/an/sprac53a/sprac53a.pdf 
    Better get proper cooling method to test it at full efficiency.
    Caution don't let it get too hot, there are chances of EOS damage.  >> http://www.ti.com/lit/an/sprace7/sprace7.pdf
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    For any upcoming show maybe it could be better to use something more mature.. most of the Pi releases had software teething issues at launch, the software took a while to be in a mature state.

    NVIDIA and BB-AI's chips are playing in different markets I think.. the chip in the BB-AI (AM572x) is designed for automotive applications, so will likely have the guaranteed X amount of years availability, and comes in an industrial temp version too, and might use more traditional methods of processing (multiple CPU cores and some general purpose accelerators in H/W, and some accelerators for image recognition features). NVIDIA's chip may not be available in many years time for use in customer designs (this is a guess though) if they keep churning out newer chips and want to sell those instead. NVIDIA has fantastic technology for doing state-of-the-art computing though.

     

    The BeagleBone Black's AM3358 had the longevity advantage too, because that chip was (is) in production or at least offered for sale, for 10 years (might be 15, I can't recall).

     

    The AM3358 was easy-ish to prototype with, to create custom designs (I tried to create my own too, using the OSD3358 which integrates that chip, PMIC, Flash and RAM), but the project went away - lots of time was wasted with Intel's Edison, we had a working prototype, and it went end-of-sale : (

    Prototyping a custom board will be much harder with the BB-AI's chip, but there should be modules with that same chip I hope.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to shabaz

    I believe development kits are basically to test processor functionality, to learn about new things - How it performs, its features usability, How to code them, most importantly to find mistakes/errors before using it for applications.. But the main thing is, they are made to be used for specific applications. They went good with previous boards similar to other board designer, but this is one mischievous processor. They just need to design the board properly.
    This is just board designing gone bad.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to cstanton

    I don't know how useful it is, but there's some Sitara Bootcamp, with Power Management training ppt : )

    https://training.ti.com/sitara-arm-processors-boot-camp-linux-power-management-overview-and-hands

     

    It's for AX335x, but the concepts mentioned in there are supported in the BB-AI/X15 (AM572x) chip too.

    There's some Linux power management training link here:

    Sitara Linux Training: Power Management - Texas Instruments Wiki

    But it's using TI's Linux image, I don't know if the same drivers are integrated in the normal BB-AI Linux image yet, and if not, what the plan for that is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to mudz

    The BeagleBoards are a bit more than development kits though.. there's some serious commitment to supporting them with software images and driver code, and supporting customers to create their own variants, or to integrate onto custom PCBs in their own designs, i.e. BeagleBone in appliances effectively, and these would be a large task if the Linux code/drivers/platform stuff needed to be maintained by the company creating their own design.

    It's a known processor, it was the same chip on an earlier BeagleBone design, the X15. So they have several years of experience with this chip. It doesn't make sense to assume they had no idea it would get hot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to shabaz

    Both the BB AI and the Jetson Nano were released to target folks looking to get involved in AI and ML, so I am not seeing a diff in target market here.

     

    Also, the Jetson Nano is Production ready.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to shabaz

    Oh, please. I've been working with the BB for some time now and comparing the support from the NVIDIA site to the now BB Google forums, the NVIDIA support and community far outshines anything the BeagleBoard folks are doing.  If you can get a response from the BeagleBoard you are lucky.

     

    And the fact the BB AI is using the same SoC as the X15 goes back to one of my original issues; its 6+ year old technology.  It was not designed for any of the newer AI and ML aps or workloads of today.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    I've had great experiences with the BB team-members for years. They're human, everyone has their off days.

    jomoenginer  wrote:

     

    It was not designed for any of the newer AI and ML aps or workloads of today.

     

    Ok, so what? There's new orgs being formed all the time, dealing with compute and AI at the edge. That's a growing deployment scenario, and even Cortex-M is being deployed for that role. The raw performance isn't the only criteria.. device longevity, industrial temp spec, hard real-time engines, are all things that the TI chips are good at.

    It sounds like you expected BB-AI to be something different from what it is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    I've had great experiences with the BB team-members for years. They're human, everyone has their off days.

    jomoenginer  wrote:

     

    It was not designed for any of the newer AI and ML aps or workloads of today.

     

    Ok, so what? There's new orgs being formed all the time, dealing with compute and AI at the edge. That's a growing deployment scenario, and even Cortex-M is being deployed for that role. The raw performance isn't the only criteria.. device longevity, industrial temp spec, hard real-time engines, are all things that the TI chips are good at.

    It sounds like you expected BB-AI to be something different from what it is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jomoenginer
    jomoenginer over 7 years ago in reply to shabaz

    Nope. I just expect the board to perform as advertised.  The "AI" in the name seems to imply it is designed for AI, meaning Artificial Intelligence.  Or, are you saying it stands for something else?  Chip longevity is only valid for currently produced products and for a specific support lifestyle, or in cases where a mature device is mandatory by spec;  not typically for new products in this particular space. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    jomoenginer  wrote:

     

    ...I just expect the board to perform as advertised.  The "AI" in the name seems to imply it is designed for AI, meaning Artificial Intelligence.  Or, are you saying it stands for something else?

    I think the board will work for AI applications..

    It's predecessor was the BB-X15, powered by some high-powered rocket : )

     

    Back at school, we were taught there used to be some cheerios commercial about feeling groovy, and one person sued the manufacturer because they didn't make him feel groovy in the mornings. The product is different but the concept feels the same : )

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to jomoenginer

    jomoenginer , I understand the frustration, especially when we want hardware to work and just work, and work as advertised.

     

    I think that with the BeagleBone range of hardware it's pushing for something different than with the repeatedly compared nVidia board and that it is open source. Unfortunately regardless of people's opinion and view of open source, that introduces the challenge of it being supported and it relies on the generosity of people with their time and effort to support it well.

     

    This isn't too different from some other boards that are released that rely on the generosity of the Community to support them, and if someone doesn't want to support it, dare I say it, they're free to walk away, and I agree there's some element of expectancy to pay for a product and have it working to a level - and I would suggest that there are products out there which meet that criteria.

     

    BeagleBone gives you the opportunity to get into the hardware on a level that proprietary hardware doesn't, and I would personally suggest that's partly what you're paying for, and it means you have to work a bit more at it, though you can then turn around and say "I did this, this is my cred" and share it, and be appreciated for it. To me that's part of the community and part of open source, you may not agree however it is what I've seen as the ethos behind most open source hardware and software products and it's a challenge to the ecosystem regardless.

     

    This's why we're looking at trying to solve the problem rather than focus on the flaw of the problem and pin someone to it for being responsible, we know what the problem is, we can find a solution and then hopefully the next problem is more a case of "do I put an if statement here?". If we hit a hard wall then we can go back and say it needs changing.

     

    Does that make sense? Help if you can, you don't have to, and we hear you on the issues.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to cstanton

    Sounds like a plan.  Thanks!