Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Beaglebone Ai Heating Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 124 replies
  • Subscribers 18 subscribers
  • Views 21835 views
  • Users 0 members are here
  • beagleboneai
  • beaglebone ai
  • BeagleBone
  • ai
  • beagleboard
Related

Beaglebone Ai Heating Issues

ipv1
ipv1 over 7 years ago

While experimenting with the device, I found that the board would shutdown without warning. The reasons is...

 

image

 

Now I tried a number of combos like us the USB tether, connect with display(yes I have the cursed microHDMI cable) and use standalone but every time, it just overheats if I do anything.

 

Idle temps are high too. Was wondering if I got a bad board or is it everyone?

  • Sign in to reply
  • Cancel

Top Replies

  • mudz
    mudz over 7 years ago +7
    After seeing all of you in so much trouble I decided - Why you should have all the fun so iI bought this kit too, to get into the same trouble pool.. After all, we all are community members. Cheers to…
  • tariq.ahmad
    tariq.ahmad over 7 years ago +6
    Hi ipv1 , I looked into this and this is a known issue: BeagleBone AI - Frequently Asked Questions (FAQ) They recommend adding a larger heat sink and cooling via fan.
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb +6
    Hi shabaz - I've made a first prototype which seems to fit quite well. Packing out the top spacing by one extra washer was enough to get it to grip the existing heatsink fins. I'll make a bracket over…
Parents
  • ipv1
    ipv1 over 7 years ago

    At this moment, my BB Ai no longer works. I removed the pull-up resistor which Jan Cumps mentioned as a solder bridge, but the board booted the same way to heat up the same way as before. Then I ran a sudo apt dis-upgrade and after rebooting, the board never booted up again.

    I added the pull-up again but no go.

     

    I also tried booting from an image but no go.

     

    So

    a. Don't remove the solder-bridge

    b. Don't run updates.

     

    I will try and use the serial interface to see if uboot is doing something or if the board itself is dead. I am hoping for the former but it may be the latter due to overheating.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to ipv1

    Kind of an expensive board to be putting a soldering iron to it which I would suspect violates the warranty.

     

    Does your board have a heat sink and or fan on the main processor?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to 14rhb

    Hi Rod,

     

    That should do it : ) Very cool look! Also, it looks like the end may be about 20mm square, so in theory you could even mount a fan sideways, to leave the slots visible and not covered by a fan.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to shabaz

    Thank you. That is a very good idea - blowing the air through (towards the ethernet) will have a clearer flow than downwards. The end measures 15mm so it is still possible. I could also add two more fins on the outside of the stack.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb

    Currently I measure 84g all up. The BB-AI weight is specified as 48g: https://github.com/beagleboard/beaglebone-ai/wiki/System-Reference-Manual

     

    My heatsink alone has added 36g and I still need the fan and brackets.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to 14rhb

    This seems at bit overkill and impractical.  So, you are expecting to get good heat transfer from the heat sink to the fins you added? 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to jomoenginer

    Hi jomoenginer , it was low-cost as I had the metal in my scrap bin. I'm currently not looking on expanding with capes nor sending this into the sky so the weight and bulk isn't an issue to me currently. With thermal paste in each groove I expect a better heat transfer than the existing surfaces to air (which is one of the worst conductors of heat energy). Once heat is pulled into my new fins they have a much larger surface area and, as shabaz suggested, the fan can go on the end.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to 14rhb

    f you can't wait to get a fan-addon for the Beaglebone AI : here is the link to order the pcb right away https://www.element14.com/community/message/282753/l/bb-ai-cooling-addon-board-available#282753

     

    this was planned to be released alongside some content, but I see the need for people to use it so please try out this prototype at your own risk.

    the first 0 batch has not yet arrived in my workshop so I can't promise it works perfectly right now

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to 14rhb

    I too would prefer to put the fan sideways on my BB-AI too, but really wanted to go with a larger fan (to reduce noise) so am stuck with mounting mine on top : ( So it's likely it will reach the same height as yours, once I've added the flat alu plate and heatsinks on top too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to mayermakes

    Is that a voltage regulator standing up?  Are there plans to lay it down so a Cape does not sort out on it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    That's maybe just a render fault (i.e. it could lie down since there seems to be space).. It's a MOSFET, for PWM control, so should run cool too.

    That MOSFET is overkill, but it's getting harder finding smaller-package through-hole MOSFETs these days (most are surface mount).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to jomoenginer

    it is a MOSFET used for the Pwm control. I have no 3d model of that package lying down so it renders the default position, there are thermal vias o nthe board, the mosfet should be mounted lying down so it won't stick up above the headers.
    As @shabaz pointed out  it is hard to find suitable tht mosfets and this particular one is used for fan and heater control on a ton of 3d printer boards and in my own projects.
    feel free to replace it with a different one that is pin compatible. the PCB is not in house yet so I haven't evaluated the design in practive, there may be some changes in later revisions.
    I also may do a smd version once evaluated  get it made with a pcba service if the demand is there for it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mayermakes
    mayermakes over 7 years ago in reply to jomoenginer

    it is a MOSFET used for the Pwm control. I have no 3d model of that package lying down so it renders the default position, there are thermal vias o nthe board, the mosfet should be mounted lying down so it won't stick up above the headers.
    As @shabaz pointed out  it is hard to find suitable tht mosfets and this particular one is used for fan and heater control on a ton of 3d printer boards and in my own projects.
    feel free to replace it with a different one that is pin compatible. the PCB is not in house yet so I haven't evaluated the design in practive, there may be some changes in later revisions.
    I also may do a smd version once evaluated  get it made with a pcba service if the demand is there for it.