Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Beaglebone Ai Heating Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 124 replies
  • Subscribers 18 subscribers
  • Views 21835 views
  • Users 0 members are here
  • beagleboneai
  • beaglebone ai
  • BeagleBone
  • ai
  • beagleboard
Related

Beaglebone Ai Heating Issues

ipv1
ipv1 over 7 years ago

While experimenting with the device, I found that the board would shutdown without warning. The reasons is...

 

image

 

Now I tried a number of combos like us the USB tether, connect with display(yes I have the cursed microHDMI cable) and use standalone but every time, it just overheats if I do anything.

 

Idle temps are high too. Was wondering if I got a bad board or is it everyone?

  • Sign in to reply
  • Cancel

Top Replies

  • mudz
    mudz over 7 years ago +7
    After seeing all of you in so much trouble I decided - Why you should have all the fun so iI bought this kit too, to get into the same trouble pool.. After all, we all are community members. Cheers to…
  • tariq.ahmad
    tariq.ahmad over 7 years ago +6
    Hi ipv1 , I looked into this and this is a known issue: BeagleBone AI - Frequently Asked Questions (FAQ) They recommend adding a larger heat sink and cooling via fan.
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb +6
    Hi shabaz - I've made a first prototype which seems to fit quite well. Packing out the top spacing by one extra washer was enough to get it to grip the existing heatsink fins. I'll make a bracket over…
Parents
  • ipv1
    ipv1 over 7 years ago

    At this moment, my BB Ai no longer works. I removed the pull-up resistor which Jan Cumps mentioned as a solder bridge, but the board booted the same way to heat up the same way as before. Then I ran a sudo apt dis-upgrade and after rebooting, the board never booted up again.

    I added the pull-up again but no go.

     

    I also tried booting from an image but no go.

     

    So

    a. Don't remove the solder-bridge

    b. Don't run updates.

     

    I will try and use the serial interface to see if uboot is doing something or if the board itself is dead. I am hoping for the former but it may be the latter due to overheating.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to ipv1

    Kind of an expensive board to be putting a soldering iron to it which I would suspect violates the warranty.

     

    Does your board have a heat sink and or fan on the main processor?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to 14rhb

    I too would prefer to put the fan sideways on my BB-AI too, but really wanted to go with a larger fan (to reduce noise) so am stuck with mounting mine on top : ( So it's likely it will reach the same height as yours, once I've added the flat alu plate and heatsinks on top too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 7 years ago in reply to mayermakes

    Is that a voltage regulator standing up?  Are there plans to lay it down so a Cape does not sort out on it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to jomoenginer

    That's maybe just a render fault (i.e. it could lie down since there seems to be space).. It's a MOSFET, for PWM control, so should run cool too.

    That MOSFET is overkill, but it's getting harder finding smaller-package through-hole MOSFETs these days (most are surface mount).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to jomoenginer

    it is a MOSFET used for the Pwm control. I have no 3d model of that package lying down so it renders the default position, there are thermal vias o nthe board, the mosfet should be mounted lying down so it won't stick up above the headers.
    As @shabaz pointed out  it is hard to find suitable tht mosfets and this particular one is used for fan and heater control on a ton of 3d printer boards and in my own projects.
    feel free to replace it with a different one that is pin compatible. the PCB is not in house yet so I haven't evaluated the design in practive, there may be some changes in later revisions.
    I also may do a smd version once evaluated  get it made with a pcba service if the demand is there for it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb

    Parcel arrived with my USB-C cable so onwards:

    Some thermal paste and a 12v fan and I'm finally powered up image

    Temperature measured using gdstew help in Reading BeagleBone AI Temperatures and comes in after 10 minutes at a stable 32 degrees centigradeimage

    {gallery} Powerup
    image
    image
    image
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to 14rhb

    Fantastic work with reducing the heat 14rhb.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to clem57

    Thank you clem57 .This way also doesn't void the warranty, although I very kindly got sent mine from Element14 to test out and so that puts me slightly out of any 'claim' loop if it failed.

     

    The current stumbling point would be if I knock anything and don't notice the fan isn't directed at the heatsink. And I also am using 12v so need another PSU. I'll mount them on a baseboard to mitigate against the first risk. The second and any size issues aren't really a concern for me as I only want to experiment into AI - understand how I can make algorithms to identify those pesky Box Moths while rejecting other insects.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to 14rhb

    Hi Rod,

     

    This is awesome!! I'm looking forward to powering it up this weekend too - I'm off to the shed to mount my fan/heatsink too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to shabaz

    Thank you Shabaz,

     

    It has been powered for a few hours now, I upgraded the Debian OS and I am now installing OpenCV. The temperature is still reported as 34-35 degrees C...the slight increase probably due to the ambient air temp rising slightly through the day.

     

    I haven't added an SD Card either at this point. That decision might cause issues as I get into processing data.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    The fan voltage regulator nees a heatsink to lower the temperature image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    The fan voltage regulator nees a heatsink to lower the temperature image