Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Beaglebone Ai Heating Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 124 replies
  • Subscribers 18 subscribers
  • Views 21524 views
  • Users 0 members are here
  • beagleboneai
  • beaglebone ai
  • BeagleBone
  • ai
  • beagleboard
Related

Beaglebone Ai Heating Issues

ipv1
ipv1 over 7 years ago

While experimenting with the device, I found that the board would shutdown without warning. The reasons is...

 

image

 

Now I tried a number of combos like us the USB tether, connect with display(yes I have the cursed microHDMI cable) and use standalone but every time, it just overheats if I do anything.

 

Idle temps are high too. Was wondering if I got a bad board or is it everyone?

  • Sign in to reply
  • Cancel

Top Replies

  • mudz
    mudz over 7 years ago +7
    After seeing all of you in so much trouble I decided - Why you should have all the fun so iI bought this kit too, to get into the same trouble pool.. After all, we all are community members. Cheers to…
  • tariq.ahmad
    tariq.ahmad over 7 years ago +6
    Hi ipv1 , I looked into this and this is a known issue: BeagleBone AI - Frequently Asked Questions (FAQ) They recommend adding a larger heat sink and cooling via fan.
  • 14rhb
    14rhb over 7 years ago in reply to 14rhb +6
    Hi shabaz - I've made a first prototype which seems to fit quite well. Packing out the top spacing by one extra washer was enough to get it to grip the existing heatsink fins. I'll make a bracket over…
  • shabaz
    shabaz over 7 years ago in reply to mudz

    Hi!

    No idea yet, but I will try to power up later today, and follow the information people have been posting about how to monitor the CPU temperature.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to shabaz

    I hope this low wattage fan won't affect power adaptor supply. Hoping for the best.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    As far as I know, CPU cooling fans are working 5 volts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    Thank you I will keep the same scheme.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to shabaz

    Just noticed there is also a plate behind fan with hole, there might be a problem for air flow. I'm afraid fan might not work at its full efficiency.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to mudz

    These fans are super low power, but don't bet too much on small fans over the desktop board CPU. In that case, they have not serious problems of powering. I am using one of the two macbook pro old model fan that are very low consuming.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to balearicdynamics

    I'm using a 40mm fan out of my junk box which runs at 12v....not sure where I salvaged it from. Fairly sure it wasn't a PC though as it is too small for the usual case-cooling fans.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to mudz

    Hi!

    It's not a very powerful fan, it will just move air at a low rate. A more powerful fan could also be a good idea, but then there could be the need to consider power consumption more (and also noise).

    I think you're right, the small holes may not be very good.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to shabaz

    The BeagleBone form factor limits the size of the fan mounted on top to 40mm. The GPIO headers are slightly more than 40mm apart. I understand why they wanted to keep that form

    factor but in this case I think it was a mistake. I have my AI up and running with the 25mm fan I bought mounted on the heat sink. It is a lot quieter than I thought it would be but I don't

    think it is running the advertised 10K RPM. I'm reading a temperature of about 48 deg. C when it is idle and 52 deg. C under light load. In case anybody missed this I posted this earlier:

     

     

    The next thing I did was go look for where the SoC temperatures could be read and I think I found them several

    sub-directories deep in the /sys directory. I do wish that there was a standard directory to put these in as

    everybody puts them in very different places in the /sys directory. There are 5 different thermal zones and

    each one has a directory in the /sys/devices/virtual/thermal/ directory named thermal_zone0 -  thermal_zone4.

    To display the temperature for thermal zone 0 use this command:

     

    debian@beaglebone:~$ cat /sys/devices/virtual/thermal/thermal_zone0/temp

    47000

    debian@beaglebone:~$

     

    The response, 47000 (your mileages WILL vary) is 47.0 deg. C.

     

    At the time the AI was mostly idle with me on a terminal inside an LXDE window. The temperatures I was

    reading were within a couple of degrees C across all the zones. There are many thermal management

    configuration files in the thermal_zoneX directories and it would be great to get documentation on what/where

    the thermal zones are as well as the thermal management settings used for them.

     

     

    I wrote a bash script that reads and prints out a "properly" formatted temperature from one selected zone or all zones. From what I saw during testing it looks like zone 2

    is the dual core ARM Cortex-A15. It is always the highest temperature by a couple of degrees C. I can't figure out how to make the script available on element14 other

    than just paste it in a response so some help there on the best way to do that would be appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to gdstew

    Hi Gary,

     

    I'm using the command you mentioned in your blog post too, and I get similar-ish temperatures (maybe 43-45 degrees C idle, in 22.5 deg C ambient) with fan and heatsinks. I briefly tried running stress --cpu 4 --timeout 60  for want of anything to test the system slightly, but immediately after this stress test, the temperature of the five zones had not risen much (just a few degrees) so it is probably not a good test, e.g. I could be using the wrong flags (also, it won't test anything other than the main cores, and none of the accelerators).

     

    Regarding the script, I think you'll be able to attach it if you've authored the discussion, or definitely if you've authored the blog post. So, (as an example) it should be possible for you to edit your discussion https://www.element14.com/community/message/283031/l/reading-beaglebone-ai-temperatures#283031

    since you authored it, and then add it as an attachment. It could also be placed inline, with syntax highlighting (some info on how to do that is here: Using Editor Tools for Blog Posts  )

    Another option is github, that entails setting up an account and downloading a tool or to your PC (although there may be a way to directly do it online) and can be done from the CLI too.

     

    For example I'm going to put my notes in a blog post so that I can refer to it later, otherwise stuff will get lost in all these discussion comments, and then if I had a script I could attach it to that blog post.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>