Vision Thing
  • Challenges & Projects
  • Project14
  • Vision Thing
  • More
  • Cancel
Vision Thing
Forum Problems getting started or is it dead?? <SOLVED>
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Vision Thing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 12 subscribers
  • Views 2695 views
  • Users 0 members are here
  • beaglebone ai
  • boot problems
Related

Problems getting started or is it dead?? <SOLVED>

phoenixcomm
phoenixcomm over 7 years ago
You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I got my BB AI about a week ago I had problems getting the fan mounted. But when I plug it in via USBA &gt; USBC type 3 cable but all I get is this. Is my BB dead?

Thanks

Cris H.

 

problem was thas the motherboard didn't do it. I bought a wall rat from 5-blow and now it boots!

NOW how to change the static addresses image

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 7 years ago in reply to Sean_Miller +3
    Sean_Miller wrote: The lights by the Ethernet port should start blinking. First things I'd check: Amp rating of your power supply (2.5 or greater) Unplug the fan and see if it boots Try it with an SD card…
  • Sean_Miller
    Sean_Miller over 7 years ago +2
    The lights by the ethernet port should start blinking. First things I'd check: Amp rating of your power supply (2.5 or greater) Unplug the fan and see if it boots Try it with an SD card image and without…
  • shabaz
    shabaz over 7 years ago +2
    Hi Chris, I agree with the comments above too, there's quite a fair chance it could be the PSU. I too saw the same symptom (brief start-up, many LEDs flickering, and then nothing) when I used a new Samsung…
  • Sean_Miller
    Sean_Miller over 7 years ago

    The lights by the ethernet port should start blinking.

     

    First things I'd check:

    • Amp rating of your power supply (2.5 or greater)
    • Unplug the fan and see if it boots
    • Try it with an SD card image and without the SD installed.
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago

    phoenixcomm , a few questions:

     

    Where is the fan connected to?

    What type of USB port are you plugging the BeagleBone AI into? Is it a dedicated power supply, or a personal computer?

    If it's a personal computer, what standard of USB is it? (2 or 3?)
    Are you booting from the onboard eMMC or an SDCard?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to Sean_Miller

    Sean_Miller  wrote:

     

    The lights by the Ethernet port should start blinking.

     

    First things I'd check:

    • Amp rating of your power supply (2.5 or greater)
    • Unplug the fan and see if it boots
    • Try it with an SD card image and without the SD installed.

    I went to the Beagle bone  site and downloaded a fresh image. Then I booted with no problems. Then go into the browser (Chrome) and entered 192.168.7.2 to get Cloud 9. It takes several minutes to get to that point. BTW, you should get at least 2.5 AMP supply. The official Raspberry Pi 4 adaptor from MicroCenter works great!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 7 years ago in reply to cstanton

    cstanton Its plugged into the USBA type 3 on my motherboard.  and I am using a type 3 USBA to USBC

    I am booting from the onboard eMMC.

    And I do not have the fan powered up.

    I assume there is an image on the eMMC memory.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 7 years ago in reply to Sean_Miller

    Sean_Miller yes after I plugged in an ethernet connection RJ45 blinked also but then all the LEDs go out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 7 years ago in reply to cstanton

    cstanton I have no SD card so I am booting from the onboard image.

    and I have the USBA  to USBC type 3 cable plugged into the blue USB connectors on the back of the cpu.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to phoenixcomm

    I did find https://www.amazon.com/slp/usb-3-type-c/ah83of3yv6vw6z8  #4 is type c both ends. phoenixcomm  I may be able to get one near Thanksgiving from China. Takes a long time to ship on a boat, ha ha..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to clem57

    Just let me know if you can wait for it... I will check out the price if you wish...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mp2100
    mp2100 over 7 years ago in reply to phoenixcomm

    Do you know what version of USB 3 your motherboard supports?  The original USB 3.0 only provides 900 mA, so it's only 4.5 watts, probably not enough to run the BB AI.

    https://en.wikipedia.org/wiki/USB_3.0#Power_and_charging

    From your short video, the LEDs briefly light up like a normal beaglebone, then stop. It could be it starts booting but then needs more amps and doesn't get them.

     

    Some USB 3 ports can deliver a lot more power, but only if it meets the "power delivery spec".

    https://en.wikipedia.org/wiki/USB_3.0#Power_and_charging

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Hi Chris,

     

    I agree with the comments above too, there's quite a fair chance it could be the PSU. I too saw the same symptom (brief start-up, many LEDs flickering, and then nothing) when I used a new Samsung charger. Swapped over to an official Pi PSU from Farnell/Newark (I used a Pi 3 5.1V 2.5A supply, but the Pi 4 5.1V 3A supply would be the better choice) and then it worked.