• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Getting Started
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
  • Author Author: e14 Contributor
  • Date Created: 17 Sep 2015 3:48 PM Date Created
  • Views 1163 views
  • Likes 3 likes
  • Comments 5 comments
  • vertical_farm
  • sensors
  • simplicity_studio
  • efm32
  • ezr32
Related
Recommended

Getting Started

e14 Contributor
e14 Contributor
17 Sep 2015

A quick start guide for how to get started developing with EFM32, EZR32, and Simplicity Studio.  Also includes some basics on prototyping with sensors, and contains helpful documentation to aid in development.

Attachments:
imagegetting_started.pdf
  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +2
    I like their initiative, but there are lots of microcontrollers in existence that they could have used to solve this particular problem. That said, I am hoping to see someone in the contest prove me wrong…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to DAB +1
    DAB, I think that there are tons of reasons they have chosen this board instead of another, also if equivalent. And the choices can be totally independent by the specific hardware (supposed) superiority…
  • RWReynolds
    RWReynolds over 11 years ago in reply to DAB +1
    The one thing that might set the SiLabs boards apart is the low energy aspect. I know there are basically low energy micro wars going on right now. So I'd have to do some pretty major research to prove…
  • RWReynolds
    RWReynolds over 11 years ago in reply to amgalbu

    Ambrogio,

     

    What do you think of a custom board, specifically designed for agricultural applications, based on the EFM32 micro?

     

    The example code and IDE are definitely superior.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago

    I don't think this is the ultimate board for agricultural applications. It's obviously a diy board for prototyping as many other boards out there

    In ny case, in my opinion it's a really good board and I really like the quality of the sofware and samples provided

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to DAB

    The one thing that might set the SiLabs boards apart is the low energy aspect. I know there are basically low energy micro wars going on right now. So I'd have to do some pretty major research to prove the SiLabs is the best.

     

    One thing that might make that so however is the multiple low energy levels, 4 is a lot, the wake-up times and the level of functionality available in some of the low energy states.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to DAB

    DAB,

     

    I think that there are tons of reasons they have chosen this board instead of another, also if equivalent. And the choices can be totally independent by the specific hardware (supposed) superiority.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    I like their initiative, but there are lots of microcontrollers in existence that they could have used to solve this particular problem.

     

    That said, I am hoping to see someone in the contest prove me wrong and show conclusively that this board is superior for agriculture control applications.

     

    DAB