Flexible, cost-optimized embedded designs with Xilinx FPGAs – Super Easy or difficult?
Download solutions for this workshop here: http://avnet.me/arty_s7-50_mblz_soln
In order to follow along and take full advantage of this workshop complete the first lab by downloading and installing Vivado 2020.1. Then download the attached lab 2 along with the C file and complete the pre-lab assignment. You will need to purchase the Arty-S7Arty-S7 and the Pmod SensorPmod Sensor board to follow along if you have not done so already.
You can view a Q&A of this session here: Webinar Briefing & FAQ: Arty-S7 Workshop: Part 3: Rapid Sensor Prototyping with Digilent Peripheral Modules is Available On-Demand!
The Spartan-7 FPGA offers the most size, performance, and cost-conscious design engineered with the latest technologies from Xilinx and is fully compatible with Vivado Design Suite versions 2017.3 and newer. Putting this FPGA in the Arty form factor provides users with a wide variety of I/O and expansion options. Use the dual row Arduino® connectors to mount one of the hundreds of hardware compatible shields available, or use the Pmod ports with Digilent's pre-made Pmod IP blocks for a more streamlined design experience. Arty S7 was designed to be MicroBlaze ready and comes out of the box ready to use with the free Xilinx WebPack licensing with the Vivado Design Suite.
Get started building custom microcontroller designs with Xilinx FPGA as it’s easier than ever!
In this seminar series, we’ll explore how Xilinx FPGAs and SoC’s mitigate common challenges engineers encounter when building embedded designs. You’ll discover Xilinx’s embedded solutions options as well as diverse IP library, including partner IP, that enables anyone to build a complete and custom embedded solutions.
We’ll walk through the steps getting started using Xilinx design tools to build a custom microcontroller from installing the design tools to communicating with an external sensor. And you’ll find out that this is easier than ever and anyone can do this!
Here's a good primer that shows you all the cool things you can do with Arty-S7 board:
Session 3:
This is the final part in a 3 part series. To take advantage of this you will need to follow along and complete each of the previous two workshops (links below)!. You will also need to purchase the following products online:
![]() | ![]() |
Buy NowBuy Now |
Buy NowBuy Now |
Each session will be available On Demand at the conclusion of the live presentation. However, if you attend live then you will be able to ask questions or address any issues you have when following along.
Dates and Register for Free:
The Presenters:





Top Comments