Join Cahit Gezgin, South Central FAE, as he discusses the use of the SupIRBuck on-line design tool for accelerating design cycle as compared to manually selecting, matching and testing high and low side FETS in Point of Load applications. He will demonstrate how initial designs can be generated in minutes as compare to hours or days in the lab. This design tool supports IR's latest Gen II devices delivering from 2-15A output power with input voltage on these devices ranging from 1.5V to 27V. They are excellent choices for power management in the embedded computing, FPGA/MCU, computing, networking and industrial markets. Prize information: 5 attendees will be chosen to receive their choice of a SupIRBuck eval kit. About this prize: These kits are suited for applications requiring from 2-15A output and are excellent choices for power management in the embedded computing, FPGA/MCU, computing, networking, and industrial markets. These SupIRBuck devices are all supported by our on line design tool http://www.irf.com/design-center/mypower/ which will ensure than any design efforts can be approached with a minimum of analog design experience / knowledge. |