Learning Center
  • Learn
  • More
Learning Center
Blog Experimenting with Op Amps: Schmitt-trigger
  • Blog
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Learning Center to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 18 May 2023 7:55 PM Date Created
  • Views 18652 views
  • Likes 20 likes
  • Comments 31 comments
  • opamp
  • analogue
  • analog
Related
Recommended

Experimenting with Op Amps: Schmitt-trigger

Jan Cumps
Jan Cumps
18 May 2023

The Art Of Electronics features a set of practical op-amp circuits. One of them is an op-amp controlled Schmitt-trigger. In this post, I build the circuit and show some lab techniques. 

image
image source: edited photo of page 267 of my copy of The Art Of Electronics, 3rd edition

A Schmitt-trigger is a circuit that will clean up a noisy digital input signal. In the ideal world, digital signals are low or high. In the real world, there can be noise on those signals. When you switch between levels, that noise may cause glitches in the output, if the signal crosses the logic level a few times while switching - due to the noise:

image
image source: my capture of the actual circuit

The purpose of the Schmitt-trigger is to take the first logic level crossing, and ignore the noise. It builds a safety zone (hysteresis) that takes care that noise will not generate bounce in the output.

This post tries to address two topics: 

  • build and analysis of the circuit
  • how you can test it

The circuit is simple:

  • the non-inverting input of the op-amp is set to a reference point (the logic level), defined by a resistor divider. In this case: Vref / 2 = 2.5 V
  • the input that needs to be cleaned up goes to inverting input
  • assuming a gain of 1: when the inverting is above the non-inverting, the output wants to go negative. When the inverting input is below the non-inverting, the output wants to go positive

If the input hovers around that switching point when changing levels - because the input signal is noisy - the output would glitch.at each crossing. during the level switch

image

What we want, is that the output immediately reacts at the first crossing, then keeps its value until the input is switching again. We can achieve that with positive feedback. Positive feedback boosts the gain and will exaggerate the effect of the first level crossing. Instead of nicely following the input, it will flop to the right power rail. Then that feedback will help to keep the op-amp in that state- overruling the noise. The op-amp will only flip back if the input has switched enough to overcome that feedback hold. It splits the logic level into two logic levels: one high voltage level, and one low level. The op-amp will only flip output if the input has moved from above the high level until under the low level, or the other way around. That's hysteresis. That's a Schmitt-trigger.

These levels can be calculated. The high level is defined by the voltage set on the non-inverting input. The low level is a function  of the positive feedback (R7 and R6 || R5). (read comment  (Missing Forum Reply)  and follow ups)

Building the circuit

Although a comparator is better suited for this, I used an op-amp. In this case, one that can be driven to ground rail: LM324N. It's not necessary to have a rail-to-rail or to-ground op-amp. A simpler one may meet your requirements. As voltage reference, I used an 7805.

image

For first tests, I used a potentiometer to control the input, and an LED to see what happened on the output

image

First measurements with a multimeter

I probed the input voltage with a voltmeter and used the potentiometer to move that input value between 0 and 5 V. Then I looked if the LED switched on or off. This learned me that the logic levels are 1.9 V and 2.8 V. I also looked at the switching behaviour of the output, with a handheld oscilloscope:

image image

This is good. My potentiometer movements were slow, but the output switches fast. The speed may be improved by putting a small capacitor in parallel with the feedback resistor (10 - 100 pF).

Test the level crossover with an arbitrary waveform generator

The first test shows that the trigger switches fast when the expected levels are crossed. But it's not an easy way to prove that the hysteresis deals with multiple level crossings. An arbitrary waveform generator can help to create multiple crossings. I used an affordable Multicomp Pro MP750065 to generate such a form:

image

On this image, you see that at the low level, the threshold is crossed several times, but the design nicely ignores it. It will only entertain low level switches once the signal has crossed the high level:

image

That's it. If you look at the breadboard photo, you may spot a flat cable. That's because I'm preparing another post where I try to automate the measurements, using a DMM6500 and a 10 channel multiplex card. But that 'll be posted in the  Test & Tools  area …

image

  • Sign in to reply
Parents
  • DAB
    DAB over 3 years ago

    Well done Jan.

    I remember when the first schmitt trigger IC's came out.

    They were so useful for debouncing switches and buttons.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to DAB

    The National Semiconductor 1972 databook that michaelkellett mentioned in another post, has a nice JFET  + BJT Schmitt-trigger.
    image
    image source: NATIONAL LINEAR APPLICATIONS HANDBOOK January 1972, from archive.org. Fair use.

    I'm rabbit-holing myself in that book these days Slight smile.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to DAB

    The National Semiconductor 1972 databook that michaelkellett mentioned in another post, has a nice JFET  + BJT Schmitt-trigger.
    image
    image source: NATIONAL LINEAR APPLICATIONS HANDBOOK January 1972, from archive.org. Fair use.

    I'm rabbit-holing myself in that book these days Slight smile.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jc2048
    jc2048 over 3 years ago in reply to Jan Cumps

    Be aware that, depending on the JFET you choose, the thresholds may well be below ground. Might be useful with a fairly large signal around earth (ac coupled, with a load resistor to 0V), but you might be puzzled as to why it's not doing anything if you feed it a signal between the rails.

    I looked at a bipolar transistor Schmitt here

    /members-area/personalblogs/b/blog/posts/transistors-the-schmitt-trigger

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to jc2048
    [quote userid="36226" url="~/learn/learning-center/f/forum/52955/experimenting-with-op-amps-schmitt-trigger/209463"]Be aware that, depending on the JFET you choose, the thresholds may well be below ground. Might be useful with a fairly large signal around earth (ac coupled, with a load resistor to 0V), but you might be puzzled as to why it's not doing anything if you feed it a signal between the rails.[/quote]

    Simulating with a jfet (switch type) and bjt (not a high gain one) I have here:

    image

    jfet schmitt trigger.zip