CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Forum do we need to buy a battery for codebug to work
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 13 subscribers
  • Views 1725 views
  • Users 0 members are here
Related

do we need to buy a battery for codebug to work

e14 Contributor
e14 Contributor over 11 years ago

do we need to buy a battery for codebug to work

pls let me know

  • Sign in to reply
  • Cancel

Top Replies

  • notdodgy
    notdodgy over 11 years ago +1
    I have used it with a battery and have heeded the warnings about removing it. Removing the battery needs some kind of insulated tool* to push it out as it is a tight fit to both insert and remove. Lollipop…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to notdodgy +1
    CodeBug + Lollypop maybe a good bundle Enrico
Parents
  • gregoryfenton
    0 gregoryfenton over 11 years ago

    You can add a battery to make it work without a USB connection.
    Using a battery adds its own set of problems, including one that can kill a Raspberry Pi.

    1: You need to hold A and B buttons for 10 seconds to reset the device so you can reprogram it over USB

    2: Connecting a CodeBug to a Raspberry Pi via the GPIO ports will kill the device if a battery is installed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gregoryfenton
    0 gregoryfenton over 11 years ago

    You can add a battery to make it work without a USB connection.
    Using a battery adds its own set of problems, including one that can kill a Raspberry Pi.

    1: You need to hold A and B buttons for 10 seconds to reset the device so you can reprogram it over USB

    2: Connecting a CodeBug to a Raspberry Pi via the GPIO ports will kill the device if a battery is installed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to gregoryfenton

    Connecting a Codebug to a Pi by GPIO and simultaneously powering Via USB killed a Pi, but I'm not sure that a battery powered codebug will damage a Pi, I would suspect it would be OK.

     

    The USB powered codebug fed 5V into the Pi's 3V3 GPIO, a 3V CR2032 won't kill the Pi.

    The CR2032 may be damged by this process.