CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Forum Heavy Load Switching with CodeBug
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 14 subscribers
  • Views 3067 views
  • Users 0 members are here
  • codebug
  • transistor
  • relay
Related

Heavy Load Switching with CodeBug

spannerspencer
spannerspencer over 11 years ago

Has anyone tried switching slightly heavier loads using the CodeBug's legs, either using a transistor or a relay? I'm working on something that'll need to switch two loads on and off that I'm pretty sure would melt the CodeBug if I did it directly (maybe 1-2 amps each). I'm thinking that something as simple as a transistor, switched from one of the legs, would do the job, but thought I'd ask if anyone's experimented this as yet?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago +4
    The 'GPIO Explained' schematic with the transistor and relay should work too. (For some reason the editor is mangling the URL - will raise a feedback & support request. Circuit is below): ( Finder 32.21…
  • michaelkellett
    michaelkellett over 11 years ago in reply to jc2048 +2
    Oh John, you're such an optimist I read the same data sheet and come away with 40 - 50 mOhms (40 @ 2.5V gate drive + about 30% for being hot). But still good for 3A (just about at ambient = 25) MK
  • mcb1
    mcb1 over 11 years ago +1
    At the risk of a certain intervention ... http://www.itead.cc/electronic-brick-5v-relay.html?___SID=U http://www.itead.cc/2-channels-5v-relay-module.html?___SID=U If you check the wiki they include a transistor…
Parents
  • shabaz
    0 shabaz over 11 years ago

    The 'GPIO Explained' schematic with the transistor and relay should work too.

    (For some reason the editor is mangling the URL - will raise a feedback & support request. Circuit is below):

    image

     

    (Finder 32.21.7.005.2000Finder 32.21.7.005.2000 is a convenient relay for up to 6A, fits stripboard nicely).

    Or a MOSFET based circuit, but I left them out of GPIO Explained due to opportunities to go wrong if people attempt to use alternatives!),

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • spannerspencer
    0 spannerspencer over 11 years ago in reply to shabaz

    Excellent suggestion, Shabaz, and I'm now wondering whether to go with Jon's MOSFET option, or whether to get a double pole relay and switch both loads from just one of the CodeBug's legs. Although I may need to control them separately... I'll have to think about that some more image

     

    Either way, always appreciate the ideas from all your guys!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to spannerspencer

    Hi Spanner,

     

    Personally I'd go with Jon's suggestion for my own boards, only caveat is that it is a surface mount device which not everyone is comfortable with. If you're using a relay, then you may as well use the NPN method, since it doesn't care what specific NPN transistor you use.

    But yes, many ways to swing a cat : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago in reply to spannerspencer

    Hi Spanner,

     

    Personally I'd go with Jon's suggestion for my own boards, only caveat is that it is a surface mount device which not everyone is comfortable with. If you're using a relay, then you may as well use the NPN method, since it doesn't care what specific NPN transistor you use.

    But yes, many ways to swing a cat : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jc2048
    0 jc2048 over 11 years ago in reply to shabaz

    Absolutely. And there may be real advantages to having the isolation that the relay gives; without knowing a bit more about what "Spanner Spencer" is trying to do it's difficult to say.

     

    The bipolar transistor is much more robust handling-wise, too, particularly if poeple aren't used to electronics and don't understand about the possibility of static damage.

     

    Soldering an SOT23 is quite easy, though. They're probably the easiest SMD parts to prototype with (at least I can see the things, which isn't the case with some of the surface mount resistors you can get now).