CodeBug
  • Learn
  • Learning Center
  • STEM Academy
  • CodeBug
  • More
  • Cancel
CodeBug
Forum Heavy Load Switching with CodeBug
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join CodeBug to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 14 subscribers
  • Views 3070 views
  • Users 0 members are here
  • codebug
  • transistor
  • relay
Related

Heavy Load Switching with CodeBug

spannerspencer
spannerspencer over 11 years ago

Has anyone tried switching slightly heavier loads using the CodeBug's legs, either using a transistor or a relay? I'm working on something that'll need to switch two loads on and off that I'm pretty sure would melt the CodeBug if I did it directly (maybe 1-2 amps each). I'm thinking that something as simple as a transistor, switched from one of the legs, would do the job, but thought I'd ask if anyone's experimented this as yet?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago +4
    The 'GPIO Explained' schematic with the transistor and relay should work too. (For some reason the editor is mangling the URL - will raise a feedback & support request. Circuit is below): ( Finder 32.21…
  • michaelkellett
    michaelkellett over 11 years ago in reply to jc2048 +2
    Oh John, you're such an optimist I read the same data sheet and come away with 40 - 50 mOhms (40 @ 2.5V gate drive + about 30% for being hot). But still good for 3A (just about at ambient = 25) MK
  • mcb1
    mcb1 over 11 years ago +1
    At the risk of a certain intervention ... http://www.itead.cc/electronic-brick-5v-relay.html?___SID=U http://www.itead.cc/2-channels-5v-relay-module.html?___SID=U If you check the wiki they include a transistor…
Parents
  • jc2048
    0 jc2048 over 11 years ago

    A MOSFET like this would do you (assuming that your load is operating from a voltage less than 20V)

     

    http://uk.farnell.com/taiwan-semiconductor/tsm2312cx/mosfet-n-ch-20v-4-9a-sot23/dp/1864587

     

    The Vbe threshold is low enough that the 3V CodeBug outputs will switch it. The on resistance is only 27mOhms, so even at 3A it only has to dissipate a quarter of a watt (0.243W) which the package alone should manage.

     

    Connect the gate to the CodeBug output, the source to GND, and the drain to your load (with the other side of the load connected to the supply you're using). Remember to connect the ground of the CodeBug and the ground of the load power supply together.

     

    If the load is inductive (coil of some sort) include a catching diode as per the transistor circuit in shabaz's post.

     

    Observe static precautions handling the transistor before you get it wired in the circuit.

     

    If you want to prevent it turning on and off  before the CodeBug initialises its output pin ("flapping around" to use the technical term), include a resistor from the gate down to ground to keep the MOSFET turned off until it is actually being properly driven by the output.

     

    If you decide to take this approach, let us all know how you get on.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • spannerspencer
    0 spannerspencer over 11 years ago in reply to jc2048

    Ah, nice! I was just this moment looking at an AOT460 MOSFET for the same purpose, Jon -- but the one you suggested looks preferable (cheaper, too!). Excellent suggestion, and thanks for the setup description.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • spannerspencer
    0 spannerspencer over 11 years ago in reply to jc2048

    Ah, nice! I was just this moment looking at an AOT460 MOSFET for the same purpose, Jon -- but the one you suggested looks preferable (cheaper, too!). Excellent suggestion, and thanks for the setup description.