microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
micro:bit Blog BBC micro:bit - Submit your Big Ideas
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jlucas
  • Date Created: 14 Jun 2016 4:23 PM Date Created
  • Views 7544 views
  • Likes 13 likes
  • Comments 47 comments
  • bit
  • micro:bit
  • bbc micro:bit
  • bbc
  • microbit
  • big ideas
  • ten bbc micro:bit projects
Related
Recommended

BBC micro:bit - Submit your Big Ideas

jlucas
jlucas
14 Jun 2016

image

 

Introduction

 

Our 10 BBC micro:bit Projects in 10 Days series introduced the incredible creative potential of this unique pocket sized computer system. But we've really only scratched the surface. Now we want to hear your ideas.

 

The BBC micro:bit is currently only available for sale in the UK through Farnell element14, CPC and our approved re-sellers, but we've managed to secure ten devices to give away to members of our global community.

How to Enter

 

For your chance to get hold of one of these sought-after devices, simply read our 10 BBC micro:bit Projects in 10 Days series and 'like' your two favourite projects to earn the BBC micro:bit badge. Then, leave a comment under this blog telling us about a project you'd like to try out using the BBC micro:bit.

 

The ten participants who submit the best, most creative project ideas will each receive a BBC micro:bit and will be invited to write about their project here on element14.

 

Submissions are open until 23:59 (BST) on Sunday 31st July 2016. Full terms and conditions can be in the attached PDF.

 

To find out more about the BBC micro:bit initiative and the unique functionality of the device, visit the official BBC micro:bit website or read our exclusive interview with Premier Farnell's Strategic Alliance Director Richard Curtin.

Attachments:
image10 BBC microbit projects in 10 days Terms Conditions.pdf
  • Sign in to reply

Top Comments

  • jlucas
    jlucas over 10 years ago +7
    Thanks for all of your submissions guys, some really excellent project ideas here. I'm happy to announce that the following ten members have been selected to receive a BBC micro:bit device to undertake…
  • dougw
    dougw over 10 years ago +5
    I have been intrigued with the BBC micro:bit since it was announced last year. It represents a very ambitious and visionary initiative to boost interest in technology and computing. I suspect the dividends…
  • jlucas
    jlucas over 10 years ago +4
    Apologies for the delay guys. We had some shipping issues but these are now resolved and we'll be sending them out this week. Looking forward to seeing all of your projects.
Parents
  • dougw
    dougw over 10 years ago

    I have been intrigued with the BBC micro:bit since it was announced last year. It represents a very ambitious and visionary initiative to boost interest in technology and computing. I suspect the dividends will reach further than even the optimistic expectations for the program. The features of the micro:bit have been carefully designed to include as much technology as possible for the lowest possible cost. This has resulted in a very impressive module, but there were necessary compromises that had to exclude more expensive displays and user interfaces.

    My big idea is to expand the micro:bit user interface to include a graphical LCD and keypad at the lowest possible cost.

    To do this I would use a Nokia 5110 LCD, which is an extremely low cost and popular display. It has an SPI interface which is also used by some larger LCDs, so expanding to even better displays is not  a huge leap from this low cost starting point.

    For the keypad, I would use a I2C capacitive keypad to eliminate the cost of a whole matrix of electro-mechanical switches.

    I have been avidly following micro:bit documentation as it becomes available and have already designed and printed a small PCB that implements this SPI LCD interface as well as an I2C interface for the keypad.

    It also has 3 analogue sensor connectors and a power switch for the micro:bit.

    I would also 3D print a case to make a complete hand-held computer.

    I am very much looking forward to testing this card out and showing how to implement a low cost user interface for the micro:bit.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to dougw

    That sounds like it could be an enabler for a whole range of interesting projects and activities.

     

    Not sure if it exists or not yet for the micro:bit but what might be quite good is something along the lines of the Pico Technology list of educational science projects/ideas

    https://www.picotech.com/library/experiments

    to try and get young people to start interacting with their wider environment. Project ideas from a wide range of subject areas that both can be done in the classroom as well as at home.

     

    Perhaps one of the interesting things about the micro:bit is that for once there is a captive audience that all have access to the same platform.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 10 years ago in reply to shabaz

    OK. When they become available to buy, I promise I'll get one and do a project with it. Not necessarily the whole of the science interface, though (to do that properly, as a complete, integrated package, would take much more skill and effort than I could throw at it).

     

    Nice name. You're much better tuned to a young audience than I am. micro:lab might work too. It carries some of the same ideas as 'professor' suggests.

     

    Perhaps the micro:professor could have an electron wizzing round her head. [I presume she has to wear a lab coat and glasses as per the regular stereotype.] I'm determined to get an electron in the branding somehow or other.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to jc2048

    There may be scope for two science interfaces here. One bench-top design for classroom science lab type use that can be easily connected up to existing lab type equipment and then a low cost handheld 'multimeter/logger' type one for use by the pupils for measuring and logging data outside of the classroom in field/home environments.

     

    One aspect to consider perhaps is the final transfer of the logged data and how this is recorded longer term. I can still remember having to cutting up ticker tape and tape/glue it into my Physics workbook in order to keep a record of the experiment data for later revision purposes. With a data logger however, may need to consider some sort of till roll type printer attached to the science interface in order to quickly allow the pupils to get a hard copy that can be taped into their workbooks.

     

    Similar with a portable science interface. If we are going to encourage the class to start data logging in the field, then there will need to be some mechanism to off-load and archive that data somehow for later analysis and sharing or inclusion in a project report.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to jc2048

    It looks as if Seeed Studio have created a sensor starter kit geared toward science type experiments.

     

    Grove Physics Kit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 10 years ago in reply to beacon_dave

    Hmm. We've hardly started and you're already forking the project.

     

    I agree though. Definitely room for both.

     

    Perhaps for the handheld one you could allow for three plug-in sensors. Then you could call it a Tricorder. (Joke, though plug-in sensors is quite a nice idea).

     

    For the instruments that I was thinking of [more of an engineering interface, really, rather than a science one] I assumed that the control panel would be a tablet connecting via the BLE (is that technically possible? - I don't know much about BLE, or tablets come to that). Scope traces wouldn't make much sense on a 5x5 LED array. That would immediately lead to storage capability and hardcopies of graphs and whatnot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to jc2048

    Yes, you should be able to use a BLE paired tablet as an interface.

     

    BBC microbit basic bluetooth capabilities demo

    https://vimeo.com/153078747

     

    It means that the effective cost rapidly increases though if you don't already have the tablets available. In some cases one might be better off with a R-Pi with a small touch screen - similar to Ben Heck's Pi BitScope project.

     

    Episode 223: Ben Heck’s Raspberry Pi Bitscope Mod Episode

     

    The 5 x 5 LED matrix is rather limiting in this respect which is why Douglas' low cost UI sounds like it will be a very useful project. Especially for logging applications out in the field where you may not want to carry an expensive/bulky iPad tablet around with you. Once back at home then yes, you could pair up over BLE to transfer, analyse and perhaps submit the data via a virtual learning environment.

     

    In the classroom, if the teacher is the only one with the tablet then they will likely have to pair and disconnect the BLE 20-30 times to get the data off each micro:bit in turn to retrieve the logged data so as it can be saved/printed for later use.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 10 years ago in reply to jc2048

    Yes, you should be able to use a BLE paired tablet as an interface.

     

    BBC microbit basic bluetooth capabilities demo

    https://vimeo.com/153078747

     

    It means that the effective cost rapidly increases though if you don't already have the tablets available. In some cases one might be better off with a R-Pi with a small touch screen - similar to Ben Heck's Pi BitScope project.

     

    Episode 223: Ben Heck’s Raspberry Pi Bitscope Mod Episode

     

    The 5 x 5 LED matrix is rather limiting in this respect which is why Douglas' low cost UI sounds like it will be a very useful project. Especially for logging applications out in the field where you may not want to carry an expensive/bulky iPad tablet around with you. Once back at home then yes, you could pair up over BLE to transfer, analyse and perhaps submit the data via a virtual learning environment.

     

    In the classroom, if the teacher is the only one with the tablet then they will likely have to pair and disconnect the BLE 20-30 times to get the data off each micro:bit in turn to retrieve the logged data so as it can be saved/printed for later use.