microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
micro:bit Blog BBC micro:bit - Submit your Big Ideas
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jlucas
  • Date Created: 14 Jun 2016 4:23 PM Date Created
  • Views 7570 views
  • Likes 13 likes
  • Comments 47 comments
  • bit
  • micro:bit
  • bbc micro:bit
  • bbc
  • microbit
  • big ideas
  • ten bbc micro:bit projects
Related
Recommended

BBC micro:bit - Submit your Big Ideas

jlucas
jlucas
14 Jun 2016

image

 

Introduction

 

Our 10 BBC micro:bit Projects in 10 Days series introduced the incredible creative potential of this unique pocket sized computer system. But we've really only scratched the surface. Now we want to hear your ideas.

 

The BBC micro:bit is currently only available for sale in the UK through Farnell element14, CPC and our approved re-sellers, but we've managed to secure ten devices to give away to members of our global community.

How to Enter

 

For your chance to get hold of one of these sought-after devices, simply read our 10 BBC micro:bit Projects in 10 Days series and 'like' your two favourite projects to earn the BBC micro:bit badge. Then, leave a comment under this blog telling us about a project you'd like to try out using the BBC micro:bit.

 

The ten participants who submit the best, most creative project ideas will each receive a BBC micro:bit and will be invited to write about their project here on element14.

 

Submissions are open until 23:59 (BST) on Sunday 31st July 2016. Full terms and conditions can be in the attached PDF.

 

To find out more about the BBC micro:bit initiative and the unique functionality of the device, visit the official BBC micro:bit website or read our exclusive interview with Premier Farnell's Strategic Alliance Director Richard Curtin.

Attachments:
image10 BBC microbit projects in 10 days Terms Conditions.pdf
  • Sign in to reply

Top Comments

  • jlucas
    jlucas over 10 years ago +7
    Thanks for all of your submissions guys, some really excellent project ideas here. I'm happy to announce that the following ten members have been selected to receive a BBC micro:bit device to undertake…
  • dougw
    dougw over 10 years ago +5
    I have been intrigued with the BBC micro:bit since it was announced last year. It represents a very ambitious and visionary initiative to boost interest in technology and computing. I suspect the dividends…
  • jlucas
    jlucas over 10 years ago +4
    Apologies for the delay guys. We had some shipping issues but these are now resolved and we'll be sending them out this week. Looking forward to seeing all of your projects.
  • bhavikbhansali
    bhavikbhansali over 10 years ago

    Hello.....

     

    My idea 1 is to  develop the BBC micro:bit North Indicator by using the BBC micro:bit compass as well as 5 X 5 LED matrix.

    By using the data of compass arrow in LED matrix is continuously shows the NORTH Direction. which means if anyone rotate towards north to east the arrow at LED matrix will rotate in opposite direction to show the north indicator. and in this i will use one of the push button as reset button to reset the entire north indicator program. Entire thing is run on simple 2 AA battery.

     

    My idea 2 is to develop the BBC micro:bit Mood Indicator by using the BBC micro:bit compass as well as 5 X 5 LED matrix.

    By using the Bluetooth Low Energy on board to recive the person mood through mobile app and show it in LED matrix. And in this i will use one of the push button as reset button to reset the entire program. Entire thing is run on simple 2 AA battery.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fyaocn
    fyaocn over 10 years ago

    Micro:Bit is one unique board, not for its fully function and powerful feature, but for its easy to use and easy to learn even for Kids.

    I have to admit that this time BBC is ringing the bell for next-generation hero from UK. If so, the vote out of EU is not problem, because UK is still taking a lead.

    My propose is to use minimum resources for a fun toy. A BLE controlled crossbow blot to fire a cotton ball stick with paints on head.

    The crossbow blot is fixed on one SG90 steering driven platform. Try to use only 3 Digital/Analog pins to control 2-D angle and fire-button to let off the cotton ball stick.

    Just try to amuse some naughty kids.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello, my idea is to create an watchdog for blind people or for people who have low vision.

     

    All this can be achieved thanks to the small size of the micro bit and:

     

    1. An array of infrared sensors 8 × 8 which serves to make a recognition of the person
    2. Ultrasonic sensor for the detection of possible obstacles and of the relative distance
    3. bluetooth module with the ability to interact via a cell so that if the person needs assistance have to press a button or connect to the voice recognition and sends its GPS coordinates to a fixed number, this advantage of the GPS module of the mobile
    4. pressure sensor to detect the heartbeat and possibly monitor it via your mobile phone
    5. conductive liquid sensor, this sensor provides the ability to tell if the visually impaired person is walking on a slippery surface and then take precautions

        3 motors for vibration

        a battery power supply

     

    Possible additions are 2:

     

    • integrate it to the glasses, all the sensors on the front of the eyeglasses in such a way that the micro can process the information in a specific direction and insert the 3 moped vibration on the lateral slats, this is because the type of vibration the person understands if it has a simple obstacle in front, or a slippery surface, or a person
    • The second alternative is to integrate it with a stick, this to ensure that we exploit the stick support to proactively report the presence of slippery surfaces and, if desired, you can use a combination of accelerometer, gyroscope and ultrasound sensor to understand if in the next few centimeters, there it will a step, and also because the stick can be integrated flexible photovoltaic panels to extend the life of the device.

     

    I thought to be able to integrate the stick also for a possible energy recovery through a piezoelectric placed under the stick, in such a way that every time the stick is placed on the ground there is a quantity of energy recovered.

     

     

     

    I hope I have explained to outline my idea and that it is of interest

     

    Good day

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to beacon_dave

    Does anyone know if they still use ticker tape timers in school physics experiments for measuring acceleration ?

     

    If so, just pondering if this could be modernised slightly with the likes of the micro:bit. Either by using the built-in accelerometer, however that may not be so clever when dropping weights, so alternatively by using a punched ticker tape with an optical sensor and a micro:bit as a data logger, giving near real-time analysis of that data without the need for the rather tedious measuring of dots and manually plotting graphs. The 'timer mechanics' could be a simple plug-on shield to the micro:bit containing a photodiode a couple of tape guides and even use the micro:bit's built in LED's as the light source. Might need to mount it on a weighted base to prevent it from flying off the table though.

     

    The likes of Douglas's LCD display idea could provide access to the data or alternatively it could be transferred to the teacher and displayed on a large screen.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oksbwn
    oksbwn over 10 years ago

    I would love to tryout this board and make a health tracker which will record the daily physical activities fitted into the shoes and will sync the data to smartphone or server for analytics. That can again be extended by pairing with smartphone to so that any accidents with the person can be detected.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>