microbit
  • Learn
  • Learning Center
  • STEM Academy
  • microbit
  • More
  • Cancel
microbit
microbit Forum BBC micro:bit battery power
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join microbit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 53 subscribers
  • Views 4697 views
  • Users 0 members are here
Related

BBC micro:bit battery power

spmbrown
spmbrown over 10 years ago

Not asking about power via USB micro connector. What kind of JST connector is required? There are lots of different connectors known generically as JST.

 

Does anyone know the tolerance +/-V for battery supply. Is there a voltage regulator on the board?

 

The reason I require this information and the reason it should have prominence in product specifications and FAQs is to know whether rechargeable batteries may be used.

 

Can I use two NiMH? How many? 2 x 1.2V = 2.4V or 3 x 1.2V = 3.6V

 

What about LiPo batteries e.g. from mobile phones or those used for RC models (for example) at 3.3V & 3.7V

 

If anyone can tell me specifically which JST connector to use and what battery voltages are OK, I can make and/or re-purpose my own battery packs.

 

Stephen

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +1
    According to this article, the voltage was brought all the way up to 4v. micro:bit Power Consumption | The REUK Blog Not sure how much strain (if any) this would have placed on the components.
  • shabaz
    shabaz over 10 years ago in reply to gadget.iom +1
    Interesting info. As you say, that will likely stress the parts if the circuit is not designed for this. Just checking, looks like the NXP chip on-board is rated up to 3.6V for correct behavioiur, but…
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    According to this article, the voltage was brought all the way up to 4v.

    micro:bit Power Consumption | The REUK Blog

     

    Not sure how much strain (if any) this would have placed on the components.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to gadget.iom

    Interesting info.

    As you say, that will likely stress the parts if the circuit is not designed for this.

    Just checking, looks like the NXP chip on-board is rated up to 3.6V for correct behavioiur, but behaviour is undefined but won't cause damage up to 3.8V. Beyond that damage may or may not be caused for that chip, in the short term or over a long term.

    In practical terms, I would just use a 3V or 3.3V regulator. Since it is designed for connecting to a 2xAA battery pack, 3V is a known good voltage to select for the regulator if a higher voltage source needs to be used.

    A LiPo cell directly connected is not advisable given what information we have currently, since it has such a wide voltage range, up to 4.2V.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago in reply to gadget.iom

    Interesting info.

    As you say, that will likely stress the parts if the circuit is not designed for this.

    Just checking, looks like the NXP chip on-board is rated up to 3.6V for correct behavioiur, but behaviour is undefined but won't cause damage up to 3.8V. Beyond that damage may or may not be caused for that chip, in the short term or over a long term.

    In practical terms, I would just use a 3V or 3.3V regulator. Since it is designed for connecting to a 2xAA battery pack, 3V is a known good voltage to select for the regulator if a higher voltage source needs to be used.

    A LiPo cell directly connected is not advisable given what information we have currently, since it has such a wide voltage range, up to 4.2V.