Most electronic devices need power to function, typically a constant supply voltage. Because fluctuations can happen at the load or the input power source, voltage regulators are used to supply constant voltages. Increased circuit complexity has contributed to the demand for more reliable and efficient DC-DC converter designs. This eBook covers the fundamentals of DC-DC converters and their industrial and commercial applications.
Here's a Sample of the DC-DC Converters eBook
2.1 Operation of a DC-DC Converter