Member and Staff Blogs Father's Day Badge-a-Thon: Shed Dweller
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 8 Jun 2016 11:55 AM Date Created
  • Views 9785 views
  • Likes 20 likes
  • Comments 108 comments
  • fathers day
  • shed
  • badge-a-thon
Related
Recommended

Father's Day Badge-a-Thon: Shed Dweller

spannerspencer
spannerspencer
8 Jun 2016

The shed is the universal domain of the dad. This probably isn't news to you.image

 

But that's nothing to do with the shed itself. What draws the old man to the garden construct is the solitude it promises (aside from the colony of spiders, but their company is necessary to facilitate the absence of other humans), and the tools and toys he can tinker with therein.

 

So to kick off our week's worth of exclusive Father's Day badges, I'd like you to post a comment below, with an accompanying photo, about your current favourite piece of tech that you enjoy playing with alone; whether it's in the shed, your workshop, your office or the cupboard under the stairs where you're allowed to keep all your junk.

 

And let's all show our appreciation for that most noble of structure, the garden shed, by liking this blog post, too!

 

Remember, to get the rest of the Father's Day badges this week, you'll first need to earn this one!

 

You have until 26th June, 2016, to get all the badges, so don't delay!

  • Day One: June 13th - Father's Day Badge-a-Thon: Shed Dweller
  • Day Two: June 14th - Father's Day Badge-a-Thon: Boys' Toys
  • Day Three: June 15th - Father's Day Badge-a-Thon: DIY Ninja
  • Day Four: June 16th - Father's Day Badge-a-Thon: The IoT of Chaps
  • Day Five: June 17th - Father's Day Badge-a-Thon: The Maker
  • Day Six: June 18th - Father's Day Badge-a-Thon: The Maker
  • Day Seven: June 19th - Father's Day Badge-a-Thon: Day of the Dad
  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 10 years ago +11
    Favourite bit of tech? That's tricky. Actually, no it's not - it's always that last thing you bought! Mine would have to be a stero microscope for SMD work. (The laser cutter just to the right comes close…
  • e14 Contributor
    e14 Contributor over 10 years ago +9
    Ah, yes, favorite techie. My "shed" is actually my workshop where I spend most of my "idle" time. You see, I'm a scrollsaw guy. Scrolling is like making pictures from wood. The picture below is me working…
  • rsc
    rsc over 10 years ago +8
    The most fun is turning off the lights and turning on the plasma and the lasers (little ones at home - BIG ones at work). scott
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +8
    Well, my most fun piece of kit right now is the CNC I built, a nice 1500x1500 cutting area... But my Shed is actually my Basement (Too cold in the winters here in Canada to be working in a garden shed…
  • e14 Contributor
    e14 Contributor over 10 years ago +8
    My shed is on wheels - a sort of Mobile Man Cave..... I disappear down to Henry, my Motorhome, to write software and design modular synth hardware for the Raspberry Pi. Henry has a long-range wi fi aerial…
  • balearicdynamics
    balearicdynamics over 10 years ago +7
    In the meantime take a look: Bed -> Kitchen -> table-for-all -> tools -> window -> terrace ... Animals and insects that prefer to live here: spiders, small but very fast to build webs just in one night…
  • Fred27
    Fred27 over 10 years ago +7
    If it's pictures of our shed (rather than the tech in there) we're going for then I'll add this. A fairly recent upgrade to my previous bit of space next to the washing machine. https://0xfred.wordpress…
  • profcooksez
    profcooksez over 10 years ago +7
    I enjoy making things that are not supposed to work ... work. Right now I got this Verifone 3750 for $5 and now I would like to make it work as a USB printer for my PI. Welcome suggestions.
  • jw0752
    jw0752 over 10 years ago +7
    I like to disassemble and salvage old circuit boards for the components which I then study and build into simple circuits to confirm my understanding. Recently I got a ZD-985 desoldering station and this…
  • Nate1616
    Nate1616 over 10 years ago +5
    My favorite gadget would have to be my 3d Printers. My space/office/man cave was taken over when we had our 3rd child so wish i could of showed my setup. But here is one of the printers in my fleet.
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    My favorite tool is no doubt my custom water cooled PC,

    I was going to upgrade the PC, but decided to watercool and overclock it.

     

    I use this for LTSpice, Eagle and much more.

    i5-2500K running at 4.4Ghz with a max temp of 60c. This pic was before I upgraded the graphics card to a Sapphire R9 290X reference card.

    image

    I added another Alphacool radiator for the 290X card with its EK fullcover block

    image

    The reservoir is now mounted higher where the fan is in the pic below. Before that I had to tilt the PC when filling the loop to avoid accidentally running the pump dry.

    image

    I have a DIY class A headamp driving a pair of Philips Fidelio X2's as my PC sound.

    This, and my Weller solder station, is without a doubt my favorite tool for DIY image

     

    I am however in the process of collecting parts for a CNC PCB mill. That will probably become a favorite as well image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to e14 Contributor

    I have to be getting old because I am finding myself saying "I remember when", or "back when I was starting out", then give an example of something with fossilized excrement on it that we used to solve a problem that people don't even have to deal with any more... That said, I am amused that systems have gotten to the point where a cooling system is needed (instead of just a heat sink), which is impressive to think of the clock speeds that are being used causing that kind of heat to build up. Luckily this is a "dad" forum.

     

    Jack

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to jack.chaney56

    Maybe this link sounds interesting to you ... http://www.overclockers.com/an-introduction-to-extreme-cooling/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to jack.chaney56

    Maybe this link sounds interesting to you ... http://www.overclockers.com/an-introduction-to-extreme-cooling/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to balearicdynamics

    I've read up on most things PC cooling, the liquid nitrogen and peltier elements etc is overkill for me. I think mainly competitive overclockers use those methods.