Member and Staff Blogs Father's Day Badge-a-Thon: The IoT of Chaps
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: spannerspencer
  • Date Created: 8 Jun 2016 4:03 PM Date Created
  • Views 7515 views
  • Likes 9 likes
  • Comments 70 comments
  • fathers day
  • internet of things
  • chap
  • badge-a-thon
  • iot of chaps
  • iot
Related
Recommended

Father's Day Badge-a-Thon: The IoT of Chaps

spannerspencer
spannerspencer
8 Jun 2016

What-o chaps! Splendid day, what?image

 

Well, as you know it'll be Father's Day shortly, which is rather splendid, and we're clapping politely in anticipation of the grand show by handing out a week's worth of exclusive Father's Day badges for all you smashing chaps.

 

Ah yes, chaps! Just what is a chap? According to Mr. B:

"A proper chap knows exactly where it's at. A proper chap is a rogue, in well-heeled brogues, and knows exactly when it's right to wear a hat.

 

"He wears it outdoors and takes it off when he gets in, and never matches pocket square and tie.

 

"A proper chap drinks tea or a lovely drop of gin, and a proper chap knows exactly why."

A tad unfairly, the chap can be seen by the uncouth as somewhat old fashioned. Such tosh, of course!

 

However, perhaps you fine fellows can help the chap community to update their already spiffing image by incorporating the Internet of Things into their dandy repertoire? No small task, my good chum.

 

Here's the conundrum I'm chucking toward your mental wickets, and if you'd be good enough to add your idea into the comments so we can have a nice chin wag about it, that'd be splendid. And it simply wouldn't be cricket if we didn't have a proper conversation, so I'll also ask you to stop back a little later on, and post a second comment in response to one of the other chaps' clever notions, too.

 

So that's two comments to land the badge, my good chum!

 

How do we bring together the Internet of Things and chaps? Consider the following components of the chap, and then give them some digital, connected dazzle in the comments section below:

  • A well groomed moustache.
  • A shiny walking cane.
  • A fine pipe.
  • A nice cup of tea.
  • A prim bow tie, or cravat.
  • A dashing tweed jacket.
  • A splendid hat.
  • A lovely drop of gin.
  • A sturdy cricket bat.

 

Remember you'll need the previous Father's Day japes, including the Shed Dweller, Boys' Toys and DIY Ninja badges before you can pin this number to your tweed lapel.

 

You have until 26th June, 2016, to get all the badges, so don't delay!

  • Day One: June 13th - Father's Day Badge-a-Thon: Shed Dweller
  • Day Two: June 14th - Father's Day Badge-a-Thon: Boys' Toys
  • Day Three: June 15th - Father's Day Badge-a-Thon: DIY Ninja
  • Day Four: June 16th - Father's Day Badge-a-Thon: The IoT of Chaps
  • Day Five: June 17th - Father's Day Badge-a-Thon: The Maker
  • Day Six: June 18th - Father's Day Badge-a-Thon: The Maker
  • Day Seven: June 19th - Father's Day Badge-a-Thon: Day of the Dad

 

To put a bit of fuel in your inspiration pipe, here's Mr. B the Gentleman Rhymer to get your dander up. Cheerio old sport!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • dougw
    dougw over 10 years ago in reply to Instructorman +5
    A wee drop of gin.... How about this dispenser I automated - full IoT gin.
  • jwatson
    jwatson over 10 years ago +3
    How about an auto-igniting pipe triggered whenever one dons ones smoking jacket (IoT paired wearable tech/lounge wear) or enters ones manfriend smoking room to play poker! The 'rapopipe'. For the ladies…
  • Workshopshed
    Workshopshed over 10 years ago +3
    A facial recognition system to automatically doff your hat when you pass a lady in the street.
  • fvan
    fvan over 10 years ago in reply to beacon_dave +3
    Have you seen this one? Tipping Tophat Totally Tips! (final submission)
  • balearicdynamics
    balearicdynamics over 10 years ago +2
    MMMMM LET ME THINK A well groomed moustache: Integrating super low energy nano tubes sampling the breathed air just a second before. If the air is not healthy an alarm reach the smartphone "wear your particulate…
  • Workshopshed
    Workshopshed over 10 years ago in reply to spannerspencer +2
    By monitoring the tone of your social media posts a drink maker could automatically select tea or gin.
  • beacon_dave
    beacon_dave over 10 years ago in reply to Workshopshed +2
    A splendid innovation sir - one even worthy of a post to the Ben Heck Show for a build consideration. What does the lady of the show think ? makerkaren
  • spannerspencer
    spannerspencer over 10 years ago in reply to Workshopshed +2
    Auto-Doff -- nice!
  • danielw
    danielw over 10 years ago +2
    Tea has a perfect temperature. Rarely achieved, at Tea°C, one cannot resist the "Second Cup," only to find ones self disappointed. I wager that a cup with thermal profiling allowing one to record the temperature…
  • makerkaren
    makerkaren over 10 years ago in reply to pettitda +2
    I asked Ben to help me make one of these months ago. Attach string of tea bag to device, set and start timer, insert teabag into cup of hot water. When timer goes off, it lifts the tea bag out of the tea…
Parents
  • danielw
    danielw over 10 years ago

    Tea has a perfect temperature. Rarely achieved, at Tea°C, one cannot resist the "Second Cup," only to find ones self disappointed.

     

    I wager that a cup with thermal profiling allowing one to record the temperature of Tea°C.

    After brewing up the cup could signal ether through an BCD (Bone China Display), OHD (On Handle Display) or via a mobile app when the brew has reached Tea°C. A built in heater to maintain Tea°C would be a rather spiffing addition.

     

    Of course a chap would also have to consider environmental influences such as environmental temperature, and weather This is because it's a well known fact that variability between bright sun, overcast, gloomy, drizzle, rain, raining cats and dogs, absolutely stair rodding, and the occasional flurry of snow can all have a bearing on Tea°C.

     

    Finally, This information can be downloaded to the international brewtopia database. So when partaking at the abode of an acquaintance one can simply touch ones phone and NFC will adjust the cup as required, thus ensuring that tea temperature will not be of concern.

     

    To assist the Brewer when venturing from ones own abode, the Brewtopia database could also store other preferences such as Steep Time ( A measure of how long to brew the tea from weak to builders, also referred to as stewosity), Milkiness (This one's obvious), and if you're sweet enough already (and if not, how many sugars you require with handy conversions between lumps, teaspoons, heaped teaspoons and in case one is bereft of a teaspoon, the trusty fallback, the desert spoon!)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 10 years ago in reply to danielw

    That's a good thing ... especially since tea that's too hot can potentially increase the risk of cancer and tea that's too cold isn't really worth drinking ...

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 10 years ago in reply to danielw

    That's a good thing ... especially since tea that's too hot can potentially increase the risk of cancer and tea that's too cold isn't really worth drinking ...

     

    - Gough