Member and Staff Blogs Plotting the Transfer Characteristic of a JFET
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 8 Jan 2020 2:33 PM Date Created
  • Views 7708 views
  • Likes 11 likes
  • Comments 12 comments
  • pulse generator
  • experimenting
  • semiconductors
  • jfet
  • differential amplifier
  • integrator
  • jc2048
  • transfer characteristic
  • op amps
Related
Recommended

Plotting the Transfer Characteristic of a JFET

jc2048
jc2048
8 Jan 2020

Introduction

 

Having used JFETs (type BF256BBF256B) in some of my test circuits whilst experimenting with MOSFETs, I thought it might be interesting to look at the transfer function and see if I could recreate the curve you sometimes see on a datasheet which relates the gate voltage to the drain current.

 

If you're not used to JFETs (Junction Field-Effect Transistors), they're similar to MOSFETs but the insulation between the gate and the channel is provided not by an actual insulator but rather by a reverse-biased p-n junction. The immediate effect of that is we need to be careful not to forward-bias the diode (by raising the gate more than a diode-drop above the source), or at least, if we do, to ensure that the current that flows is suitably limited. Operation of the device is then in the region down from that diode-drop voltage to whatever negative voltage (negative relative to the source) it takes to close off the channel. [I'm referring to n-channel parts here - reverse all the voltages for a p-channel part.]

 

This is what a typical curve might look like. I've taken this from an old app note [1] because the JFET I'm going to be measuring doesn't have any curves at all on the datasheet.

image

 

There are several parameters we might be interested in that we could take from the curve. One of those is the zero-voltage current (the drain current when the gate-source voltage is zero), though that could be easily measured in other ways. Another parameter of interest is the negative voltage where the current falls to zero. A little less obviously, we could get the incremental transconductance from the slope of the curve at a particular gate voltage.

 

The app note I mentioned above is for a tester that does the same as what I'm trying to do here. I didn't discover it until part-way through, so the detail of mine is somewhat different, although the basic principle of operation is similar. If you wanted to build one, you might do better with theirs as it handles n-type and p-type devices; mine is just suitable for the n-type parts that I had available to test.

 

Circuit

 

Here's the circuit I came up with. The JFET I've got as the 'device under test' [DUT] was just an arbitrary choice from the ones in the simulation library. The BF256BBF256B part I'm testing doesn't seem to have a spice model.

 

image

 

The heart of it is an op-amp integrator that generates the ramping voltage that's applied to the gate. That voltage is a downwards ramp, from zero to about -6V. To reset it, I have a simple pulse generator that turns on a MOSFET across the integration capacitor. That periodically discharges the capacitor. It's not all that elegant, but I'm only throwing it together for an experiment.

 

On the output side, the drain of the JFET has a resistor to convert the output current to a voltage and then there's a differential amplifier to shift it down so that it's ground-referenced for the 'scope probe to measure.

 

Here it is built on a breadboard:

 

image

 

I had a couple of problems with it. One simple one was that the reset didn't take the ramp back to zero voltage, but left an offset of about -100mV at the gate. That was a shame as it stops us looking at the zero-volt current so, instead of taking the non-inverting input to ground, I lifted it with a diode drop.

 

The other problem was that the integrator 'sang' a bit. There was a low level of 1MHz oscillation on the ramp. I dealt with that by increasing the size of the integrator capacitor by a factor of ten (and dropping the charging resistor by the same factor) [originally I had 47nF and 47k for the two]. That has the effect of rolling-off the gain faster, which I suppose is why it cut out most of it, but you can still see the effect slightly along the top of the ramp waveform. That might well be down to using the breadboard [capacitance between the strips of contacts], but I can live with it for the purposes of this blog.

 

Testing a BF256BBF256B

 

Here are the results I get when testing a BF256BBF256B part.

 

This shows the gate ramp voltage [yellow] and the drain current [blue]. You can see where the pulse generator does the reset back up to just above zero. The drain current is 100mV = 1mA, so on the following trace we have 2mA per division.

 

image

 

Here it is in more detail.

 

image

 

Finally, this is what it looks like if I get the 'scope to plot it XY, where we see it in the more traditional form. The spread at the top is due to the slight oscillation I just mentioned.

 

image

 

The scale up is 2mA per division, so the zero-volt current is about 9mA. That's in the middle of the range given by the datasheet [6mA to 13mA]. The cut-off is harder to measure because my circuit isn't very good (there's a small offset on the current measurement) and it's difficult to see where it gets to zero. It looks like it may be around -2.7V.

 

The one feature that's slightly surprising is the transconductance. By eye, the transconductance at zero looks to be roughly about 4.5mS (9mA/2V), but that's the minimum value given on the datasheet. Perhaps it's down to the drain voltage (the datasheet uses 15V, but I've only got the 9V of the supply, less a volt for the current sense).

 

Conclusions

 

Although it quickly showed up the limitations of the breadboard, otherwise it worked reasonably well as an experiment. If I have some time I'll measure a selection of parts and see how much spread there is to the zero-voltage current and the cut-off point.

 

[1] Fairchild application note AN-6610 https://www.onsemi.com/pub/Collateral/AN-6610.pdf.pdf

 

If you found this interesting and would like to see other blogs I've written, a list can be found here:
https://www.element14.com/community/people/jc2048/blog/2018/10/24/jc2048-blog-index

  • Sign in to reply

Top Comments

  • dougw
    dougw over 6 years ago +5
    I really like the content you generate.
  • Jan Cumps
    Jan Cumps over 6 years ago +5
    Apart from the whole exercise, I find that each of the separate blocks in the test gig are little gems. The way to create that reset, lifting the level in the integrator, re-referencing the output to ground…
  • fmilburn
    fmilburn over 6 years ago +4
    I am learning a lot from these. Thanks...
  • three-phase
    three-phase over 6 years ago +4
    Very interesting blog to read, thanks for posting. Kind regards
  • jc2048
    jc2048 over 6 years ago +4
    I have a bag with nine BF256B JFETs left in it, so I tested them all to get an idea of the spread of values we might see. Here are all nine curves composited together with Gimp (there really are nine traces…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to Jan Cumps +4
    (maybe we can create a programmable binning device for fets )
  • Jan Cumps
    Jan Cumps over 6 years ago +4
    I keep returning to these blog posts. With the shopping cart i won for the Photonics contest, I ordered 5 N-channel and 5 P-channel jfets. Time to play with discrete components again.
  • genebren
    genebren over 6 years ago +3
    Another nice blog on FETs. Thanks for sharing.
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to jc2048 +3
    Maybe it’s worth binning the ones with identical curves for when you need matched pairs ... (link is to internet archive. on-line library - photo is fair use of an in-context example of my own copy)
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to jc2048 +3
    jc2048 wrote: ... What are you thinking of doing with your FETs? Looking at the properties or doing some design with them? Initially I want to relearn working with them. Get the feeling of driving a FET…
Parents
  • three-phase
    three-phase over 6 years ago

    Very interesting blog to read, thanks for posting.

     

    Kind regards

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 6 years ago

    Very interesting blog to read, thanks for posting.

     

    Kind regards

    • Cancel
    • Vote Up +4 Vote Down