Member and Staff Blogs Simple analog JFET switch - part 2: linear range and limitations
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 22 Jun 2020 7:36 PM Date Created
  • Views 4181 views
  • Likes 6 likes
  • Comments 3 comments
  • ltspice
  • transistor
  • simulation
  • jfet
  • silicon
  • analog
Related
Recommended

Simple analog JFET switch - part 2: linear range and limitations

Jan Cumps
Jan Cumps
22 Jun 2020

I reviewed an analog small signal switch in post 1: Simple analog JFET switch - part 1: schema, simulate and test.

Here I'm checking what the limits are - the small linear part of the operational region where the P-channel JFET acts as a resistor.

image

The circuit is published on neatcircuits.com

 

JFETs are linear for small signals. The schema here is for a consumer audio signal level, and that signal fits in that range for the J176 that I'm using.

image

source: wikipedia

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

source: w2aew youtube channel

 

The device, in the DC stable state (bias condition), has source and drain virtually at ground level.

The gate is also almost at ground level, just a diode drop (D1) above ground.

 

I've simulated this by using LTspice DC operating point analysis.

This time, the resistors are all 3 47K ones.

The biggest difference between the simulation and my bench measurement is the diode drop I measure is 530 mV, not the 509 mV that LTspice gives.

image

image: DC operating point simulation (steady state)

 

A P-chanel JFET where the gate is just 0.5 V above source, is conducting.

In the image below, I've indicated what VGS curve this design is operating in when the switch is on:

 

image

source: annotated ON Semiconductor datasheet for J176

 

When testing the design, it all works well, with an input signal of up to 1.6 Vpp.

In the capture below,

  • the yellow trace is a 3 kHz, 1.58 Vpp input signal measured on the drain pin. You can't see it because it's under the output signal, that perfectly matches.
  • the light blue signal is the output of the JFET, measured on the source pin. Perfectly matching (and hiding) the input.
  • the magenta line is the gate. Held at 0.5 V
  • the dark blue line is VGS. Measured with a differential probe because both points are not ground.

 

image

image: oscilloscope capture just before Gate-Source Cutt-off starts

 

But when the amplitude of the input rises (I've put the dashed cursor B at the level where the effect becomes obvious), the source no longer follows the drain.

What's happening?

image

image: oscilloscope capture when Gate-Source Cutt-off is crossed

 

To see that, check the dark blue VGS signal.

At a certain point (I put full-line cursor A there), VGS reaches the Gate-Source Cutt-Off voltage (VGS(off)).

According to the data sheet this is between 1 and 4 V for the J176.

For my transistor, it happens to be around 1.3 V.

VGS is the diode drop - VG. So that gives us an AC leeway of 1.3 V - 0.5 V = 0.8 V on the negative side.

An AC signal with 1.6 Vpp is just manageable with my JFET.

Increasing the supply voltage will not help, because the diode drop is the deciding factor here, and it's reasonably flat when using large pull-up resistor that draw only small current.

image

source: ON Semiconductor datasheet for J176

 

The effect on the output is pertinent. Once the signal pushes the source low (and as such increases the positive voltage between source and gate), you get closer to that cut-off point.

One it's reached, the FET stops being the linear resistor it was and the output gets strongly attenuated.

It's some kind of self-balancing system because the further above the cut-off, the stronger the effect.

This will render the negative part of the sinus input signal into a flattened, lob-style curve, while the positive half is still good.

 

Here is LTspice's take on this situation:

image

image: LTspice simulation, taken at input and output before and after the decoupling capacitors

 

The output is slightly attenuated vs the input in LTSpice because I measured before the input cap and after the output.

I can easily change that, but maybe this can be an exercise for you? The model is attached to post #1.

 

Given this effect, and taking worst case (VGS(off) = 1 V), we are still safe for a consumer product's line signal.

To handle professional audio line levels, you should consider  a J175 or another JFET with a higher VGS(off).

 

Related blog
Simple analog JFET switch - part 1: schema, simulate and test
Simple analog JFET switch - part 2: linear range and limitations
  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 6 years ago +2
    Interesting and very nice follow up on part 1. John
  • DAB
    DAB over 6 years ago +2
    Great post Jan. It has been a while since I last played with some FETs so I found your post very interesting. DAB
Parents
  • b139b
    b139b over 3 years ago

    This is a very interesting post! Thank you for posting this! I found it while searching for a replacement JFET for my Grundig TS1000 reel to reel recorder. This recorder uses a JFET type GF405 to switch audio signals. There is no replacement nor information for the GF405 on the net. T12 on the schematic. 

    Could you please give me a tip witch JFET type I could use as a replacement? Are there some types that "sounds better" for audio applications?

    Thank you Blush imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • b139b
    b139b over 3 years ago

    This is a very interesting post! Thank you for posting this! I found it while searching for a replacement JFET for my Grundig TS1000 reel to reel recorder. This recorder uses a JFET type GF405 to switch audio signals. There is no replacement nor information for the GF405 on the net. T12 on the schematic. 

    Could you please give me a tip witch JFET type I could use as a replacement? Are there some types that "sounds better" for audio applications?

    Thank you Blush imageimage