The Z80 is still manufactured today and I was wondering whether there is any interest for a community or discussion group.
The Z80 is still manufactured today and I was wondering whether there is any interest for a community or discussion group.
Hi Shabaz,
Very interesting musings about Z80 and possible 'mimicry' ... And thank you for the literature suggestions.
I believe having gotten some idea of Sharp policy in the dozen or so years I've made a living out of their products in many applications.
Do share your viewpoint that a lot of Japanese manufacturers of the time had more than enough innovation capability of their own, in order
not having to rely on copying; they did however clever- and selectively enter into strategic alliances and joint ventures.
I was appalled to learn that the company was recently taken over by Foxconn, of all the lousy manufacturers of today ...
The Japanese goverment should be ashamed for not having done anything to prevent this - the company that produced the unique amber
EL-displays for the Space Shuttle and where Philips had to buy all their LCD patents !
Back to the good ol' eighties and Sharp policy: I still feel the only explanation that makes sense for the model number, (LH-)5801, is as follows.
Next to their OEM production of Z80 clones - LH080, etc. - they wanted a proprietary microprocessor design for their indeed innovative line of
pocket computers. However they did not want to isolate these products too much from the brands and models that had become well-known
market leaders, in order to reach the broadest possible acceptance. So they devised the number 5800, with a wink to the 6800; but in order
to prevent the impression that they would suggest to make a predecessor, or down-graded version, they made the number their own by changing
it into 5801. Speculative ? Sure, but have I "entered into the realms of phantasy" ?
There was btw a LH-5803, which was meant to emulate the 1500 in its successor, the PC-1600 in order to attain full SW-compatibility. (It didn't
work 100% - much like my XP Pro overlay on Windows 10; this was probably also the reason for the PC-1600 being a less stable system than the trustworthy 1500).
Cheers
Ray
Hi COMPACT,
Sorry for my late response.
Thanks for your friendly reply, and for sharing your broad knowledge to fill-in some of the white spots in mine.
Further to the Nestlé project (and risking being thrown out by the moderator on account of wandering too much off topic ...): the 'poor'
PC-1500A had to communicate with 68000 processors in the Swiss units. When the info required to tackel this problem didn't come in time
to meet the project deadline, I decided to try and overcome the speed differences ... in BASIC (call me crazy). The only solution to get around
a formal handshake was applying probability calculation. It worked fine and reliable.
Reading the history of the Z80, it seems safe tot conclude that Sharp must have been (one of) the very first (1980/81) to produce a CMOS
derivative (?) with many on-chip extras. Just out of curiosity I've once tested the PC-1500A for power consumption (keep in mind that there
was also an I/O controller on board, the LH-5811). Battery life was specified as 300 hrs, i.e. with the usual unrealistic operational limitations.
So after a fortnight of continously running an endlessly repeated program with heavy duty calculations, that made as much use as possible
of display functions, and most of all of the BEEP option, I expected to find my PC-1500A 'dying'. But after more than 3 weeks only the LCD
contrast showed some signs of a nearing 'low battery' condition. Unfortunately I had to abort the experiment, simply because I needed the
pocket computer for my programming work.
The first assembler, as far as I know, was made by Rasso von Schlichtegroll, fairly soon after the PC-1500's introduction; later he developped
a successful line of system programs and tools under the RvS brand, eventually commercialized by the Holtkötter publishing firm.
Jumping to the present, recently produced emulators may be the best way to keep the PC-1500(A) alive (and leave curious young users
in awe). As to the limited storing capacity of RAM chips in those days: the LH-5811 has a direct adressing capability of 64 kB - nothing fancy;
but because of the PU and PV flipflop registers, the full addressing range was 512 kB. And would you believe it: in the early eighties a small
third party company, AMS in Germany on the Danish border, managed to pack this huge amount of storage inside the pocket computer !
I'm not sure if/how his maybe conflicted with an eventual RAM module in the bay for external memory ... Later they had their Gold Card
produced in Taiwan for the top models in Sharp's organizer line: 256 kB, while Sharp was still fiddling with 32/64 kB.
Didn't know the TI-84 was Z80-based; always wanted to have one, never got around to it ... The origin of my interest stems from the late
seventies, and was thus calculator-oriented. I could go now into the old AOS vs. RPN debate, but this would be a) off-topic, and b) maybe
not of interest to anybody in this group. Suffice it to say that It is useless to try and grasp Sharp's design concept for its pocket computers
without taking her EL-5100 scientific calculator into account.
Cheers
Ray
Hi Ray,
At around that time, a lot of the handheld devices were getting powerful, so the ultimate decision to use that instead of any other device may have been simply because it was what someone was experienced in.
From the very little production/shop floor experience I have, it was interesting (at the places I worked) to see that the tools used in production were different to what the rest of the organisation were using. In other words, different CAD tools, different procedures, and different hardware. I'm not saying it is ropey, but a lot of stuff is designed to be one-off or very low quantity production.
Regarding the suggestion of Z80 origins made to look like a non-Z80 device, I've no idea. Certainly it won't execute Z80 software without modification and assembly with a different assembler.
Many processors at the time were similar, from a birds-eye view. Even the different processor designs that soon emerged like RISC and SPARC still have instruction sets and registers, and buses.
There was historically plenty of anti-Japanese tech sentiment in the 1980's, when many people thought that Japanese firms were copying or stealing ideas. That idea still exists today. It's unfounded, and likely no more than western firms stealing western ideas from each other. Perhaps that sentiment inspired the suggestion that it looks similar to the Z80 I cannot tell, since I don't know where and when that suggestion originated. The Japanese government encouraged firms to buy rights to patented tech, that was a major policy at the time.
Depending how keen you are to research down that road, there are some books worth reading, they mention names of people who would know better than speculation, of which unfortunately there is a lot of on the Internet. The first is We Were Burning, and the second is Industrial Innovation in Japan. The first is an easier book to read. According to that, Sharp was extremely quick off the block developing calculators, and amongst the first to productize (not invent) CMOS, so it's quite natural they would either license a Z80 design, or design their own chip. Neither of which would be good reasons to fake instruction names to look like a different processor.
Hi Ray,
The Nestlé project sounds fascinating.
You'd expect the LH-5801 to be superior to the Z80 for its designated applications. The designers could pick, choose, optimise and add the features that they wanted.
It is was unlikely that a LH-5801 device needed to have the DRAM memory and 8080 legacy support because it was for low power consumption devices such as battery powered calculators.
Itsinbuilt timer is very handy. The Z80 required the addition of a CTC (Counter Timer Counter) or similar to do this.
There's nothing wrong about creating a CPU that's lacking the Z80's index registers. If fact these index registers can be a pain to use. The Game Boy version of the Z80 is also missing these index registers and look at the quality of the software for that.
If you look at most Z80 code, the IX and IY index registers if used, were seemingly used as a last resort. This is because the Index Register op codes need an 8 bit offset to be specified within the instruction.
It's also interesting to note that Cristophe Gottheimer's assembler for the LH-5801 uses the Z80 JR (jump relative) and mnemonics instead official Bcc (Branch) mnemonics. A clue to the LH-5801's origins perhaps?
One thing people always seem to overlook is that the Z80 limitations were set by the memory device performance limitations of the day. The designers at Zilog even incorporated inbuilt wait state support to handle slower memories and DRAM refresh support.
This this in mind the Zilog designers worked out that they could use a 4-bit accumulator and run it twice for 8 bit results in the time taken for a single memory fetch.
At the time common memory devices were small with 1K * 1 Static and 4K * 1 Dynamic RAMs being the most affordable. The larger and faster ones came years later.
Cheers and welcome to the community.
Very!
Hi Shabaz,
Let me try to recapture the lost part of my post with the Nestlé story first.
I meant to argue that your and COMPACT's reply suggested the LH-5801 had less hardware facilities than the Z80:
- "the PC-1500's CPU only has three registers" (you)
- "a Z80 inspired CPU with the index registers missing " (C)
For me this makes it a bit hard to understand, how a pocket computer with this CPU has been able to achieve such extraordinary results
in numerous high-level applications. Or is this just a matter of clever trickery by the application programmers ?
First of all (as far as I know), other than Z80, LH-5801 had 8-bit (full-width) registers - esp. in the accumulator.
Program counter and stack pointer were even 16 bit.
Secondly some items from the feature list of the Sharp CPU:
- (3) Use of a 6-byte general purpose register. in addition to the accumulator. allows to comprise three pairs of 2-byte date pointers. (misspelling Sharp)
- (12) Reducing program steps by means of 28-kind single step vector subroutine jurnp
If only there were a feature-by-feature or architecture comparison of the two microprocessors ...
Judging from the applications side (remember I lack sufficient knowledge of micoprocessors), I would say, LH-5801 was - maybe inspired by some
standard Z80, 6502, or even 6800 - yet an advanced proprietary design with a remarkable number of on-chip peripheral facilities. Your and COMPACT's
observations concerning family traits, in one way or another, are very interesting and seem to confirm my assumption all along, that LH-5801 was just not
your run-off-the-mill Z80 clone.
As stated before, the Nestlé project utilized a MUX. Later someone else devised real multi-tasking software for the PC-1500A. I suppose that requires
a quite sophisticated interrupt scheme/structure (esp. at a clock rate of only little more than 1 MHz), or can one do this by clever programming via a
high-level language ?
Last but not least: thank you all for a friendly welcome into this community !
Cheers
Ray
Hi Ray,
That's interesting that it was used to control part of a Nestle production line. I do recall an episode on TV of 'How It's Made', which showed a production line in a factory which made piano music rolls, and part of it was controlled by an ancient Apple IIe machine. Since it worked, I guess the factory felt no need to port the code to anything more modern. Better to trust what is working : )
Into modern times, and a lot of retail stores in my area run very suboptimal hardware - consumer PCs! - always clogging up with dust from the Manager's office, running slow, and on the floor getting kicked around.
Hi Shabaz,
Thank you for your reply. This was actually the first time ever (I'm 73) I participated in any professional community discussion on the Net.
So please don't mind my many newbie mistakes - one of them not being a prompt replier.
For everyone else here, interested in the Sharp PC-1500(A), your link to the pc-1500.info site is spot on, as this site offers the best,
i.c. most comprehensive info there is.
The LH-5801 microprocessor turned out to be a very powerful tool indeed in many applications of this pocket computer.
One of the projects I've been involved in was at a Nestlé plant for the production of powdered milk. The Swiss manufacturer
of the 5 parallel operating in-stream weighing-doseing units to be installed, required 5 full-fledged PCs as controllers - the chosen
brand being Commodore. The engineer in charge however judged this brand to be below industrial reliability standards, and
proposed the PC-1500A instead, i.e. 1 pocket computer instead of 5 PCs ! (a printer - not its 4-color plotter mate, CE-150 - was added).
Later system SW for real multi-tasking was developped by a third party - we utilized a MUX.
Before the mid-eighties there was also assembler/disassembler, hexmonitor, etc. software available; furthermore a C-compiler was offered,
along with Forth and several extended BASICs.
From your and Compacts reply it would seem the LH-5801 had only
(continued in post nr. 106)
Sorry for the belated response.
Please do share what you have done!