The Z80 is still manufactured today and I was wondering whether there is any interest for a community or discussion group.
The Z80 is still manufactured today and I was wondering whether there is any interest for a community or discussion group.
I worked at Mostek maintaining the Fairchild Sentry testers used to test the Z80s when they first began to manufacturer them. The second computer I every
built (parts, pcb, solder) was the SDB-80 which was the Mostek Software Development Board for the Z80 with 16K bytes (8 - MK4116 16K bit) dynamic RAMs
which Mostek also made. The first wire wrap board I ever made was a 48K byte dynamic RAM board also using MK4116s that worked with the SDB-80. I can
tell you there were a bunch of happy technicians when we were told that Mostek would be second sourcing the Z-80 and even happier when we were told we
could buy SDB-80 kits and build them ourselves! Those were really fun days. I still have a Zilog Z80 in a ceramic package that says it was manufactured in
Dallas even though Mostek was actually in Carrollton a suburb in Dallas County just north of north-west Dallas.
Wow! that's amazing that you got such a large DRAM board working with Wire-wrap.
Do you still have any photos or schematics of it?
It was quite rare to come across Mostek parts in Australia. We usually got Zilog, SGS and Sharp.
And from memory the SGS parts didn't support the undocumented instructions.
Hi COMPACT,
May I add another PC-1500A project story in response to your earlier interest, and present that, assuming you have also read my posts to Shabaz ?
(It would be boring i.m.o. to tell intertwined stories to two forum members, as if they didn't read each others 'incoming' posts, wouldn't it ?)
This story unfolded in the aftermath of PC-1500A's demise - ending in the permafrost of Siberia ...
As the story hasn't anything to do per se with Z80, does it interest you, and would it be acceptable in this thread ?
Would appreciate hearing from you
Cheers
Ray
Hi Shabaz,
As Appendices at the end of the 276 page PC-1600 Tech Ref Manual I found mnemonics, op-codes, and what have you of both the SC- and the
LH-processor. Not my cup of thea, really ... But maybe someone else finds the clues, required to answer the question: was LH-5801/3 a Z80
derivative, or not ?
For me Chapter 7 is much more evocative, and it confirms my belief all along, that not only 'Ol Blue Eyes did everything "My Way" ...
It is quite impressive what Sharp has integrated on-chip*, next to the processor 'core' - this goes for the Z80A derivative, as well as for the LH.
I've called what they have packed into this pocketcomputer "no mean feat". If you look at the features, you can say that again:
- 3 microprocessors, two 8-bit main CPUs (one emulating the PC-1500A a.o.) + one 4-bit subprocessor (I/O)
- 3 x 36 kB ROM
- RS-232C I/F
- serial optical I/F, 38.4 kbaud
- analog input (ADC)
- automatic power off with external wake-up from peripheral
- floppy and RAM-disk options
- 60-pin fully programmable system/expansion bus output
- 2 memory module slots
Impressive ? Sure ! A joy to work with (as a programmer or a user) ? Not really ... And that's a shame.
PC-1600 has never been able to replace PC-1500A in the market, possibly because it became the victim of its own over-complexity ?
At the time (mid eighties and on) Sharp had already her organizer concept ready, later shared in the PDA concept with Apple (Newton),
and so probably didn't care too much ... (PC-12xx, 14xx, E200, and E500 series thriving)
Cheers
Ray
* a.o. the complete port processor, LH-5811, of PC-1500 in the SC main CPU
Hi Ray,
It could be derived from the Z80, I really cannot tell one way or another.
I used the Z80 a lot in the home 8-bit computer era with plenty of machine code (I had no assembler) but I cannot recall much apart from a few instructions and op-codes that won't seem to leave the brain : )
The embedded 8-bit stuff I encountered later was mostly Motorola based (6805 and 6811 particularly) and a few other manufacturers.
Hi Shabaz,
Further to the Z80 discussion in relation to the Sharp PC-1600: reading the Technical Reference Manual, answers to several questions can be
found: http://pockemul.com/Documents/PC1600/PC1600TechnicalReference.pdf .
First of all, the main CPU, SC-7852, is a Z80A-clone. Second: Sharp specifies LH-5801/3 for what they call the subprocessor; so early production
probably was equipped with the 'old' PC-1500A CPU, which was then later on replaced by an upgraded version, the LH-5803.
After that the LH-58xx series was obviously discontinued, in favour of their SC family of micrprocessors - maybe to improve Z80(A)-compatibility.
The best - most comprehensive yet concise - overview: https://sharppocketcomputers.com/index.htm#basic . As an aside: It is remarkable that
after the 4-bit SC dual processor in Sharp's first pocketcomputer, the PC-121x had been succeeded by the 8-bit LHs, 4-bit SC-processors were
used again in later models.
Where the master-slave operation in the PC-1211 worked flawlessly, cooperation between the SC-Z80A and the LH-subprocessor more often than
not led to system instability, up to complete crashes.
The main disappointment with the PC-1600 however was its substandard (for Sharp at least !) LCD. Cramming this 4 times bigger display plus an
extra full size PCB, etc. into the same case as the PC-1500 however, is of course no mean feat ...
Maybe taking a glance at mnemonics and opcodes in the PC-1600 Tech Ref Manual can bring our decission nearer as to the LH-5801 was a Z80
derivative, or not. Memory allocation of the SC-Z80 surely differs considerably from that of the LH-5801, yet addressing range is equal (512 kB),
thanks to the flipflop registers in the LH; the SC seems having to do a lot of bank switching in large applications ...
Cheers
Ray
Hi Shabaz,
Very interesting musings about Z80 and possible 'mimicry' ... And thank you for the literature suggestions.
I believe having gotten some idea of Sharp policy in the dozen or so years I've made a living out of their products in many applications.
Do share your viewpoint that a lot of Japanese manufacturers of the time had more than enough innovation capability of their own, in order
not having to rely on copying; they did however clever- and selectively enter into strategic alliances and joint ventures.
I was appalled to learn that the company was recently taken over by Foxconn, of all the lousy manufacturers of today ...
The Japanese goverment should be ashamed for not having done anything to prevent this - the company that produced the unique amber
EL-displays for the Space Shuttle and where Philips had to buy all their LCD patents !
Back to the good ol' eighties and Sharp policy: I still feel the only explanation that makes sense for the model number, (LH-)5801, is as follows.
Next to their OEM production of Z80 clones - LH080, etc. - they wanted a proprietary microprocessor design for their indeed innovative line of
pocket computers. However they did not want to isolate these products too much from the brands and models that had become well-known
market leaders, in order to reach the broadest possible acceptance. So they devised the number 5800, with a wink to the 6800; but in order
to prevent the impression that they would suggest to make a predecessor, or down-graded version, they made the number their own by changing
it into 5801. Speculative ? Sure, but have I "entered into the realms of phantasy" ?
There was btw a LH-5803, which was meant to emulate the 1500 in its successor, the PC-1600 in order to attain full SW-compatibility. (It didn't
work 100% - much like my XP Pro overlay on Windows 10; this was probably also the reason for the PC-1600 being a less stable system than the trustworthy 1500).
Cheers
Ray
Hi COMPACT,
Sorry for my late response.
Thanks for your friendly reply, and for sharing your broad knowledge to fill-in some of the white spots in mine.
Further to the Nestlé project (and risking being thrown out by the moderator on account of wandering too much off topic ...): the 'poor'
PC-1500A had to communicate with 68000 processors in the Swiss units. When the info required to tackel this problem didn't come in time
to meet the project deadline, I decided to try and overcome the speed differences ... in BASIC (call me crazy). The only solution to get around
a formal handshake was applying probability calculation. It worked fine and reliable.
Reading the history of the Z80, it seems safe tot conclude that Sharp must have been (one of) the very first (1980/81) to produce a CMOS
derivative (?) with many on-chip extras. Just out of curiosity I've once tested the PC-1500A for power consumption (keep in mind that there
was also an I/O controller on board, the LH-5811). Battery life was specified as 300 hrs, i.e. with the usual unrealistic operational limitations.
So after a fortnight of continously running an endlessly repeated program with heavy duty calculations, that made as much use as possible
of display functions, and most of all of the BEEP option, I expected to find my PC-1500A 'dying'. But after more than 3 weeks only the LCD
contrast showed some signs of a nearing 'low battery' condition. Unfortunately I had to abort the experiment, simply because I needed the
pocket computer for my programming work.
The first assembler, as far as I know, was made by Rasso von Schlichtegroll, fairly soon after the PC-1500's introduction; later he developped
a successful line of system programs and tools under the RvS brand, eventually commercialized by the Holtkötter publishing firm.
Jumping to the present, recently produced emulators may be the best way to keep the PC-1500(A) alive (and leave curious young users
in awe). As to the limited storing capacity of RAM chips in those days: the LH-5811 has a direct adressing capability of 64 kB - nothing fancy;
but because of the PU and PV flipflop registers, the full addressing range was 512 kB. And would you believe it: in the early eighties a small
third party company, AMS in Germany on the Danish border, managed to pack this huge amount of storage inside the pocket computer !
I'm not sure if/how his maybe conflicted with an eventual RAM module in the bay for external memory ... Later they had their Gold Card
produced in Taiwan for the top models in Sharp's organizer line: 256 kB, while Sharp was still fiddling with 32/64 kB.
Didn't know the TI-84 was Z80-based; always wanted to have one, never got around to it ... The origin of my interest stems from the late
seventies, and was thus calculator-oriented. I could go now into the old AOS vs. RPN debate, but this would be a) off-topic, and b) maybe
not of interest to anybody in this group. Suffice it to say that It is useless to try and grasp Sharp's design concept for its pocket computers
without taking her EL-5100 scientific calculator into account.
Cheers
Ray
Hi Ray,
At around that time, a lot of the handheld devices were getting powerful, so the ultimate decision to use that instead of any other device may have been simply because it was what someone was experienced in.
From the very little production/shop floor experience I have, it was interesting (at the places I worked) to see that the tools used in production were different to what the rest of the organisation were using. In other words, different CAD tools, different procedures, and different hardware. I'm not saying it is ropey, but a lot of stuff is designed to be one-off or very low quantity production.
Regarding the suggestion of Z80 origins made to look like a non-Z80 device, I've no idea. Certainly it won't execute Z80 software without modification and assembly with a different assembler.
Many processors at the time were similar, from a birds-eye view. Even the different processor designs that soon emerged like RISC and SPARC still have instruction sets and registers, and buses.
There was historically plenty of anti-Japanese tech sentiment in the 1980's, when many people thought that Japanese firms were copying or stealing ideas. That idea still exists today. It's unfounded, and likely no more than western firms stealing western ideas from each other. Perhaps that sentiment inspired the suggestion that it looks similar to the Z80 I cannot tell, since I don't know where and when that suggestion originated. The Japanese government encouraged firms to buy rights to patented tech, that was a major policy at the time.
Depending how keen you are to research down that road, there are some books worth reading, they mention names of people who would know better than speculation, of which unfortunately there is a lot of on the Internet. The first is We Were Burning, and the second is Industrial Innovation in Japan. The first is an easier book to read. According to that, Sharp was extremely quick off the block developing calculators, and amongst the first to productize (not invent) CMOS, so it's quite natural they would either license a Z80 design, or design their own chip. Neither of which would be good reasons to fake instruction names to look like a different processor.
Hi Ray,
The Nestlé project sounds fascinating.
You'd expect the LH-5801 to be superior to the Z80 for its designated applications. The designers could pick, choose, optimise and add the features that they wanted.
It is was unlikely that a LH-5801 device needed to have the DRAM memory and 8080 legacy support because it was for low power consumption devices such as battery powered calculators.
Itsinbuilt timer is very handy. The Z80 required the addition of a CTC (Counter Timer Counter) or similar to do this.
There's nothing wrong about creating a CPU that's lacking the Z80's index registers. If fact these index registers can be a pain to use. The Game Boy version of the Z80 is also missing these index registers and look at the quality of the software for that.
If you look at most Z80 code, the IX and IY index registers if used, were seemingly used as a last resort. This is because the Index Register op codes need an 8 bit offset to be specified within the instruction.
It's also interesting to note that Cristophe Gottheimer's assembler for the LH-5801 uses the Z80 JR (jump relative) and mnemonics instead official Bcc (Branch) mnemonics. A clue to the LH-5801's origins perhaps?
One thing people always seem to overlook is that the Z80 limitations were set by the memory device performance limitations of the day. The designers at Zilog even incorporated inbuilt wait state support to handle slower memories and DRAM refresh support.
This this in mind the Zilog designers worked out that they could use a 4-bit accumulator and run it twice for 8 bit results in the time taken for a single memory fetch.
At the time common memory devices were small with 1K * 1 Static and 4K * 1 Dynamic RAMs being the most affordable. The larger and faster ones came years later.
Cheers and welcome to the community.
Very!
Hi Shabaz,
Let me try to recapture the lost part of my post with the Nestlé story first.
I meant to argue that your and COMPACT's reply suggested the LH-5801 had less hardware facilities than the Z80:
- "the PC-1500's CPU only has three registers" (you)
- "a Z80 inspired CPU with the index registers missing " (C)
For me this makes it a bit hard to understand, how a pocket computer with this CPU has been able to achieve such extraordinary results
in numerous high-level applications. Or is this just a matter of clever trickery by the application programmers ?
First of all (as far as I know), other than Z80, LH-5801 had 8-bit (full-width) registers - esp. in the accumulator.
Program counter and stack pointer were even 16 bit.
Secondly some items from the feature list of the Sharp CPU:
- (3) Use of a 6-byte general purpose register. in addition to the accumulator. allows to comprise three pairs of 2-byte date pointers. (misspelling Sharp)
- (12) Reducing program steps by means of 28-kind single step vector subroutine jurnp
If only there were a feature-by-feature or architecture comparison of the two microprocessors ...
Judging from the applications side (remember I lack sufficient knowledge of micoprocessors), I would say, LH-5801 was - maybe inspired by some
standard Z80, 6502, or even 6800 - yet an advanced proprietary design with a remarkable number of on-chip peripheral facilities. Your and COMPACT's
observations concerning family traits, in one way or another, are very interesting and seem to confirm my assumption all along, that LH-5801 was just not
your run-off-the-mill Z80 clone.
As stated before, the Nestlé project utilized a MUX. Later someone else devised real multi-tasking software for the PC-1500A. I suppose that requires
a quite sophisticated interrupt scheme/structure (esp. at a clock rate of only little more than 1 MHz), or can one do this by clever programming via a
high-level language ?
Last but not least: thank you all for a friendly welcome into this community !
Cheers
Ray
Hi Shabaz,
Let me try to recapture the lost part of my post with the Nestlé story first.
I meant to argue that your and COMPACT's reply suggested the LH-5801 had less hardware facilities than the Z80:
- "the PC-1500's CPU only has three registers" (you)
- "a Z80 inspired CPU with the index registers missing " (C)
For me this makes it a bit hard to understand, how a pocket computer with this CPU has been able to achieve such extraordinary results
in numerous high-level applications. Or is this just a matter of clever trickery by the application programmers ?
First of all (as far as I know), other than Z80, LH-5801 had 8-bit (full-width) registers - esp. in the accumulator.
Program counter and stack pointer were even 16 bit.
Secondly some items from the feature list of the Sharp CPU:
- (3) Use of a 6-byte general purpose register. in addition to the accumulator. allows to comprise three pairs of 2-byte date pointers. (misspelling Sharp)
- (12) Reducing program steps by means of 28-kind single step vector subroutine jurnp
If only there were a feature-by-feature or architecture comparison of the two microprocessors ...
Judging from the applications side (remember I lack sufficient knowledge of micoprocessors), I would say, LH-5801 was - maybe inspired by some
standard Z80, 6502, or even 6800 - yet an advanced proprietary design with a remarkable number of on-chip peripheral facilities. Your and COMPACT's
observations concerning family traits, in one way or another, are very interesting and seem to confirm my assumption all along, that LH-5801 was just not
your run-off-the-mill Z80 clone.
As stated before, the Nestlé project utilized a MUX. Later someone else devised real multi-tasking software for the PC-1500A. I suppose that requires
a quite sophisticated interrupt scheme/structure (esp. at a clock rate of only little more than 1 MHz), or can one do this by clever programming via a
high-level language ?
Last but not least: thank you all for a friendly welcome into this community !
Cheers
Ray
(addendum to audio discussion)
It would seem that I was not right after all in stating that various audio debates have become a thing of the past.
(while visiting him, my son pointed this out to me:)
- (as to the objectivists vs. subjectivists debate) a class-D* power amp has been presented at recent Munich High-End Show**,
which is said to be "100% mathematically correct". The following statement, however, is the relevant one in our issue:
"We build what we simulate and simulate what we build. ... We believe that all matters for the sound quality can be measured
although we often have to develop new measurement methods that are indicative of the subjective sound quality. We direct
all R&D efforts on such measurable metrics. If this does not agree with the listening results we improve our objective metrics."
For all interested: https://www.audioxpress.com/news/purifi-audio-promises-to-reduce-distortion-in-speakers-and-amplifiers .
For all not versed in audio who-is-who: the people behind Purifi are leading developpers in their field.
- (as to the being there - at recording - experience) Dr. Edgar Choueiri, professor of applied physics at Princeton University,
has developped a 3D audio processor, enabling the listener to enjoy his records in 3D via a normal stereo set: BACCH SP.
All we can do is hope and pray that MS will leave this alone, to prevent it from suffering the same fate as HDCD ...
Ray
*for all not versed in audio: the D does not stand for digital; class D means switching amps.
**once again: HD Vinyl nowhere to be seen (heard), no news, no nothing - a hoax ... ?
COMPACT wrote:
Take a look at this - I think it is impressive!
Sorry for this late response, COMPACT (seen too many doctors lately) !
Thanks for sharing this fascinating, illustrated time-line through the life and works of one of the key figures in (micro)computer history.
I knew most of the facts and figures, but getting everything presented from the horse's mouth really is something else.
From the many things that caught my eye, let me comment on a few:
- (1965) "The Olivetti Programma 101 ... contained a small computer made of discrete components ... ". However much my admiration for the
development of the IC, I've never been able to commit myself to applying them in my designs, still (since the sixties) preferring hand-picked
discrete components over 'black boxes'. That way I feel full freedom and more in control of things, although I'm aware of the drawbacks; so
call me oldfashioned ...
- (1970) "The layout of the Z80-CPU. Handdrawn by Federico (by two thirds) ... ". "Those were the days !" - no CAD-CAM. Has anybody ever
assessed the error rate in both cases ?
Having written this, I wonder: wouldn't we have been better off here, sticking to your original question and everything directly related, than
wandering off(-topic) to audio nirvana ... ?
Cheers
Ray
The questions you've raised are certainly worthwhile, albeit far from new ...
First of all, there is broad consensus, that audio is the art of reproducing sounds, recorded in one acoustic environment, in an other - usually totally
different. As a (recent) result, room acoustics have become a hot item; with DSP prices coming down, ever more components in the reproduction
chain - both amps and active speakers e.g. - are equipped with some form of electronic adaptation. While this may seem progress, oldtimer audio
buffs (like us ?) probably wonder, what has become of good (?) old tone controls, or - a bit more sophisticated - equalizers ? The 'tilt control' on the
QUAD 34 pre-amp, beloved in the eighties (and not much unlike RIAA equalization, COMPACT), springs to mind. DSP-based room-correction
circuitry is said to spare you fysical adjustments, like COMPACT described; I don't think I'm convinced.
As to equalizers, in the nineties we were allowed one afternoon to 'play' with the famous Cello Audio Palette, originally intended for studio-use, and
the wet dream of many an audiophile. Although we really had a great time at the circular controls of that gem, we had second thoughts afterwards:
had we not in fact been indulging ourselves in 'bettering' recordings of top-notch mastering engineers ? Who did we think we were ?! Our host had
'encoded' the favourite tracks on his discs with the letters of the controls and the corresponding numbers of the scale settings ... (audiot).
Live vs. recorded comparisons were popular in both the UK and USA during the fifties, aiming at answering the question: how close have we come
with HiFi ? It was reported frequently that even highly experienced audiences (regular concert visitors) sometimes had trouble discerning one from
the other. But this only works in the same room, with the speakers exactly positioned, where the instruments/vocalists were before (and everything
else also kept constant, preferably). So there's not much hope of ever bridging the gap from concert hall/studio to listening room ... And "Bringing
the concert hall to your living room" a bluddy (marketing) lie !
The 'being there (present)' experience /illusion is in fact the last frontier in high-end audio. When auditioning a Cello set with Martin Logan CLS,
a much more experienced audiophile commented: "Ah, this is precisely the sort of set that enables you to hear a fly fart on the rear wall of the
recording studio !". That made us think: are we chasing ultra resolution in sound reproduction, or is our real aim musical satisfaction ? It took some
time to cure ourselves of 'audiophilia nervosa', but we have since been enjoying our music via much more down-to-earth equipment.
Stereo is btw. as much an illusion (and this goes as well for 'glued-together-again' digital signal samples, in an attempt to mimic analog sound).
I believe, though, ultimately most people do not care that they are listening to illusions, nor how far off they are from reality - they've simply come
to like them !
I hope you see my point: this kind of discussions is in fact a thing of the past, and when repeated all the same, bound to be ... pointless.
"The whole audiophile experience is subjective."
That was exactly my point, aimed directly at Ray. The problem with subjective interpretation of audio reproduction is
that it is always "in the ear of the beholder".
"and audiophiles are passionate of what constitutes a great sound"
They just can't explain in objective terms what constitutes that great sound. And there is clearly such a thing as being
too passionate. That is one reason why the ear of the beholder is not a good thing.
"The recorded sound may not be technically perfect but it sure does sound crisp and clear."
There are a few acoustic instruments that produce sound that is not crisp and clear, a muted horn is a good
example. Various kinds of distortion are widely used with electronic instruments and some of these also produce
sound that is not crisp and clear. Does a crisp and clear reproduction of these instruments constitute great sound?
It does not represent a faithful reproduction of the instrument's sound in the acoustic environment where it was
made (being there as you previously put it). And to me that faithful reproduction is what constitutes a "great sound".
It's just not possible to do, at least for now, no matter how much technology, subjective audiophile BS, or money
thrown at it.
The whole audiophile experience is subjective.
Our universe conspires to prevent perfect recording and playback and audiophiles are passionate of what constitutes a great sound.
I wish that some Astronauts would set up some speakers and microphones outside the International Space Station to see how well they work.
Here is one audiophile's take on things. Have a listen for 90 seconds.
The Australian company RODE is successful making microphones and associated paraphernalia. The recorded sound may not be technically perfect but it sure does sound crisp and clear.
Their latest offering is a wireless Lavalier microphone transmitter receiver combination for digital cameras. ("Go") which is very convenient.
Sorry but those are easily provable deficiencies in vinyl recordings/turntables.
COMPACTS claim that audiophiles want the sense of being there at the original recording is a classic example of subjective.
How do they have the slightest idea of what the acoustics were at the original recording without actually being there? How
do you objectively reproduce something you've never heard?
I do like your down-to-earth way of enjoying your music, COMPACT !
As audio advisors, we've always aimed at improving someone's music enjoyment for reasonable money. In the age of streaming, and what have you,
it's hard to pin-point that to a fixed amount, but in the nineties we felt, you could not expect the average customer to be willing to spend more than say
$ 5.000 on a decent player, amp, and pair of speakers (cable-mania was not yet wide-spread then). Of course, this statement immediately raises the
question: what is 'decent' ?
Objectively: equipment, apart from reliable and user-friendly, should be free of apparent flaws like hum/hiss, disturbing 'plops', or distortion levels that
were considered acceptable before the seventies. Furthermore limited performance is less of a problem than a lack of balance*.
Subjectively: equipment should raise the enjoyment level of the customer at least to 'content', but we were only really satisfied, when he reported
"having heard details in his music, he had never heard before", "discovering his music anew" - that sort of thing ... (one customer even declared:
"You have enriched my life" - he has become a friend). Best proof of having succeeded in improving matters came from the wife, though. If she made
a spot-on remark while removing the emptied coffee cups, we knew we had hit bull's eye. Why ? Because women just listen without any prejudice,
while men (audiophiles) are busy trying to hear what they have read ... ; sadly, didn't do much for the WAF (Wife Acceptance Factor).
Cheers
Ray
* that is a.o. why 2-way mini-monitors (not the Bose crap !) can be so very satisfying - certainly if they've been designed by Andrew Jones
P.S.: thank you for the Faggin-link, COMPACT - I'll dive into it
Hi COMPACT and Garry,
(Better late than never:) I'm sorry, if I have provoked replies that to me read like a kind of vinyl bashing ... won't go into that, because the
arguments are mostly too well-known to make a discussion in this day and age still worthwhile. I've been used to these arguments in audio
circles, but didn't expect them here, to be honest. And the worn-out objective vs. subjective discussion - culminating in head vs. heart ratings -
better be left alone, too, wouldn't you agree ?
Never mind; I was in fact just closing off some musings with an anecdote, but perhaps it would have been wise to present it with a bit more
context. Here that is yet.
The show was during the vinyl revival in the nineties, and we only had a speaker brand plus hi-grade vinyl at the time - all the rest was borrowed
from friendly colleague-importers. A high-grade CD-player was part of the demo set, but only used on request from our visitors. Btw, we didn't
do analog vs. digital comparisons.
The purpose of the shredded Mona Lisa poster was to show in a (simplified) pictorial manner, what digitizing is in essence. Apart from a good deal
of laughter, we als got recognition by colleagues referring visitors to our demo room. Only Philips was 'not amused' (and that was long before we
demoed the CD Clarifier the next year, thereby proving their slogan - "Perfect for Ever" - wrong; but that's an other story).
I also like to make an other point: as an importer of high-grade audio, I had to audition/listen to numerous gear/sets. With a few exceptions
the equipment was not 'my cup of tea', and I was pretty sure that I wouldn't be able to enjoy my music through it. Most of the time I tried to
imagine however, what enthralled the owner/seller. And by doing so, I often succeeded in 'hearing his point' ...
To prevent allegations that I'm living in the past, and that vinyl is obsolete, let me turn my eyes to the future* for a change: after virgin, HQ, and
Quiet Vinyl, vinyl lovers recently were treated to (the promise of) the Holy Vinyl Grail: HD-Vinyl. Multi millions have been invested in this project
that stems from the country where mr. Adolf H. was born, and that is frequently mixed up with your beloved 'Down Under', COMPACT. At the
risk of being judged too critical this time (and even because the concept is basically on digital), I think it's a mad men's scheme, and am certainly
not alone in that: https://www.analogplanet.com/content/hd-vinyl-exciting-concept-its-last-years-news .
Cheers
Ray
* the commercial product has been announced several times - yet have seen nothing so far ...
Hi COMPACT,
"Like oscilloscopes, sound should be sampled at about 5x or more than the desired maximum bandwidth", COMPACT wrote.
This ex-Tektronix test & calibration engineer couldn't agree more, but ... at the time of development, this was technically way out of reach for the
people working on e.g. the quadrophonic sound registration on vinyl, as well as those working on the Red Book standard.
Nowdays, cartridges with a frequency range of up to 50 kHz are available, serving people who have been convinced that they need super-tweeters
at the other end of their music reproduction chains ...
"And how does one get a speaker to playback perfect square waves?", COMPACT asked.
Peter Walker of QUAD Mfg fame came pretty close; in fact it was his ultimate way of testing (300 Hz) his almost single-handedly developped ESL
(Electrostatic LoudSpeaker; (fifties). Ever auditioned one ? You will never forget the listening experience ! We've also enjoyed Martin Logan's CLS
very much; of the electrodynamic units, Manger and Dynaudio probably have the best pulse responses. With ED speakers one tries to avoid square
waves because reproducing the top part would mean sending DC trough the poor unit(s), which very few would survive eventually. Furthermore,
audio is about reproducing natural sounds, not technical noises*; and music is the most complicated of sounds. Faithfully reproducing it means
getting the rise and fall right - these coïncide with the attaque of the musical instrument played, and the decay of the resulting sound. The most
demanding instrument attaque-wise, in terms of amplifier slew rate, turned out to be the harpsichord (& family), which is easy to understand once
you look at its playing mechanism. The same cousin who introduced me to electronics via his self-built Xtal receiver, made replicas of famous old
European harpsichords, together with his father (my godfather). I quickly grew to like the sound, that many audiophiles loathe. A possible cure might
be listening to the first chords of Bach's Italian Concerto in a harpsichord rendition (as it was meant to be) - it sings so much more that way than on
the piano ! (Try Glenn Gould's fifties recording vs. his almost anemiatic eighties registration by Sony).
(to be continued)
Ray
* I know, that same Peter Walker in an interview made a statement in relation to his ESLs that seems to argue otherwise ...