• Products and Partners
    Products and Partners
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
Member's Forum How to detect 5V?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 632 subscribers
  • Views 3342 views
  • Users 0 members are here
  • zener
  • electronics design
  • led
  • voltage detector
Related

How to detect 5V?

0phoff
0phoff over 10 years ago

Hi everyone,

 

I'm rather new to electronics but would love to be able to work on projects at home! (now I only do electronics at school)

As a first project, I would love to convert an old Power Supply Unit into a power bench!

 

I read that PSU have a line called Power Good, which outputs 5V if the PSU is working correctly. I thought it would be cool to connect an LED to this line, so I could see if everything is OK!

For this I first thought of a simple LED+resistor, but then I figured this would make the LED emit light (less bright) even when there is eg. 3V on the line.

So I was thinking of a simple circuit with a zener diode with a breakdown voltage of 5V, but I'm not sure whether this would work as expected...

Since I pay for the components myself, I wanted to be sure this would work, before buying everything!

 

Can anyone tell me if this idea would work, and if not how to do it otherwise? I've looked on the internet and the main solution I find is with a comparator. I cannot use this because if the PG Line is wrong, I cannot know if the 5V line of the PSU is actually 5V...

What I want is an easy little circuit that has a LED emit light when there is 5V and not emit light when there is no 5V. (doesn't have to be completely exact) As far as I have found, this power good line varies between 0-5V (does not go higher).

 

Thanksfor your help!

 

Schematic of my idea:

image

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    While TINA-TI seems to work nicely on top of wine for Linux users, I also found a different package, Qucs, which runs natively on Linux (at least, Intel/AMD).  This might eventually be a better fit for the SoCs like RPi since it would probably use less resources.  I am looking through their circuit libraries with the tool on Xubuntu:

     

    image

     

    Go here if you are interested (executables and source code): http://qucs.sourceforge.net/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to jc2048

    Although not needed for this project, there is an awesome silabs part that I found recently, called TS9001 (a couple of variants, open drain or usual totem pole type).

    It is adjustable, so needs additional resistors, but has ultra-low current consumption, the kind of thing that could be used to build a rechargeable or primary cell monitor that could be permanently or semi-permanently! connected, it has about 0.6uA typical, 1.3uA worst-case (25 degrees C) current consumption (and a tiny bit more that would be eaten up with the additional resistor circuit) which was awesome.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 10 years ago in reply to Jan Cumps

    That's a neat idea. For a battery monitor, you could alternatively arrange it with a red LED to the supply to indicate that the battery was below the threshold.

     

    One thing to watch is that the output drive isn't as good as you'd get with a microcontroller I/O pin - 5mA max according to the datasheet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jc2048

    For Linux desktop users, just install the wine package first.  Then, you can install and run TINA-TI as if it were a Windows desktop.  Note that I tested on a Xubuntu desktop system.  If I had a RPi Raspbian desktop, I'd try it there too but I am running OpenELEC.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to 0phoff

    If the measure needs to be precise, there are dedicated ICs: 'Supply Voltage Supervisors'. They are 3-pin devices that can directly drive an LED if voltage is above a certain threshold.

     

    For 5 V monitoring, there's the TPS3809I50D (trips at 4.55 V).

     

    The EEVBlog µCurrent uses a 2.64V one of that family as battery monitor:

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • 0phoff
    0 0phoff over 10 years ago in reply to jc2048

    Thanks for the explanation! I really appreciate the effort you put into it!

    Putting a 5V zener was a silly mistake idd! And my electronics profesor would kill me if he had known I forgot Kirchoff haha image

    I'll definitely try out the Spice Simulators. (We actually worked with them at university once, so shouldn't be to hard to master... )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 10 years ago in reply to 0phoff

    "It seems I was over-complicating things in my head!"

    But that's good. It lead to you asking questions, forming a specification for what you wanted to do, and then looking for a means to do it. You are learning to be an engineer.

     

    Your second circuit with the zener wouldn't work as you've drawn it. The zener doesn't allow current to flow until the voltage reaches 5V, so with only 5V as the source it never starts to conduct. If you make the zener about 2V, then you've got 2V for the zener, 2V for the LED and about 1V for the resistor. Current would start to flow when the input got up to 4V, and the brightness would then steadily increase as the voltage went to 5V [the brightness of an LED is proportional to the current].

     

    Here's what it looks like in a simulation with a 2V zener. I've got the input (VG1 - a voltage generator) ramping up from 2.5V to 5V and then back down again. You can see the current (measured by AM1 - an ammeter) which flows through the LED start to increase just below 4V. The peak current you can adjust with the resistor (a lot of LEDS have reasonable brightness at just a few milliamps, so don't feel you have to drive it at 20mA)

     

    image

     

    image

     

     

     

     

    If you think about it for a moment, you'll see that instead of the zener you could use a second LED. (One of the great things about designing is that there are always several ways to do things.) Wouldn't make sense for a commercial design, but a quick fix if the only components you have are LEDs and resistors.

     

    When I said "you've got 2V for the zener, 2V for the LED and about 1V for the resistor," I was informally giving you one of Kirchhoffs laws. If you don't mind a bit of theory, have a look at

    Kirchhoff's circuit laws


    https://en.wikipedia.org/wiki/Kirchhoff%27s_circuit_laws

     

    specifically the voltage law. It looks a bit scary, but really it's just a bit of applied common sense. In English, he's just saying we can't get something for nothing. [Technically, Kirchhoff's voltage law doesn't apply to this circuit because the zener and the LED both have some capacitance that can store energy, but once everything settles, after a fraction of a second, the capacitances are no longer relevant and we can treat it as though Kirchhoff did apply.]

     

    Could I suggest that you get one of the free simulators that are on offer? That way you can learn to design for yourself without having to buy lots of components. But don't just rely on simulation; when you get a circuit that works well in simulation, build it and measure it and you'll learn what the weaknesses of simulation are and how the real world doesn't always conform to the models you are given (Mother Nature is a somewhat contrary old lady at times).

     

    TINA-TI  SPICE-Based Analog Simulation Program
    http://www.ti.com/tool/tina-ti

     

    LTspice IV
    http://www.linear.com/designtools/software/#LTspice

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to 0phoff

    Thank you for feeding back your findings. image

    Let us know how you get on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 0phoff
    0 0phoff over 10 years ago in reply to shabaz

    Yeah I googled around for a bit and it seems to be like you said!

    Getting an old PSU in a few weeks probably so I'll make sure to read the documentation of that specific piece before buying the components! image

    Thanks for your help! It seems I was over-complicating things in my head! image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to 0phoff

    It is a guess, it depends on your power supply (google the part number in case you can find user documentation for it).

    It isn't necessarily 5V, but usually is a voltage, e.g. a 12V supply may output 11V if the power is good, and 0V if the power is bad.

    However, you still need to check the documentation, there is no real standard on this. Also, don't assume that the signal means that

    the output is exactly 5V or 12V or whatever your supply is rated at. It could be out by 1 volt or more. It is a crude "go/no-go" indicator.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>