• Products and Partners
    Products and Partners
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
Member's Forum Best way to regulate electricity
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 631 subscribers
  • Views 706 views
  • Users 0 members are here
  • build the thing
  • leds
  • mysterious box
  • don't blow up the thing
  • voltage regulation
Related

Best way to regulate electricity

malus_lupus
malus_lupus over 8 years ago

I plan to build this sorta complex I guess box or wall. Not really that complex but can be considered that. I was wondering something. This wall will have LEDs on it probably one for the top row and one for the bottom. I would like to have one for each unit but I suspect what is required for one LED is not something I can do for all parts since I probably do not have enough components.

The question is of course what is the best way to regulate voltage to an LED when the input voltage varies from 0-30 volts. I know resistor is out, so too is POTs, the only thing I can think of is a voltage regulator at 5 volts of course. However, I want to make sure, also if I should build a specific circuit and such. Probably need to make or add a heatsink as well right?

Then again if I do this right I could really only need two for all the LEDs on the top row and on the bottom.

If you need an explanation of what I am making it is hard to explain but basically I am making units. Each one has a different object on it per se, a switch, a dp dt reverse polarity switch, pot, headphone jack and such for when I have different things needing different testing. Each unit I would want will have an LED and a knob with a piece of metal attached to it so I can close the circuit when I want. You could say a dirty switch. Easier and cheaper to make one than to keep using switches. The prototype was cardboard to see how to do it and if I can I will use a 3D printer to make the real deal. I know some people like explanations.

I was planning to cross the LED with each unit so when I turn the unit on it lights up so I know it is live. Which is possible to do with two regulators if not just one. I have to add more wires but yeah. The thing is I want to make sure it is just a regulator with a heat sink or should I add things like caps, and resistors for x purposes I know nothing about. The power supply is DC almost forgot. The LEDs from the datasheet which may be slightly inaccurate says 5 volts is sufficient.






  • Sign in to reply
  • Cancel
Parents
  • DAB
    0 DAB over 8 years ago

    Hi Justin,

     

    It all depends upon what you want the LED's to do.

    If you want a constant brightness during the different input voltages, then you want to maintain a constant current with a minimum voltage across the LED.

    If you want a constant voltage across the LED stack, then you can expect to see some difference in brightness.

     

    I would look at voltage/current regulators and/or DC to DC converters to make sure the LED end meets your needs.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • DAB
    0 DAB over 8 years ago

    Hi Justin,

     

    It all depends upon what you want the LED's to do.

    If you want a constant brightness during the different input voltages, then you want to maintain a constant current with a minimum voltage across the LED.

    If you want a constant voltage across the LED stack, then you can expect to see some difference in brightness.

     

    I would look at voltage/current regulators and/or DC to DC converters to make sure the LED end meets your needs.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer