• Products and Partners
    Products and Partners
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
Member's Forum Query re: datasheet values
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 8 answers
  • Subscribers 630 subscribers
  • Views 2423 views
  • Users 0 members are here
Related

Query re: datasheet values

Andrew J
Andrew J over 7 years ago

I do struggle with making sure I understand what a data sheet is telling me so I'm hoping someone can confirm or otherwise explain my understanding of something.  I'm looking at the data sheet for a LTC1624 - http://www.farnell.com/datasheets/1713911.pdf?_ga=2.75130708.790743949.1554834791-441347304.1541859637&_gac=1.136456708.1554891125.EAIaIQobChMI16fD9tLD4QIVz5TtCh3QQglqEAAYAiAAEgKKrvD_BwE

 

The electrical characteristics state that Vfb feedback current is typically 10nA, max 50nA; Vfb feedback voltage is min 1.178v to max 1.20v.

 

I'm trying to analyse a circuit, not dissimilar to that shown as an example application in the data sheet, and have built it up in LTSpice.  When I simulate this, I can see voltage going into the Vfb pin of 1.15v to 1.3v with peaks of 1.8v falling down to 1.3v  (this is a switching regulator at 200Khz).  I can see current at the Vfb pin of 14.75nA with peaks of -130nA and 110nA.  It will swing from 14nA to -130nA to 110nA back to 14nA in a period of 0.02ms. 

 

This can vary significantly with output load (the above is with a 1kohm load and is more extreme with lower resistance.)  If I build the example application in the data sheet the current to the Vfb pin is within the specified range but the voltage is under the minimum level or over the maximum (again, depending upon load.)

 

My assumption would be that my circuit would be a problem but it's confusing because the example application also simulates outside the specifications.  This is when I start to think I'm not interpreting the data sheet information correctly.  Could someone proffer some advice?

 

I've not posted pictures of the circuit or the simulation results because it's more a question of correctly/incorrectly interpret the specifications - obviously I can if it's important/useful enough.

 

Thanks

 

Andrew

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi Andrew,

     

    The voltage at that pin can go beyond 1.178..1.2V (this is a tolerance of the internal reference, not really a range), it's easiest to consider it like an input pin - it's a feedback input. The switching regulator will have spikes, the IC cannot respond (i.e. accept feedback) fast enough to completely remove them from the output (and hence there are spikes at the feedback pin too, since that's seeing a representation of the output voltage divided down).

    The engineer creating the circuit needs to know the datasheet feedback voltage value, so that they can pick the voltage divider values (R1 and R2) so that the Vfb input pin sees 1.178..1.2V when the output is at the desired voltage.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    I think I understand.  So I need to tune the resistor divider values to get that voltage range (and current range?) without too much regard to transient spikes?

     

    thanks,

     

    Andrew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    That's correct regarding the voltage value (The current value indicates what that input pin will take, and so the potential divider must provide that current - that can be done by choosing potential divider resistances such that the current through the potential divider itself is much larger than that to reduce error, but not so great that too much power is wasted. As an example, if the divider ratio was decided to be (say) 1:2 and R1 and R2 were then (say) 10M and 20M respectively that might not be appropriate, but if they were 10k and 20k respectively then that may be more appropriate. But, the datasheet has to be consulted regarding this feedback circuit, often it will suggest what ballpark either R1 or R2 should be in, or there may be an example circuit with values, it's important not to stray too much from that ballpark to prevent instability.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to michaelkellett

    Thanks for taking the time Michael.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 7 years ago in reply to Andrew J

    Reading data sheets is a bit of an art, and all the manufacturers have their own different ways of doing things.

     

    LT define the FB pin current under "Electrical Characteristics" - these are usually things that the part determines.

     

    The absolute maximum is defined for Vfb (-0.3V -> 2.7V) but they don't define current for anything other than Vfb = 1.8V.

     

    We can tell from the block diagram that it is a high impedance input but that's about it.

     

    We can get an idea of where the current comes from, the voltage on the FB pin changes by 30mV in about 1.5us, and the current during this time is about 158nA.

    This is equivalent to a pin to ground capacitance of (I * t)/v = approx 8pF - which seems quite reasonable.

    In your circuit there is a 100pF cap in // with this input so the current into that will be much higher.

     

    When worrying about the MOSFET, the Vgs that will hurt it is the Vgs relative to the source, not the Vgs net on the circuit. You can see this by adding a trace V(Vgs) - V(Vsw), and it doesn't go above 6V.

     

    Good luck with you exploration - that's enough distraction for me today - must get back to the job I'm avoiding image

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    Thanks Jon.  My original purpose wasn't to task someone to "please look at this circuit for me and see that it works", which is why I didn't post it originally (I don't want to be one of those sorts of members.)  I was really trying to clarify what the data sheet was telling me that I couldn't understand - even the LT application looked odd in simulation against the specs in the data sheet.  It's not easy to research that level of specificity (I know, I tried)!  I guess conversations evolve along the way (and I appreciate the help that everyone gives as it does so.)  Hopefully that makes sense.

     

    Look at that lovely, rich LT Spice interface you got going on there!  I use the MacOS version which doesn't have such new-fangled options such as 'copy bitmap to clipboard'  It barely has options at all image

     

    image

     

    I was, at some point in the future, going to blog about my experience/journey with all this, including attaching files so I guess the blog interface is different to the discussions interface.  

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    Thanks Jon.  My original purpose wasn't to task someone to "please look at this circuit for me and see that it works", which is why I didn't post it originally (I don't want to be one of those sorts of members.)  I was really trying to clarify what the data sheet was telling me that I couldn't understand - even the LT application looked odd in simulation against the specs in the data sheet.  It's not easy to research that level of specificity (I know, I tried)!  I guess conversations evolve along the way (and I appreciate the help that everyone gives as it does so.)  Hopefully that makes sense.

     

    Look at that lovely, rich LT Spice interface you got going on there!  I use the MacOS version which doesn't have such new-fangled options such as 'copy bitmap to clipboard'  It barely has options at all image

     

    image

     

    I was, at some point in the future, going to blog about my experience/journey with all this, including attaching files so I guess the blog interface is different to the discussions interface.  

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer