Member's Forum Testing a Mosfet and Schottky in-circuit; Bit more advice
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 31 replies
  • Answers 27 answers
  • Subscribers 630 subscribers
  • Views 8850 views
  • Users 0 members are here
Related

Testing a Mosfet and Schottky in-circuit; Bit more advice

Andrew J
Andrew J over 7 years ago

I presume this is possible with power off, looking for resistance between drain and source?

 

I'm pretty sure I've killed it - resistance is 0.33Ohms between these two pins image  Out of circuit, on a good one, it is > 13MOhms.  Looking at my circuit, I've solder the Schottky Rectifier the wrong way around - cathode to ground imageimageimage  Pretty sure that won't have done the Mosfet any good, it was too hot to touch.  Can't believe I've been so stupid - by good luck, rather than management, the other Schottky I have in the circuit (not shown below) is the right way around.

 

Is there a way of testing the Schottky rectifier in-circuit - I've tried it and the DMM 'beeps' as it detects a normal junction; measures 0.159v and 0.579V depending upon orientation of test leads?  Just to clarify - in the schematic below you can see how the Schottky rectifier should be - however, as I say, it's actually reversed and I don't know if that might affect readings. So, with the COM lead to the cathode and test (red) lead to anode it reads 0.159v; with the COM lead to the anode and test (red) lead to cathode it reads 0.579V.  I can test one out of circuit and I get 0.157V and OL respectively.  I think that indicates it is ok but in circuit it isn't reading as OL: I have to remove it to swap it around in any case so would the advice be to chuck it and use a new one? 

 

I'm really hoping I can get it off with wick and an iron and without damaging the board; ditto the Mosfet. I really don't want to lump out for a rework station.

 

Is there likely to be damage to other components down stream?  Any tips for testing components without removing them from the circuit?

 

This is only part of the circuit but shows the relationship between the Mosfet and Schottky rectifier:

 

image

 

[silently screaming inside]

  • Sign in to reply
  • Cancel
  • jc2048
    0 jc2048 over 7 years ago in reply to Andrew J

    That suggests that you've lost the sense resistor (the current that you'd need in a 10mOhm sense resistor to drop that much voltage would be a ridiculously high figure). Probably not surprising given the dissipation when the MOSFET went - I should have thought of that.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I'm wondering if it's damaged. 

    I see 2.340V on ith/Run and Vin of 27.682V

    I'd verified that Boost is around 5v and measure it at 5.472V

    Those are all values I'd expect to see - ith/Run is close to max and I'd actually expect it to settle at a lower value of around 1.6V based on a LTSpice simulation)

     

    Sense is meant to be > Vin-15V so > 12V or so.  This voltage fluctuates between around 15V and 24V but I have measured it at around 10V which would be out of range. 

     

    SW is -0.0034v; TG is -0.0033v and Vfb is 0.0005V.  It's these values that concern me - the Mosfet isn't going to turn on at that voltage for example!!  TG should be measuring somewhere just under 5.5V given the value of SW.  SW should be swinging up to Vin (I can only measure with a DMM currently but it isn't moving.)  I'm trying to understand how these three pins are driven, specifically TG: if the Mosfet won't turn on, I can't see how the  feedback circuit would operate.  I'm struggling a bit with that as it isn't clear in the datasheet, at least to me.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 7 years ago in reply to Andrew J

    It's good that you see something sensible on the Ith/RUN pin. At least it's doing something and not totally dead.

     

    Do you see voltage on the BOOST pin? Initially, the boost capacitor charges from the internal 5.6V regulator, so you should see about 5V there, even if the switch logic doesn't want to drive the MOSFET. [Once it starts switching, the BOOST pin will ride up and down 5V above the voltage on the SW node.]

     

    Is there any sign of activity on the gate drive? Does it maybe start and then stop?

     

    The MOSFET you've got there isn't ideal. It only gets 5V of gate drive, so definitely needs to be 'logic level' device (or better) if you want to realise anything like the current it is capable of switching, achieve the rDS(on) value, and so on. That part has a max threshold value of 4V. Chances are certain you have a better specimen than that [to give an idea of the possible spread, the datasheet allows them bounds of 2V to 4V, though you'll never see the min and max value in practice], but I don't think it's what they would expect you to be using.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to Andrew J

    Well, on the plus side, I haven't refried the Mosfet!  On the other hand, something isn't working the way it should as it's not turning on - gate voltage is only 0.5V.  U1 is definitely turned on - the ith/run voltage is >1.9V; it's getting power to Vin and Sense.  Back to the datasheet to try and get a better understanding of what that is doing!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I wasn't sure how possible it was to test in-circuit and how skewed the result would be. 

     

    However, having taken both pieces of the board, the Schottky rectifier is reading 0.159Ohms and OL; a known good one is reading 0.157Ohms and OL.  I think that's ok and I put it back on the board in the correct orientation.

     

    The Mosfet is reading 0.33Ohms between drain and source (out of circuit).  A known good one is reading >34MOhms.  So I think the one I removed is dead.  In goes a new one and back to testing.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 7 years ago

    Resistance reading in-circuit is difficult because of paths round through the power and through the ICs [via the protection circuits]. You'll tend to see initially low readings that move because you're charging decoupling capacitors. I don't like doing it because of the possibility of damage to chips [a handheld meter is probably worse than a good bench meter in that respect], but then I tend to be very over-cautious.

     

    Commercially, you'd chuck the components and use new ones (the parts cost is much, much lower than the cost to you of a person messing around with parts that are suspect). Actually, you might well label the board carefully, put it to one side, and move to the next, unused prototype, unless there were good reasons for sticking with the same one.

     

    For a personal project it's different and you may want to experiment a bit. The MOSFET and Schottky are fairly robust. Just because you can't bear to touch it doesn't mean it is dead. The controller is working current mode, monitoring the current through the MOSFET with R2. With the back-to-front Schottky clamping the output, the controller would keep increasing the current through the MOSFET to try and get the voltage up but there would be some limit to that, so the part's dissipation wouldn't necessarily have been enough to destroy it.

     

    So you might try just reworking the Schottky [if the Schottky SMD package is the type with fold-under legs, they're easy to get off even with a standard soldering iron as you can lift one end at a time]. Are you able to substitute a bench supply for the power rail? If so, one approach might be to apply a very low voltage that was under the controllers's lock-out voltage and was safe for the following circuit and see if the MOSFET feeds that to the coil without there being any gate drive.

     

    The feedback arrangement is a bit odd [and, possibly, a bit dangerous]. If you lost the connection to R6 you'd lose the feedback and the converter would ramp up the voltage to try and compensate, so you want to be careful with that depending on where it comes from and what it's supposed to be doing.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to jc2048

    I measured the current of the DMM in diode test mode and it generates 1mA so I thought it may be ok; the out-of-circuit reading for the other direction is OL rather than 0.579V so I may not be out of the woods.  However, doing a bit of reading around, I find that a reading of 0.5v to 0.8v could be expected.  The DMM is also beeping to indicate a normal junction rather than a short-circuit.  I have to take it out anyway so if I do and don’t read OL then I shall chuck it.

     

    I’ll also test the resistance as you say John and see what results.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 7 years ago in reply to jw0752

    image

     

    0.159V doesn't look too unreasonable for a test current of between 1mA and 10mA.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 7 years ago

    Hi Andrew,

     

    Try reading the diode with just a regular Ohm meter. You should see low ohms in one direction and very high ohms in the other. Your  0.579 V sounds a little too high for a schottky and the 0.159 volts sounds way too low. In circuit however can confuse the readings. Out of the circuit you should only get a voltage reading in one direction with the diode test.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to dougw

    I shall whip it and the MOSFET off tomorrow or Saturday and test.  Pretty sure the MOSFET is dead but I have a few more of both.  Vin is from a rectified 60va transformer.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<>