• Products and Partners
    Products and Partners
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
Member's Forum Using a DC-DC Isolator to allow single power input to case?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 40 replies
  • Answers 15 answers
  • Subscribers 630 subscribers
  • Views 7168 views
  • Users 0 members are here
Related

Using a DC-DC Isolator to allow single power input to case?

Andrew J
Andrew J over 6 years ago

I'm working on something where I use an Arduino talking via I2C to a DAC, an ADC and an RTC and I'm provisioning an I2C isolator and a digital isolator (for digital pins) to provide separation between the two.  I'm doing this to prevent blowing up the Arduino if something goes wrong and also just because I want to as part of experimenting/learning.

 

This only works if both power and ground on sides A and B of the isolators are separate from each other.  To complicate matters, if this all works and I encase it then I only want one power cord into the case - something like a 15V wallwart affair.  This would, inevitably, tie grounds together and the isolators won't work: not 'won't work in an isolation' sense, but not work at all - I've tried it!

 

So I'm wondering if I could feed the 15V supply into a 12V regulator and subsequently a 5V regulator for Side B (I need 12V and 5V on that side) and into a 12V DC-DC isolator that outputs 5V for side A which also powers the Arduino. 

 

Something like this Tracopower supply.  When I look at this I see that the Vin ground is connected on Side B, but the Vout -Ve is isolated for Side A so it seems like it would do the trick.  I thought I'd ask here first before committing to spending money to try it out or indeed if there were other ideas.

 

My main criteria are:

5V, 1A output

Clean enough to power an Arduino and 5V vin isolator (I could use a supply with a higher ouput voltage and feed through a 5V regulator)

Only 1 main power input.  If there's no solution that allows for this, I'd do away with the isolation altogether.  In reality it's not really needed.

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    0 Jan Cumps over 6 years ago

    i believe that the two outputs aren't isolated from each other. It's balanced out: Vmin - Common - Vplus.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to Jan Cumps

    Hi Jan,

     

    I believe there were two models listed on the data sheet. One had +/- with a common and the other was just +/- with no common. If I read it correctly both of these options were isolated from the Input ground.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to jw0752

    The way I read the datasheet is that you either have a single supply, or dual with common middle point:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to jw0752

    The way I read the datasheet is that you either have a single supply, or dual with common middle point:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Gough Lui
    0 Gough Lui over 6 years ago in reply to Jan Cumps

    Indeed, I tested both the HVP-70 and Micsig DP10013 in this posting:

    https://goughlui.com/2018/12/16/review-eevblog-hvp-70-70mhz-micsig-dp10013-100mhz-high-voltage-differential-probes/

     

    You do get what you pay for to some extent ... if you need isolation for high-voltage circuit probing, these are good options. But if you're interested in low voltage, then you might want a standard differential probe otherwise the noise might cause problems for your measurement.

     

    As for the original query - yes, many Traco Power modules are isolated, and this is the approach taken by the Infineon Differential Gate Driver demo board as well as the B&K Precision DAS240 Multi-Channel Logger (along with a digital isolator) to provide isolation.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    Andrew J  wrote:

     

    Interestingly, perhaps, Side A SDA was pulling down ok, Side B wasn't.  SCL Side B was following Side A.

    The clock does not have to negotiate, because it always comes from the master.

    It's on the data lines that there may be conflicts that need to be dealt with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    Interestingly, perhaps, Side A SDA was pulling down ok, Side B wasn't.  SCL Side B was following Side A.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Andrew J

    Ah, I see.. got it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    A heads-up that sharing a ground is virtually the same as sharing Vcc. It's a closed circuit: a PSU output is very low impedance.

    for the current, and for any bogus current too, it is as if your power supply is a wire between Vcc and GND.

     

    I may get flack for this abstraction. So be it image.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to shabaz

    I think I have just confused things not actually posting in detail but I thought that would just cloud things in respect to my question!  Obviously mistaken!!

     

    The grounds don't need to be connected, it wasn't a specific requirement.  In an ideal isolated world they wouldn't be.  What I wanted was to try and protect the Arduino, not to have to plug it into a PC to power it, and not to have two input power supplies - a 15V and 5V as drawn on the right in the image in the post above.  I have components that require regulated 5V and regulated 12V and the 12V regulator requires a minimum 15V input.  I can't power Side A from the Arduino once encased because the Arduino needs powering and I don't want to plug it into a PC or 5V wall wart (back to two sockets!)

     

    My first stab at that, because I didn't know any better at the time, was to isolate just the power and signal traces and not to worry about the ground as I drew above.  So the grounds are the same purely from initial expediency - saves some money as galvanic isolation isn't really required.  That doesn't work - the I2C isolator doesn't seem to like it (perhaps just because it's on a breadboard??) - so I need to move to my next idea which is to use a DC/DC isolator.  I can use either the 15V or 12V as input to the DC/DC isolator (12V is its nominal voltage.)  Now in terms of 'saving money' I was using a LM7805 as one of the regulators, which I have to hand.  That doesn't like powering the Arduino with a voltage drop from 12V to 5V - as I expected, gets too hot and goes into thermal shutdown eventually.  Given that I'd need something like the Tracopower 5V switching regulator - the other one on my image - at around £5 - I might as well not worry about saving £10 and just get the DC/DC isolator and get proper isolation.  So my question was really just making sure I was thinking straight, before I spent that £15 to test it out.  I probably provided more information than necessary and just confused everyone.  Still, it's led to another interesting discussion!

     

    image

    (I forgot to draw on the 5V regulator on the right hand side where it is marked 5Vdd - imagine this is a 5V regulator!)  This then allows me to have one plug in the wall, no connection to a PC and drive both the Arduino and power components completely isolated from each other.  Again, I haven't put in all the caps, resistors, diodes etc.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Andrew J

    Hi Andrew,

     

    Why do the grounds on side A and B need to be connected? It seems as if the design could have the side A ground separated and still function. The only isolated supply that would be needed would require a 5V output for the Arduino. I might have misunderstood.

    Also, to simplify the power, could a 12V supply be used (not 15V) and then a 12V-to-5V isolated supply could be used?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to shabaz

    Given this is on a breadboard at the moment there's likely to be some noise.

     

    Side A: Arduino providing I2C comms to the isolator.  On this side is also power to an encoder and power button.

    Side B: I2C comms to DAC, ADC and RTC.  There's also a 5040 voltage ref.

     

    Here's a pic (I missed out pullup resistors, caps, bypass and reverse voltage diodes etc to avoid cluttering):

    image

    (NOTE: on the image above, I've shown Vin and GND to the Arduino which would be the case when not connected to the PC during testing/development.  When I was trying this on the breadboard, the Arduino was powered over USB from my PC)

     

    What I have above doesn't isolate at GND - but avoids having two power inputs (what I have drawn on the right) and I thought it might be 'good enough' if I tied the grounds under the trace to the left-hand 5V regulator.  As I mentioned I don't NEED isolation I was just doing it out of interest as much as anything.  I know Jan/Peter did this with their DC load to prevent any high voltage/current damaging the USB port of the connected computer.  They can provide complete isolation on both sides because one is powered by USB and one by a 12V supply; these can be bridged if the MCU isn't connected so both sides are powered by the 12V supply.  I absolutely didn't want to drive this with two separate power supplies either from a PC or, say, a 5V wall wart on top of the 15V wall wart and the Arduino is always connected.

     

    With the above setup (Arduino powered from USB), when probing the SCL line on the isolator Side B it was rising to +5V/falling to 0V as expected; however the SDA line on Side B was rising to +5V and was only pulling down a few hundred mV below 5V and in a very, very non-square wave form, with very occasional pull downs to 0V.  Trying different pullup resistors had only a minor impact on this.  When I did away with the Side A 5V regulator and took Side A 5V and GND from the Arduino, it all worked fine.

     

    So, my first 'good enough' stab at this won't work but if I swap the 5V reg on Side A for the DC/DC isolator it seems like it should achieve what I want.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Andrew J

    Hi Andrew,

     

    I just read your comment, and noticed this in the datasheet for that isolator:

    Due to the special logic levels, noise margins can be as low as 50 mV

    I don't know if that is relevant in your project, but maybe there is some power related issue that is making the communications marginal.  Anyway I didn't understand the entire requirement, regarding A and B supplies and what things are connected to them, and the reason for the common ground.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    Andrew J  wrote:

     

    ... The isolator I have is a Silicon Labs SI8602AB-B-IS and it definitely doesn't work when ground is shared ...

    They document the same as what I experienced in my test situation - and what Shabaz explained : ground levels lifted in certain scenarios.

    image

     

    I don't think this is the issue you have, but i think this is an interesting aspect that gives a peek inside the IC's implementation.