• Products and Partners
    Products and Partners
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
Member's Forum Using a DC-DC Isolator to allow single power input to case?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 40 replies
  • Answers 15 answers
  • Subscribers 630 subscribers
  • Views 7158 views
  • Users 0 members are here
Related

Using a DC-DC Isolator to allow single power input to case?

Andrew J
Andrew J over 6 years ago

I'm working on something where I use an Arduino talking via I2C to a DAC, an ADC and an RTC and I'm provisioning an I2C isolator and a digital isolator (for digital pins) to provide separation between the two.  I'm doing this to prevent blowing up the Arduino if something goes wrong and also just because I want to as part of experimenting/learning.

 

This only works if both power and ground on sides A and B of the isolators are separate from each other.  To complicate matters, if this all works and I encase it then I only want one power cord into the case - something like a 15V wallwart affair.  This would, inevitably, tie grounds together and the isolators won't work: not 'won't work in an isolation' sense, but not work at all - I've tried it!

 

So I'm wondering if I could feed the 15V supply into a 12V regulator and subsequently a 5V regulator for Side B (I need 12V and 5V on that side) and into a 12V DC-DC isolator that outputs 5V for side A which also powers the Arduino. 

 

Something like this Tracopower supply.  When I look at this I see that the Vin ground is connected on Side B, but the Vout -Ve is isolated for Side A so it seems like it would do the trick.  I thought I'd ask here first before committing to spending money to try it out or indeed if there were other ideas.

 

My main criteria are:

5V, 1A output

Clean enough to power an Arduino and 5V vin isolator (I could use a supply with a higher ouput voltage and feed through a 5V regulator)

Only 1 main power input.  If there's no solution that allows for this, I'd do away with the isolation altogether.  In reality it's not really needed.

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    0 Jan Cumps over 6 years ago

    i believe that the two outputs aren't isolated from each other. It's balanced out: Vmin - Common - Vplus.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to Jan Cumps

    Hi Jan,

     

    I believe there were two models listed on the data sheet. One had +/- with a common and the other was just +/- with no common. If I read it correctly both of these options were isolated from the Input ground.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to jw0752

    The way I read the datasheet is that you either have a single supply, or dual with common middle point:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 6 years ago in reply to Jan Cumps

    Indeed, I tested both the HVP-70 and Micsig DP10013 in this posting:

    https://goughlui.com/2018/12/16/review-eevblog-hvp-70-70mhz-micsig-dp10013-100mhz-high-voltage-differential-probes/

     

    You do get what you pay for to some extent ... if you need isolation for high-voltage circuit probing, these are good options. But if you're interested in low voltage, then you might want a standard differential probe otherwise the noise might cause problems for your measurement.

     

    As for the original query - yes, many Traco Power modules are isolated, and this is the approach taken by the Infineon Differential Gate Driver demo board as well as the B&K Precision DAS240 Multi-Channel Logger (along with a digital isolator) to provide isolation.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    Andrew J  wrote:

     

    Interestingly, perhaps, Side A SDA was pulling down ok, Side B wasn't.  SCL Side B was following Side A.

    The clock does not have to negotiate, because it always comes from the master.

    It's on the data lines that there may be conflicts that need to be dealt with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    Interestingly, perhaps, Side A SDA was pulling down ok, Side B wasn't.  SCL Side B was following Side A.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    Interestingly, perhaps, Side A SDA was pulling down ok, Side B wasn't.  SCL Side B was following Side A.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    Andrew J  wrote:

     

    Interestingly, perhaps, Side A SDA was pulling down ok, Side B wasn't.  SCL Side B was following Side A.

    The clock does not have to negotiate, because it always comes from the master.

    It's on the data lines that there may be conflicts that need to be dealt with.