• Products and Partners
    Products and Partners
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
Member's Forum Using a DC-DC Isolator to allow single power input to case?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 40 replies
  • Answers 15 answers
  • Subscribers 630 subscribers
  • Views 7183 views
  • Users 0 members are here
Related

Using a DC-DC Isolator to allow single power input to case?

Andrew J
Andrew J over 6 years ago

I'm working on something where I use an Arduino talking via I2C to a DAC, an ADC and an RTC and I'm provisioning an I2C isolator and a digital isolator (for digital pins) to provide separation between the two.  I'm doing this to prevent blowing up the Arduino if something goes wrong and also just because I want to as part of experimenting/learning.

 

This only works if both power and ground on sides A and B of the isolators are separate from each other.  To complicate matters, if this all works and I encase it then I only want one power cord into the case - something like a 15V wallwart affair.  This would, inevitably, tie grounds together and the isolators won't work: not 'won't work in an isolation' sense, but not work at all - I've tried it!

 

So I'm wondering if I could feed the 15V supply into a 12V regulator and subsequently a 5V regulator for Side B (I need 12V and 5V on that side) and into a 12V DC-DC isolator that outputs 5V for side A which also powers the Arduino. 

 

Something like this Tracopower supply.  When I look at this I see that the Vin ground is connected on Side B, but the Vout -Ve is isolated for Side A so it seems like it would do the trick.  I thought I'd ask here first before committing to spending money to try it out or indeed if there were other ideas.

 

My main criteria are:

5V, 1A output

Clean enough to power an Arduino and 5V vin isolator (I could use a supply with a higher ouput voltage and feed through a 5V regulator)

Only 1 main power input.  If there's no solution that allows for this, I'd do away with the isolation altogether.  In reality it's not really needed.

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    0 Jan Cumps over 6 years ago

    i believe that the two outputs aren't isolated from each other. It's balanced out: Vmin - Common - Vplus.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to Jan Cumps

    Hi Jan,

     

    I believe there were two models listed on the data sheet. One had +/- with a common and the other was just +/- with no common. If I read it correctly both of these options were isolated from the Input ground.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to jw0752

    The way I read the datasheet is that you either have a single supply, or dual with common middle point:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 6 years ago in reply to Jan Cumps

    More than a tutorial, it was a sort of online webinar by Jan, very very useful!

    (the draft scheme below is the slide he used to show me, recycled image )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    That's exactly how the SI chip works. 

     

    When I was testing, the probe slipped, bridged two pins and sent a high voltage into the Arduino's analog pins.  Now I'd put test points into the PCB of course

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to shabaz
    I2C isolation methods need to do tricks to detect which side is driving the bus, so slightly different voltage levels are often used for that inside the ICs.

    That was the reference I was looking for. I knew you had commented that before, but couldn't find it back.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Jan Cumps

    Hi Jan,

     

    I didn't fully understand the requirement and the both sides sharing power or ground portion, but for I2C isolation, what you're showing looks good, I think there's no way around it, I2C isolation methods need to do tricks to detect which side is driving the bus, so slightly different voltage levels are often used for that inside the ICs.

    Although I've done logic level translation for I2C using a similar method (just with a non-isolating chip), for isolation I've avoided it (no real reason, just for simpler logic levels), and taken the easier option of SPI parts where isolation is needed, and then the circuitry uses more basic isolator chips that don't need to detect which side is driving. If it had to be I2C then I'd use the same or similar parts as you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J
    I've already blown one £76 instance when I was building my power supply through inadvertent probing.  That's expensive!

     

     

    By coincidence, today, balearicdynamics and I had a chat on preventing this image

     

    image

     

    When I use my scope to measure situations where I want to put the probe reference on a different point than Ground, I use this:

     

     

    image

     

    They aren't cheap - I believe that Gough Lui has found a good cheaper one, if I recall correctly.

    On the other hand, they prevent damage to your scope or device under test when you need to probe without ground reference - or without short-cutting a circuit node to ground if you accidentally put your crocodile clip on a non-ground node.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    I've read through your's and Peter's blogs on powering your DC load and separation multiple times - they're really interesting and what got me interested in trying something similar for myself without just copying what you did.  The isolator I have is a Silicon Labs SI8602AB-B-IS and it definitely doesn't work when ground is shared - once I switched to powering Side A input from the Arduino it worked immediately.  I don't believe I did anything incorrectly when setting up the breadboard: initially, Vin side A was from an LM7805 and Vin side B was from a LM7805 pin-compatible 5V regulator with both having a shared ground. I knew that wasn't the real way forward but it allowed me to get things set up to test: with the LM7805 swapped out it works.  I know that ground potential differences can be an issue - something I also experienced when testing that Renesas MCU in December if you remember (I thought maybe I'd blown my current sense!)

     

    In the interests of not killing myself, I'm not creating anything here that NEEDS isolation in the safety sense, I'm doing it purely for the interest and to save my Arduino - I've already blown one £76 instance when I was building my power supply through inadvertent probing.  That's expensive!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J
    When I put an I2C isolator in between with both sides receiving power independently from two different regulators BUT with a common ground it wouldn't work:  SCL was fine, but SDA just couldn't get pulled low.  Once I switched to powering Side A of the isolator from the Arduino (USB power) with its ground, and Side B from the regulator it all worked ok.  In fairness to me that was what I was expecting but it doesn't hurt to test these things out.

     

    I've used an isolator (TI ISO1541) in a context with and without GND shared (I created a PCB with possibility to break ground). It worked in both cases.

    image

     

    Your scenario makes sense. Powering the left side of the isolated circuit from the adapter, then using that same adapter to power the input of the TRACO.

    The isolated outputs of the traco can then power the right side of your isolated circuit.

     

    Little disclaimer: the Traco's isolation is called "functional isolation". It's not the same as safety isolation.

    It'll do the same but you can't complain to Traco if you die image.

     

     

    edit:

     

    The isolator is sensitive for correct pull-up values. As you can see in my scope trace here, in the light blue trace, there are situations where the SDA low is higher than expected. That's typical in an isolator scenario.

    image

    shabaz, you also have experience with this I believe. Do you have advise for Andrew on using an isolator for i2c with both sides sharing power (or ground) - although that defeats the need of an i2c isolator image ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    That's a kind offer, thanks.  I'm not sure if you can check but this is what I found with breadboard testing.  The Arduino sketch outputs various commands to a DAC over I2C.  Doing so directly to the DAC was fine.  When I put an I2C isolator in between with both sides receiving power independently from two different regulators BUT with a common ground it wouldn't work:  SCL was fine, but SDA just couldn't get pulled low.  Once I switched to powering Side A of the isolator from the Arduino (USB power) with its ground, and Side B from the regulator it all worked ok.  In fairness to me that was what I was expecting but it doesn't hurt to test these things out.

     

    I don't want the Arduino powered from USB in the final version, I need its power to come from the main (single) power supply input to the case which means a shared ground and a problem if I can't separate them.  If you think about your DC load which isolates the power side from the MCU side, you have it set up to power the MCU over USB so you get the isolation you need that way and that's the way you want to run it.  I want my unit to be self-standing - I have created a wi-fi SCPI interface so don't need to plug it into a PC.  The only other way I could think of providing the separation whilst keeping a common input power source was with the DC-DC isolator.

     

    If you have a way of reproducing this scenario and testing it let me know and I can give you more info - I do have a schematic but it isn't that far off what you and Peter created for your DC load.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    If you need single output, you're good. The output is isolated.

     

    If you want me to pre-check something, I have one of the same family;

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    I Just need single output.  The important thing is being able to seperate grounds on both sides of the isolator in order for them to work.  So with this DC DC isolator, Vin can share ground with Side B, but Vout has to be isolated - that seemed to me what I was reading in regards to single output but I did want to check as I’ve never used one of these components before.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    I Just need single output.  The important thing is being able to seperate grounds on both sides of the isolator in order for them to work.  So with this DC DC isolator, Vin can share ground with Side B, but Vout has to be isolated - that seemed to me what I was reading in regards to single output but I did want to check as I’ve never used one of these components before.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Gough Lui
    0 Gough Lui over 6 years ago in reply to Jan Cumps

    Indeed, I tested both the HVP-70 and Micsig DP10013 in this posting:

    https://goughlui.com/2018/12/16/review-eevblog-hvp-70-70mhz-micsig-dp10013-100mhz-high-voltage-differential-probes/

     

    You do get what you pay for to some extent ... if you need isolation for high-voltage circuit probing, these are good options. But if you're interested in low voltage, then you might want a standard differential probe otherwise the noise might cause problems for your measurement.

     

    As for the original query - yes, many Traco Power modules are isolated, and this is the approach taken by the Infineon Differential Gate Driver demo board as well as the B&K Precision DAS240 Multi-Channel Logger (along with a digital isolator) to provide isolation.

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    Andrew J  wrote:

     

    Interestingly, perhaps, Side A SDA was pulling down ok, Side B wasn't.  SCL Side B was following Side A.

    The clock does not have to negotiate, because it always comes from the master.

    It's on the data lines that there may be conflicts that need to be dealt with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    Interestingly, perhaps, Side A SDA was pulling down ok, Side B wasn't.  SCL Side B was following Side A.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Andrew J

    Ah, I see.. got it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    A heads-up that sharing a ground is virtually the same as sharing Vcc. It's a closed circuit: a PSU output is very low impedance.

    for the current, and for any bogus current too, it is as if your power supply is a wire between Vcc and GND.

     

    I may get flack for this abstraction. So be it image.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to shabaz

    I think I have just confused things not actually posting in detail but I thought that would just cloud things in respect to my question!  Obviously mistaken!!

     

    The grounds don't need to be connected, it wasn't a specific requirement.  In an ideal isolated world they wouldn't be.  What I wanted was to try and protect the Arduino, not to have to plug it into a PC to power it, and not to have two input power supplies - a 15V and 5V as drawn on the right in the image in the post above.  I have components that require regulated 5V and regulated 12V and the 12V regulator requires a minimum 15V input.  I can't power Side A from the Arduino once encased because the Arduino needs powering and I don't want to plug it into a PC or 5V wall wart (back to two sockets!)

     

    My first stab at that, because I didn't know any better at the time, was to isolate just the power and signal traces and not to worry about the ground as I drew above.  So the grounds are the same purely from initial expediency - saves some money as galvanic isolation isn't really required.  That doesn't work - the I2C isolator doesn't seem to like it (perhaps just because it's on a breadboard??) - so I need to move to my next idea which is to use a DC/DC isolator.  I can use either the 15V or 12V as input to the DC/DC isolator (12V is its nominal voltage.)  Now in terms of 'saving money' I was using a LM7805 as one of the regulators, which I have to hand.  That doesn't like powering the Arduino with a voltage drop from 12V to 5V - as I expected, gets too hot and goes into thermal shutdown eventually.  Given that I'd need something like the Tracopower 5V switching regulator - the other one on my image - at around £5 - I might as well not worry about saving £10 and just get the DC/DC isolator and get proper isolation.  So my question was really just making sure I was thinking straight, before I spent that £15 to test it out.  I probably provided more information than necessary and just confused everyone.  Still, it's led to another interesting discussion!

     

    image

    (I forgot to draw on the 5V regulator on the right hand side where it is marked 5Vdd - imagine this is a 5V regulator!)  This then allows me to have one plug in the wall, no connection to a PC and drive both the Arduino and power components completely isolated from each other.  Again, I haven't put in all the caps, resistors, diodes etc.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Andrew J

    Hi Andrew,

     

    Why do the grounds on side A and B need to be connected? It seems as if the design could have the side A ground separated and still function. The only isolated supply that would be needed would require a 5V output for the Arduino. I might have misunderstood.

    Also, to simplify the power, could a 12V supply be used (not 15V) and then a 12V-to-5V isolated supply could be used?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to shabaz

    Given this is on a breadboard at the moment there's likely to be some noise.

     

    Side A: Arduino providing I2C comms to the isolator.  On this side is also power to an encoder and power button.

    Side B: I2C comms to DAC, ADC and RTC.  There's also a 5040 voltage ref.

     

    Here's a pic (I missed out pullup resistors, caps, bypass and reverse voltage diodes etc to avoid cluttering):

    image

    (NOTE: on the image above, I've shown Vin and GND to the Arduino which would be the case when not connected to the PC during testing/development.  When I was trying this on the breadboard, the Arduino was powered over USB from my PC)

     

    What I have above doesn't isolate at GND - but avoids having two power inputs (what I have drawn on the right) and I thought it might be 'good enough' if I tied the grounds under the trace to the left-hand 5V regulator.  As I mentioned I don't NEED isolation I was just doing it out of interest as much as anything.  I know Jan/Peter did this with their DC load to prevent any high voltage/current damaging the USB port of the connected computer.  They can provide complete isolation on both sides because one is powered by USB and one by a 12V supply; these can be bridged if the MCU isn't connected so both sides are powered by the 12V supply.  I absolutely didn't want to drive this with two separate power supplies either from a PC or, say, a 5V wall wart on top of the 15V wall wart and the Arduino is always connected.

     

    With the above setup (Arduino powered from USB), when probing the SCL line on the isolator Side B it was rising to +5V/falling to 0V as expected; however the SDA line on Side B was rising to +5V and was only pulling down a few hundred mV below 5V and in a very, very non-square wave form, with very occasional pull downs to 0V.  Trying different pullup resistors had only a minor impact on this.  When I did away with the Side A 5V regulator and took Side A 5V and GND from the Arduino, it all worked fine.

     

    So, my first 'good enough' stab at this won't work but if I swap the 5V reg on Side A for the DC/DC isolator it seems like it should achieve what I want.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Andrew J

    Hi Andrew,

     

    I just read your comment, and noticed this in the datasheet for that isolator:

    Due to the special logic levels, noise margins can be as low as 50 mV

    I don't know if that is relevant in your project, but maybe there is some power related issue that is making the communications marginal.  Anyway I didn't understand the entire requirement, regarding A and B supplies and what things are connected to them, and the reason for the common ground.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    Andrew J  wrote:

     

    ... The isolator I have is a Silicon Labs SI8602AB-B-IS and it definitely doesn't work when ground is shared ...

    They document the same as what I experienced in my test situation - and what Shabaz explained : ground levels lifted in certain scenarios.

    image

     

    I don't think this is the issue you have, but i think this is an interesting aspect that gives a peek inside the IC's implementation.