Member's Forum Using a DC-DC Isolator to allow single power input to case?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 40 replies
  • Answers 15 answers
  • Subscribers 630 subscribers
  • Views 6917 views
  • Users 0 members are here
Related

Using a DC-DC Isolator to allow single power input to case?

Andrew J
Andrew J over 6 years ago

I'm working on something where I use an Arduino talking via I2C to a DAC, an ADC and an RTC and I'm provisioning an I2C isolator and a digital isolator (for digital pins) to provide separation between the two.  I'm doing this to prevent blowing up the Arduino if something goes wrong and also just because I want to as part of experimenting/learning.

 

This only works if both power and ground on sides A and B of the isolators are separate from each other.  To complicate matters, if this all works and I encase it then I only want one power cord into the case - something like a 15V wallwart affair.  This would, inevitably, tie grounds together and the isolators won't work: not 'won't work in an isolation' sense, but not work at all - I've tried it!

 

So I'm wondering if I could feed the 15V supply into a 12V regulator and subsequently a 5V regulator for Side B (I need 12V and 5V on that side) and into a 12V DC-DC isolator that outputs 5V for side A which also powers the Arduino. 

 

Something like this Tracopower supply.  When I look at this I see that the Vin ground is connected on Side B, but the Vout -Ve is isolated for Side A so it seems like it would do the trick.  I thought I'd ask here first before committing to spending money to try it out or indeed if there were other ideas.

 

My main criteria are:

5V, 1A output

Clean enough to power an Arduino and 5V vin isolator (I could use a supply with a higher ouput voltage and feed through a 5V regulator)

Only 1 main power input.  If there's no solution that allows for this, I'd do away with the isolation altogether.  In reality it's not really needed.

  • Sign in to reply
  • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J
    When I put an I2C isolator in between with both sides receiving power independently from two different regulators BUT with a common ground it wouldn't work:  SCL was fine, but SDA just couldn't get pulled low.  Once I switched to powering Side A of the isolator from the Arduino (USB power) with its ground, and Side B from the regulator it all worked ok.  In fairness to me that was what I was expecting but it doesn't hurt to test these things out.

     

    I've used an isolator (TI ISO1541) in a context with and without GND shared (I created a PCB with possibility to break ground). It worked in both cases.

    image

     

    Your scenario makes sense. Powering the left side of the isolated circuit from the adapter, then using that same adapter to power the input of the TRACO.

    The isolated outputs of the traco can then power the right side of your isolated circuit.

     

    Little disclaimer: the Traco's isolation is called "functional isolation". It's not the same as safety isolation.

    It'll do the same but you can't complain to Traco if you die image.

     

     

    edit:

     

    The isolator is sensitive for correct pull-up values. As you can see in my scope trace here, in the light blue trace, there are situations where the SDA low is higher than expected. That's typical in an isolator scenario.

    image

    shabaz, you also have experience with this I believe. Do you have advise for Andrew on using an isolator for i2c with both sides sharing power (or ground) - although that defeats the need of an i2c isolator image ?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    That's a kind offer, thanks.  I'm not sure if you can check but this is what I found with breadboard testing.  The Arduino sketch outputs various commands to a DAC over I2C.  Doing so directly to the DAC was fine.  When I put an I2C isolator in between with both sides receiving power independently from two different regulators BUT with a common ground it wouldn't work:  SCL was fine, but SDA just couldn't get pulled low.  Once I switched to powering Side A of the isolator from the Arduino (USB power) with its ground, and Side B from the regulator it all worked ok.  In fairness to me that was what I was expecting but it doesn't hurt to test these things out.

     

    I don't want the Arduino powered from USB in the final version, I need its power to come from the main (single) power supply input to the case which means a shared ground and a problem if I can't separate them.  If you think about your DC load which isolates the power side from the MCU side, you have it set up to power the MCU over USB so you get the isolation you need that way and that's the way you want to run it.  I want my unit to be self-standing - I have created a wi-fi SCPI interface so don't need to plug it into a PC.  The only other way I could think of providing the separation whilst keeping a common input power source was with the DC-DC isolator.

     

    If you have a way of reproducing this scenario and testing it let me know and I can give you more info - I do have a schematic but it isn't that far off what you and Peter created for your DC load.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to Andrew J

    If you need single output, you're good. The output is isolated.

     

    If you want me to pre-check something, I have one of the same family;

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago in reply to Jan Cumps

    I Just need single output.  The important thing is being able to seperate grounds on both sides of the isolator in order for them to work.  So with this DC DC isolator, Vin can share ground with Side B, but Vout has to be isolated - that seemed to me what I was reading in regards to single output but I did want to check as I’ve never used one of these components before.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J over 6 years ago

    Thanks everyone, I just wanted to make sure I was thinking along the right lines.  I’ll check specific details before I acquire any specific model.  I’ve found these Tracopower units pretty good when I’ve used their voltage regulators in the past: for example, in my psu, I use one that is taking 24V down to 5V at around 500mA and it’s efficiency means that it doesn’t get very warm.  I know that’s not quite the same thing here so I’ll make the right calcs first.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to jw0752

    The way I read the datasheet is that you either have a single supply, or dual with common middle point:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to Jan Cumps

    Hi Jan,

     

    I believe there were two models listed on the data sheet. One had +/- with a common and the other was just +/- with no common. If I read it correctly both of these options were isolated from the Input ground.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago

    TEL 5-1211 looks adequate to supply 1A max at 5V with 1500 V of isolation to both output pins.

    It will dissipate over 1 W of thermal power at 1 A output, so it will get pretty warm.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago

    i believe that the two outputs aren't isolated from each other. It's balanced out: Vmin - Common - Vplus.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago

    Hi Andrew,

     

    Yes this is an isolated DC to DC converter and it will provide a voltage that is not common to the input voltage. this should allow you to do what you are talking about though I am not weighing in on that. Many DC to DC converters are not isolated so make sure you get one that is designed to be. These little DC to DC converters are very efficient and very useful. A company called Recom also has a good line of converters.

     

    https://www.newark.com/b/recom-power?ost=recom&rd=recom

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<