• Products and Partners
    Products and Partners
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
Member's Forum How to backup eMMC of the compute module ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 632 subscribers
  • Views 3907 views
  • Users 0 members are here
Related

How to backup eMMC of the compute module ?

e14 Contributor
e14 Contributor over 11 years ago

how to make a image back from the compute module to external usb for backup / restore ?

I can successfully flashing the eMMC but dd command is not working in reverse.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Firstly make sure you have "if=/dev/sd?" where ? is correct letter. No number is needed since you want the two or more partitions, right? You may want to read Instructions for Using the NEW Raspberry Pi Compute Module Development Kit for other ideas.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    I connect the USB thumb drive and use dd comand to backup eMMC in which if=/dev/mmcblk0 of=/dev/sda. This is exactly cloning the whole OS to usb drive. And then I use Win32 Disk Imager to read the usb thumb drive to save a img backup.   Is it the correct way or any other method would be much more convenient ? (like making an image file from bootable floppy)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    I connect the USB thumb drive and use dd comand to backup eMMC in which if=/dev/mmcblk0 of=/dev/sda. This is exactly cloning the whole OS to usb drive. And then I use Win32 Disk Imager to read the usb thumb drive to save a img backup.   Is it the correct way or any other method would be much more convenient ? (like making an image file from bootable floppy)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    The DD command will clone eMMC to USB bit for bit destroying the USB as you have above. Then Win32 utility can take USB and create a file of the same USB into a file name for backup.

    Clem

    PS a short cut would be to set of=/dev/sda1/backup.img to create a file on the USB. But that would be an unloaded version and not able to boot using USB which your original question implied.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer