• Products and Partners
    Products and Partners
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
Member's Forum Heatsink usage
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 630 subscribers
  • Views 4946 views
  • Users 0 members are here
Related

Heatsink usage

Andrew J
Andrew J over 4 years ago

Specifically, this heatsink: Fischer Elektronik LA6/150 12VFischer Elektronik LA6/150 12V.  I'm trying to work out how that might be used so I'm putting it out there to see if anyone has used something like it or have ideas.  From what I can tell, it 'seems' to be used with a removable bottom plate for 'flat' semiconductors but I'm thinking that something like, say, a TO220 package could be attached to the side with a self-tapper.  A bit like they show with their LAM series heatsinks (PDF, sorry for the non-Farnell link!): here they show them with transistors 'clipped' to the side on the K version so I'd assume that on the non-K version, one would just screw it on.  What think you lot?

  • Sign in to reply
  • Cancel
Parents
  • rsjawale24
    rsjawale24 over 4 years ago

    For use with a TO220 package device, the LA6/150 12V heatsink would be an overkill and expensive too. From what I have seen, this type heatsinks are used on SMD ICs like processors or FPGAs. Basically on devices that can get quite hot. If you have multiple TO220 packages for example incase of inverter circuits or any other power electronics circuits, then I think it's feasible to use and yes drilling and hole and screwing the TO220 in the LA6/150 is fine. I have used simple aluminum from the waste material of frames for french windows in my house. They work fine as a heat sink.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 4 years ago in reply to rsjawale24

    I Was more interested in sussing out how that series worked and whether the design intrinsically required the IC to be attached to the bottom 1.2mm plate or not.  Have you used one or, like me, looked at it and thought that devices could be attached to the side: it certainly looks feasible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 4 years ago in reply to rsjawale24

    I Was more interested in sussing out how that series worked and whether the design intrinsically required the IC to be attached to the bottom 1.2mm plate or not.  Have you used one or, like me, looked at it and thought that devices could be attached to the side: it certainly looks feasible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Gough Lui
    Gough Lui over 4 years ago in reply to Andrew J

    I would second the suggestion to have parallel semiconductors. Usually TO-220, I wouldn't want to be doing more than about 50W/package mainly because of the Rjc. You don't want to get anywhere near the maximum junction temperature, as the safe operating area may require cutting dissipation significantly as temperature increases and there is always the risk of a high ambient, declining heatsink efficiency due to dust accumulation ...

     

    There's usually no great downside to having things run cooler than expected ... it should mean longer device lifetimes and some tolerance for accidental overloads.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Andrew J

    If cost is the driver, then michaelkellett 's suggestion is in many cases going to be the way to go.

    For some units (niche products), the price is not the driver. It may be performance, size, or the requirement to use particular power device.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 4 years ago in reply to michaelkellett

    Yes, parallelising is a possibility I thought of.  I'm not sure that would work out cheaper overall though, but as I say, I'm still working on this and it could be an interesting exercise to get that right!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 4 years ago in reply to Andrew J

    Unless the MOSFETs are very very expensive you will do much better to improve the weak link in the chain, ie the Rjmb and the coupling to the heatsink.

     

    Suppose you put 3 MOSFETS in // - now you get 15 + 12 + 18 = 45 above ambient for a total of 80C.

     

    Now you can use a much cheaper 0.5W/C heatsink for 15 + 12 + 45 + 35 = 107.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to shabaz

    shabaz  wrote:

    ..?

    Edit: on the other hand, I wonder if they also sell the same product without the fan attachment, in which case the panel might not be supplied, so that it just radiates vertically out through holes at the top of the chassis.

    The aluminium heatsink and the fans are available separately. Also available in custom sizes, cut to customer specs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 4 years ago in reply to shabaz

    That press release is useful and states the info I was looking for!  Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 4 years ago in reply to michaelkellett

    That's what those square root like symbols refer to is it?  I've not come across those before.  So it's for a DC load which I've rated to 90W and there would be - in the simplest design - a TO-220 MOSFET, a TO-220 sense resistor (say, up to 12.5W) and a TO-220 temperature sensor.  The thermal calculation I've made is, taking to different heatsink ratings:

    imageimage

    Clearly a 0.5C/W heatsink gives me very little wiggle room.  Can I just add here that I'm still working on this and there are other approaches I might take, e.g. parallelising the MOSFET to share the load.  At this point I was interested in the feasibility of keeping things simple so I was looking at what was available, hence the query about this particular heatsink. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to michaelkellett

    Hi Michael,

    The (little) info here also agrees with that: https://www.fischerelektronik.com/en/latest-news/press-releases/2020-fischer-pressemitteilungen/thermally-optimized-holl…     I think from memory my DC load internally has something similar, although they have attached the semiconductors to the sides, which is likely not good but maybe it was practical for the layout. Quite good that there is the panel to make the heatsink independent of the enclosure, so that the circuit can be tested even with the project enclosure lid off, since that would normally cause issues with the fan ducting. 

     

    Edit: on the other hand, I wonder if they also sell the same product without the fan attachment, in which case the panel might not be supplied, so that it just radiates vertically out through holes at the top of the chassis.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 4 years ago in reply to Andrew J

    From the data sheet it seems clear that Fischer expect the devices being cooled to be attached to the bottom (thick) face.

    It's the only face with flatness and roughness specified and the text says:

     

    "semiconductor mounting surface for milled flat"

     

    I would expect the thermal impedance for devices attached to the side to be a lot worse, and to the sliding plate pretty awful and unpredictable.

     

    It isn't a very good shape for TO220 devices.

     

    How much power are you trying to shift from how many devices ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 4 years ago in reply to rsjawale24

    I‘d go from what the datasheet told me in terms of thermal efficiency.  I actually don’t need one that big but it’s smaller companions would be useful for my purpose.  Anyway, it’s one for my options list.