Member's Forum New Here & 1st Problem!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 593 subscribers
  • Views 3752 views
  • Users 0 members are here
  • opamp
  • comparator
  • lm393
Related

New Here & 1st Problem!

Gosling616
Gosling616 over 3 years ago

I am going back to my youth as an electronic engineer to design some stuff. 

I have joined hoping for help. 

This will be the start of a few minor project around building a cockpit for online flying. Basically, Arduino boards loaded with code and game libraries to detect game events. Coding is a new area for me. I’m pre PCs back then

Anyway, my current problem is more descrete. 

With Vcc at 5V and Gnd at 0v, why does my LM393N Op Amp output 0.7v when I/P 1(-) is connected to Gnd and I/P 1(+) is 2.5V by connecting to the middle of 2 x 5kOhm in series across Vcc and Gnd???

I was hoping to get 5V O/P to drive a MOSFET Board for a 12v power control over a magnetic field coil…

  • Sign in to reply
  • Cancel

Top Replies

  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago +5
    Welcome. You will get answers here. There is a lot of knowledgeable people around. The LM393 output is an open collector type. You would need a pull-up resistor to Vcc to get a proper high level. Like…
  • dang74
    dang74 over 3 years ago +3
    The LM393N is a comparator and not an op-amp. Also I think it's output is open collector. Try attaching a 10k pull up resistor to its output. See if you get 5V after that change.
  • colporteur
    colporteur over 3 years ago in reply to Gosling616

    The mosfet module you are using is similar to the one I have selected other than mine has two mosfets for driving.

    image

    I blocked diagram what I think you are trying to accomplish. Can you confirm if this is correct?

    image

    You have in an external input that is low when triggered. You want to use that low to trigger a mosfet driver that requires a high to trigger. Your plan is to accomplish the signal inversion using a comparator.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gosling616
    Gosling616 over 3 years ago in reply to colporteur

    That is correct..  I have applied a 660Ohm pull up resistor as suggested above and it now works.  Clearly the MOSFET board was pulling the O/P voltage down.  660 seems a good compromise

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gosling616
    Gosling616 over 3 years ago in reply to Gosling616

    I tried a 2k and it draws the signal to Hi, but once I connect it to the MOSFET board the signal goes low.  I worked the R Value down to 660Ohm using three x 2k and that works now.  Thanks..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gosling616
    Gosling616 over 3 years ago in reply to Gosling616

    That worked until I attached it to the MOSFET Board.  Settled on 660Ohm.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 over 3 years ago in reply to Gosling616

    Nice.  Happy to see it's working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago in reply to Gosling616

    Cheers. From the results, it sounds like there is a pull-down resistor on that signal on the MOSFET board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<