Products
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
Member's Forum Best device(s) for this cosplay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 627 subscribers
  • Views 3926 views
  • Users 0 members are here
  • cosplay
  • raspberry pi
  • Metroid
  • Samus
Related

Best device(s) for this cosplay

Amethyst
Amethyst over 3 years ago

I'm assuming many of us here are gamers, and I don't have a better clue where I'd put this. I plan to make a Samus cosplay, from Metroid. Not dedicated to one yet, but thinking Varia suit. 

I have honestly been planning this for many years, but funding left me lacking. On that note, I'm thinking of a Patreon or something, but not sure what rewards would be. Off-topic from the site, but feel free to give ideas!

For the main topic, I'd previously planned to use a mini RasPi and maybe a PICAxe, but an restarting my design with a clearer head:  but I fell behind on tech and don't know what's available. Here's the list I'd like to try to include if you have clever ideas to add, I'm all ears!

-An intake and exhaust fan in the helmet, like RasPi mini fans (5v), for temperature and breathing. I plan to fit these in the "ears" of the helmet that the hoses attach to.

-Some kind of screen in the helmet that can tell me information from the board. Looking at battery level, temperature, and possibly proximity sensor information.

I'm not sure how I can implement this though. I was previously thinking of an oLED display in the past, but they were expensive. I'm wondering if it's possible to create a reflection display off the helmet "glass" (acrylic) over the face? I've seen it work on car windshields, but what am I looking for?

-Some kind of "life form" detection I can use, eg infrared or other ideas? I would feed that input into my display.

Arm Blaster:

-Ice Beam using compressed air, unless there's a good electronic alternative? 

-Ping pong or Airsoft pellets. Which would be cheaper to build? Doesn't need to be high pressure, of course. 

-Fireballs by flash paper and cotton with a glow plug. Suggestions on safest way to control it? Not sure I want a 12v stepper in my arm cannon, not sure if a lower voltage would do the job?

Overall, what electronics do you think are the best ideas to try for something like this that's generally low power, but collectively can be demanding?

The suit is planned to be built with overlapping panels, eg outer thigh strapping over inner thigh armor. I will probably hot glue the wires on the outside of the lower layers and use connectors for LED wiring and any possible sensors I may use (eg motion sensor for behind me). Looking for what your experience is on best budget connectors for that.

image

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 3 years ago

    I have no idea what this thread is about.. but I'm alright with that!

    I saw some mention of projectors.. I picked up this thing, it was so cheap. It's very likely LCD-based, not DLP at this price.

    image

    I wasn't expecting much, just something fun for kids to play with. However, it's a bit stinky (literally) in that it gets hot and smells!

    I would like to open it but it is either glued shut, or is very tightly clipped together.

    The image quality was better than expected! It doesn't work with all HDMI sources (maybe I need to set the source resolution) but this was from my Samsung phone's USB-C-to-HDMI connection, playing a video:

    image

    That was taken with the projector about 2.5 or 3 meters away from a slightly tinted wall. not quite white, and with room lights off since obviously it cannot output a lot of light. The image was slightly larger than the camera took (I had a portrait lens).

    I wouldn't leave this thing on unattended or near clothing.. there's an excellent chance it would catch fire... or burst if one chooses the Lithium-Polymer powered version. 

    In summary it is just an (unsafe) toy, but nevertheless image quality is better than what I had expected.. about as watchable as an old standard-definition TV.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Amethyst
    Amethyst over 3 years ago in reply to shabaz

    Thanks for trying to help! Thing is, I'm looking for a small one that I can fit into a helmet, to create a HUD, potentially by a "pepper's ghost" type of effect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to Amethyst

    This looks a fairly low cost way but may be tricky to fit it all inside unless you can oversize the helmet.

    https://www.youtube.com/watch?v=omNDLQ4cKnY

    It looks like it uses a convex mirror creating a virtual focus point somewhere outside of the helmet. You might want to try a quick test to see how close you can comfortably focus.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 3 years ago in reply to Amethyst

    This looks a fairly low cost way but may be tricky to fit it all inside unless you can oversize the helmet.

    https://www.youtube.com/watch?v=omNDLQ4cKnY

    It looks like it uses a convex mirror creating a virtual focus point somewhere outside of the helmet. You might want to try a quick test to see how close you can comfortably focus.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • beacon_dave
    beacon_dave over 3 years ago in reply to Amethyst

    It looks like a car HUD is very similar to that DIY hololens, just that it is upside down and uses an extra fold mirror to make it more compact for the dashboard.

    image

    https://www.youtube.com/watch?v=KCYEbvby-sg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to Amethyst
    Amethyst said:
    The helmet is a bit big in its own right.

    This could be used to your advantage. It just depends how big you are happy with going.

    I think we perhaps need to see some example pictures of the helmet that you are aiming towards, from different angles, to see what space there is to potentially work with to come up with suggestions.

    The DIY hololens looks like it would give you the most flexibility as to what can be displayed, however as it is inside the helmet, most people will never get to see that aspect when viewed from the outside, so you could be spending a lot of time on something that isn't actually visible. However, equally, if it helps you move and react to your environment, then it may pay off in other ways.

    Also it will depend on how important is is for people to be able to see your eyes from the outside through the visor as you have to have the 45degree mirror for the Pepper's Ghost effect to work. Some pictures show the character's eyes quite visible behind the visor, others just show the green visor without the eyes. 

    Image brightness may be an issue, so you might need to use a high brightness display screen to see it when augmenting the view outside.

    Amethyst said:
    My planned thought was to have at least one fan, in the separated left ear bubble

    I think you will have a lot more flexibility with fan placement than with the display, so if you really want the DIY hololens then that will likely have to be positioned first, then other stuff worked around it. Fans come in all sorts of shapes and sizes and airflow can be ducted as well.

    The DIY hololens will likely have three main requirements. The vertical display screen, the upper 45degree mirror/lens, and the lower 45degree transparent reflection screen that you will look through which will need to be at eye level. 

    You may be able to place the display screen horizontally and place a lens below it then flip the image on the display. This would potentially reduce the overall height. A bit more like a teleprompter setup for a video camera. However you need the lens to create the virtual image far enough in front of your eyes to be able to focus on it.

    I think you will need to spend some time having a bit of play with this aspect. Perhaps replicate the DIY hololens in the video to start with to see what it looks like for real and see if the image is bright enough. Then play around with the angles to see if you can come up with something that will work better with the helmet shape.

    Amethyst said:
    I don't have a 3D printer. I'm still figuring out best way to mount things for angles for trying.

    I think you could do a mock-up of the DIY hololens using 'foamcore' artboard (thin polystyrene sheet with card either side). It's easy to cut / shape with a knife and can be glued or taped together to try stuff out.

    You can also use wire / wire mesh / modelling clay / paper mache / balsa wood etc to create basic support structures. Check out what is cheap in craft shops.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Amethyst
    Amethyst over 3 years ago in reply to beacon_dave

    The helmet is a bit big in its own right. But yes, something like this is amazing.  But The space thing, looking at the helmet... do you have any ideas how to try it? My brain is stalling.

    My planned thought was to have at least one fan, in the separated left ear bubble, which pushes air through the hose to the front inside the mask. If I don't use an exhaust in the right side, or maybe in addition to, I can put this. But I'm stalling on if this is the best idea, whether to section off that bubble or not: Eg leave just a hole for the projector?

    I'm making this out of foam to start probably, I don't have a 3D printer. I'm still figuring out best way to mount things for angles for trying.