Products
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
Member's Forum New and Exciting
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 73 replies
  • Subscribers 624 subscribers
  • Views 6693 views
  • Users 0 members are here
  • exciting technology
Related

New and Exciting

dougw
dougw over 2 years ago

What is the most exciting technology you discovered or rediscovered this year?
This is not a question about significant leading edge technologies, it is just about what you currently find exciting.

Are you into VR? Like Meta Quest 3 or Apple Vision Pro
Are you into computers? Like Raspberry Pi 5 or Apple iMac M3
Are you into e-bikes - a massive trend
Are you into Machine Learning? Like Huskylens
Are you into RISK V or FPGAs? Like BeagleV Fire
Are you into AI? Like CHATGPT

Are you into robots and automation? Like commercial drone applications or self-driving cars

Are you into communications technology? Like SDR

Are you into gaming technology? (and games)

Re you into retro electronics? Like vinyl audio or tube amps

Are you into test instrumentation? and setting up a great lab

Are you into software/firmware? Like RTOS or real-time LINUX on microcontrollers

Or all of the above?

What turns your crank these days?

What is on your wish list?

What courses do you need to take?

  • Sign in to reply
  • Cancel
Parents
  • stanto
    stanto over 2 years ago
    dougw said:
    Are you into VR?

    Yeah, I bought a HTC Vive, original, back when bitcoin originally boomed some years ago, and this year since everyone's picking up the Quest 3 I was able to afford a Vive Wireless Adapter second hand, so now I also enjoy VR wireless! (except for a battery bank). It's required a little bit of modification because the adapter overheats! It seems intel and htc originally designed it only to handle the throughput of the original Vive, but with technology moving along as it is, the battery can run it for longer and it can push a higher resolution, so to handle it, it gets very, very hot. 80degC+ and it shuts off. With a bit of 3D printing and an active fan, 30-50degC. It's pretty good, I always preferred the tracking of the Vive ecosystem. I managed to get the Valve Index hand controllers too, which have full hand and digit tracking. I've tried tinkering with the leap motion for hand tracking, but the 'drivers' to get it to work aren't fully there, and most VR interfaces expect you to have buttons on the controllers, where as you don't for your hands.

    dougw said:
    Are you into computers?

    I picked up a couple of Pi 5's, I intend on using the PCIe output to then use a PCIe to PCI adapter and either plug in an old PCI graphics card, maybe a Voodoo 1 for laughs, or a PCI soundcard which no longer has supported drivers on Windows, such as an old Soundblaster Live 5.1 which has a pretty good sound chip on. Something to play with. And the additional one will likely upgrade my PiHole come proxy and DNS server.

    dougw said:
    Are you into AI?

    I went all in and bought a GeForce 4080 with the ethereum I mined on my 3080, then sold off the 3080 and found that hey, I can run stable diffusion pretty well on it! I've also tried to run my own LLM locally, which kinda works, but doesn't entirely in a way that's like OpenAI's ChatGPT, the guides that are available out there kinda suck and it's confusing. I'd frankly like to train my own dataset to use in stable diffusion or an LLM a like but again, there's no real decent tutorials on making the training sets, which is annoying, I'd like to create art from my own styles like some music videos do.

    dougw said:
    Are you into communications technology?

    I ashamedly have a stockpile of SDR like tech that I haven't picked up yet, I have a HAM Radio shield for an Arduino, a HackRF, and a ChipWhisperer, along with some RTL-SDRs that I'd like to make antenna for to receive satellite signals, it's a mixture of not quite having the energy to work with them and not having my HAM Radio license yet, getting it has been quite awkward.

    dougw said:
    Are you into gaming technology?

    I've been having fun with the Steam Deck. I've been learning and having a bit of a hard time reverse engineering the BIOS for it, which is on a winbond flash chip, and decompiling and rebuilding its UEFI BIOS, to mixed success. It's annoying because the BIOS is a proprietary InsydeH2O BIOS and the open source UEFI Tools software doesn't quite support it because it's "too new". Valve Software removed functionality from the BIOS, such as being able to set RAM timings and the GPU and CPU clock frequencies with hidden form browsers that were unlocked, but have now removed from recent BIOS versions, and I'm trying to work out how to put them back in. It's very much a dark black box, and people who have worked out how to work with it gatekeep the information. It's also been fun to benchmark it and analyse its thermals, because it's an 'embedded system' kinda like working with the Pi, it has a very fixed scope for optimisation and getting the most out of it.

    dougw said:
    Re you into retro electronics?

    I recently repaired my Vinyl record player, though I still need to determine why it has intermittent interference that seems to be on every revolution of the turntable. I did at least manage to remove a lot of the noise being produced to have a cleaner signal, and record from it into Audacity using a mixture of USB soundcards, but having to use a battery powered laptop to prevent some kind of ground loop interference. I'm a stickler for audio.

    dougw said:
    What is on your wish list?

    I'd like a decent oscilloscope, along with a small training course on how to use *that oscilloscope*. I want to be able to observe and reverse engineering communications protocols, or be able to replicate them / emulate them on microcontrollers, I'm thinking handshakes that some games consoles do for their games controllers.

    dougw said:
    What courses do you need to take?

    HAM Radio courses, I would probably benefit from some kind of electronics course, but also programming assembly to be able to better decode and understand BIOS/firmware hex dumps.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • stanto
    stanto over 2 years ago
    dougw said:
    Are you into VR?

    Yeah, I bought a HTC Vive, original, back when bitcoin originally boomed some years ago, and this year since everyone's picking up the Quest 3 I was able to afford a Vive Wireless Adapter second hand, so now I also enjoy VR wireless! (except for a battery bank). It's required a little bit of modification because the adapter overheats! It seems intel and htc originally designed it only to handle the throughput of the original Vive, but with technology moving along as it is, the battery can run it for longer and it can push a higher resolution, so to handle it, it gets very, very hot. 80degC+ and it shuts off. With a bit of 3D printing and an active fan, 30-50degC. It's pretty good, I always preferred the tracking of the Vive ecosystem. I managed to get the Valve Index hand controllers too, which have full hand and digit tracking. I've tried tinkering with the leap motion for hand tracking, but the 'drivers' to get it to work aren't fully there, and most VR interfaces expect you to have buttons on the controllers, where as you don't for your hands.

    dougw said:
    Are you into computers?

    I picked up a couple of Pi 5's, I intend on using the PCIe output to then use a PCIe to PCI adapter and either plug in an old PCI graphics card, maybe a Voodoo 1 for laughs, or a PCI soundcard which no longer has supported drivers on Windows, such as an old Soundblaster Live 5.1 which has a pretty good sound chip on. Something to play with. And the additional one will likely upgrade my PiHole come proxy and DNS server.

    dougw said:
    Are you into AI?

    I went all in and bought a GeForce 4080 with the ethereum I mined on my 3080, then sold off the 3080 and found that hey, I can run stable diffusion pretty well on it! I've also tried to run my own LLM locally, which kinda works, but doesn't entirely in a way that's like OpenAI's ChatGPT, the guides that are available out there kinda suck and it's confusing. I'd frankly like to train my own dataset to use in stable diffusion or an LLM a like but again, there's no real decent tutorials on making the training sets, which is annoying, I'd like to create art from my own styles like some music videos do.

    dougw said:
    Are you into communications technology?

    I ashamedly have a stockpile of SDR like tech that I haven't picked up yet, I have a HAM Radio shield for an Arduino, a HackRF, and a ChipWhisperer, along with some RTL-SDRs that I'd like to make antenna for to receive satellite signals, it's a mixture of not quite having the energy to work with them and not having my HAM Radio license yet, getting it has been quite awkward.

    dougw said:
    Are you into gaming technology?

    I've been having fun with the Steam Deck. I've been learning and having a bit of a hard time reverse engineering the BIOS for it, which is on a winbond flash chip, and decompiling and rebuilding its UEFI BIOS, to mixed success. It's annoying because the BIOS is a proprietary InsydeH2O BIOS and the open source UEFI Tools software doesn't quite support it because it's "too new". Valve Software removed functionality from the BIOS, such as being able to set RAM timings and the GPU and CPU clock frequencies with hidden form browsers that were unlocked, but have now removed from recent BIOS versions, and I'm trying to work out how to put them back in. It's very much a dark black box, and people who have worked out how to work with it gatekeep the information. It's also been fun to benchmark it and analyse its thermals, because it's an 'embedded system' kinda like working with the Pi, it has a very fixed scope for optimisation and getting the most out of it.

    dougw said:
    Re you into retro electronics?

    I recently repaired my Vinyl record player, though I still need to determine why it has intermittent interference that seems to be on every revolution of the turntable. I did at least manage to remove a lot of the noise being produced to have a cleaner signal, and record from it into Audacity using a mixture of USB soundcards, but having to use a battery powered laptop to prevent some kind of ground loop interference. I'm a stickler for audio.

    dougw said:
    What is on your wish list?

    I'd like a decent oscilloscope, along with a small training course on how to use *that oscilloscope*. I want to be able to observe and reverse engineering communications protocols, or be able to replicate them / emulate them on microcontrollers, I'm thinking handshakes that some games consoles do for their games controllers.

    dougw said:
    What courses do you need to take?

    HAM Radio courses, I would probably benefit from some kind of electronics course, but also programming assembly to be able to better decode and understand BIOS/firmware hex dumps.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • electronicbiker
    electronicbiker over 2 years ago in reply to stanto

    Re: the interference on the record player - about the only thing I can think of that could do that is the slightly increased load on the motor each time the 'sensor' for the velocity-trip mechanism is moved. This happens once per rev until the music stops and the tone arm moves inwards quickly. At that point the auto-change is kicked into motion. But - while the music is playing, the tone arm is only moving inwards very slowly, the velocity-trip is very light, and there should be no problem with increased load on the motor. Unless...  The trip mechanism needs to be almost frictionless. Any trace of oil in any wrong places may prevent it functioning properly and increase the load on the motor at that point; grease is even worse. This includes the thingummy-jig that goes up the centre of the record-stacking spindle on auto-changers, but that part of the cycle is only invoked at the end of the record. Any earth-loop problem will probably be inaudible at that time above the noise of slipping pulleys, the clanking of levers, the grinding of gears, and the deafening stereo 'thud' as half-a-dozen LP's drop down the spindle, squashing the stylus into the record that has just finished playing, etc....  Sometimes I get carried away... 

    Some kind of earth loop between the motor and the trip mechanism could also be responsible, but why would there be a broken earth lead in that area, let alone an intact one?

    I used a combination of a PC, a Raspberry Pi, and Audacity to add metadata to all the digitised vynyl tracks that I recorded some years before using a semi-professional digital recorder. I find it quite amusing to see all the info scrolling across the display on the car radio while the thin weedy voices try to sing louder than the shellac-induced snaps crackles and pops!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 2 years ago in reply to stanto

    Speaking of oscilloscopes, I see there is now a road test open for the Digilent Analog Discovery 3 kit. I recently purchased a similar type of kit and they are ever so useful. These kits are also a good way to learn without have to spend thousands.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to stanto

    I am curious if VR headsets cause you any discomfort - like dizziness?