Products
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
Member's Forum Feedback Requested: Table of Contents Navigation Menu on RoadTest Reviews / Project Articles / etc.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 626 subscribers
  • Views 5265 views
  • Users 0 members are here
  • roadtest reviews
  • project articles
  • table of contents
  • navigation
Related

Feedback Requested: Table of Contents Navigation Menu on RoadTest Reviews / Project Articles / etc.

cstanton
cstanton over 2 years ago

Hey everyone,

This thread is duplicated in  Feedback Requested: Table of Contents Navigation Menu on RoadTest Reviews / Project Articles / etc. for reach to members, you can comment on either thread and voting in the poll will be reflected in both threads.

I'd like your feedback on the table of contents/navigation menu that we have mainly on RoadTest Reviews, but also on the Project Articles that we have recently introduced for Project14.

From a tablet, laptop or desktop computer, the navigation currently renders like this:

image

It is automatically generated by using header tags in the content, respecting H2 to higher numbers for sub-sections, headings should always go in the order from H1 to a higher number resulting in smaller headings for sub-sections. H1 is usually preferred for the title of the content and is automatically on the page.

The headings are also highlighted in bold when you scroll down the page, and the navigation persists. Though this can cause a couple of issues, such as the navigation taking up screen real-estate, and it also nudges the content over to the side of the page rather than using the full width.

On a mobile phone or narrow device, however, the navigation looks like this:

imageimage

On mobile, the navigation should be 'sticky' and remain at the top of the screen, particularly if you scroll 'far' down or up, and it auto switches to which heading section you're in.

What's the Question?

Should we make the desktop experience the same or similar to mobile? Here are the options:

In this poll, I am using the word 'static' to mean that you can scroll down the page, or up the page, and you can scroll away from it. You will no longer see it when you navigate away by browsing the rest of the content on that page.

I am using the term 'floating' to mean that it stays with you, it 'floats' on top of content, or perhaps next to it, and travels with you when you scroll the page, you do not browse away from it.

I thought I would add a 'bottom of the content, static, but a drop-down' because there are sites such as Guru3D where this is exactly what it's like. Nothing overly fancy, and it doesn't detract from reading the content first, which is mostly what you're hear to do when you land on the page. Here's an example: https://www.guru3d.com/review/xfx-radeon-rx-5700-xt-thicc-iii-ultra-review 

image

Though on their site you then have to scroll for the options, but I like how it shows the sub headings:

image

Let me know by voting and leaving a comment

  • Sign in to reply
  • Cancel
Parents
  • phoenixcomm
    phoenixcomm over 2 years ago

    Ok, I build pages for your desktop, not a mobile phone!

    Things to change the screwed-up publisher and editor. Let's talk about the editor first:

    Like now I just hit a CR which inserts a stupid blank line. Because instead of a <be> it will give you a new line without the empty blank line. this is because it generates a </p></p> WHY???

    The publisher: generates much grief. It does not obey the rules. and most of the time What You See is Not What You Get!!!!!!  Please DUMP this CRUD and use vanilla HTML5 now this includes the use of the <style> </style> tag NOT IN LINE!!!!  In this way I can create classes ie dim.red{ width: 400px; border: 2px;   solid red; } which can be invoked by dim < class="red"> blah, blah. </dim>. You can always not execute lines <link rel="stylesheet" href="mystyle.css">

    the WYSIWYG editor is almost worthless. see previous comment. 

    ~~ Cris H. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phoenixcomm
    phoenixcomm over 2 years ago

    Ok, I build pages for your desktop, not a mobile phone!

    Things to change the screwed-up publisher and editor. Let's talk about the editor first:

    Like now I just hit a CR which inserts a stupid blank line. Because instead of a <be> it will give you a new line without the empty blank line. this is because it generates a </p></p> WHY???

    The publisher: generates much grief. It does not obey the rules. and most of the time What You See is Not What You Get!!!!!!  Please DUMP this CRUD and use vanilla HTML5 now this includes the use of the <style> </style> tag NOT IN LINE!!!!  In this way I can create classes ie dim.red{ width: 400px; border: 2px;   solid red; } which can be invoked by dim < class="red"> blah, blah. </dim>. You can always not execute lines <link rel="stylesheet" href="mystyle.css">

    the WYSIWYG editor is almost worthless. see previous comment. 

    ~~ Cris H. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • electronicbiker
    electronicbiker over 2 years ago in reply to phoenixcomm

    I'm having difficulty understanding why this debate is taking place at all. Most commenters are saying that the text is too small, others say that a great deal of scrolling is required, that the width should be adjustable, etc. It's a classic case of not being able to please everybody all the time, and that's it, end of story. The comments above suggest that many commenters are either happy with what they've been presented with, or just don't care.

    Some simple answers - 1: If the font is too small then get a device with a larger screen or plug in a larger external VDU. 2: If the layout is not to your taste then try a different document covering the same subject. 3: If 2 is not possible then try a different package but this time insist on seeing it in use before buying. 4: If you have trouble with the colours used, try adjusting the colours displayed by your VDU, these asjustments are usually found in 'Settings' or a sub-menu therein.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to phoenixcomm

    Hi phoenixcomm , if we could keep the feedback to the functionality on the topic at the start of the thread that would be appreciated. Thank you.