Member's Forum Feedback Requested: Table of Contents Navigation Menu on RoadTest Reviews / Project Articles / etc.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 591 subscribers
  • Views 4634 views
  • Users 0 members are here
  • roadtest reviews
  • project articles
  • table of contents
  • navigation
Related

Feedback Requested: Table of Contents Navigation Menu on RoadTest Reviews / Project Articles / etc.

cstanton
cstanton over 2 years ago

Hey everyone,

This thread is duplicated in  Feedback Requested: Table of Contents Navigation Menu on RoadTest Reviews / Project Articles / etc. for reach to members, you can comment on either thread and voting in the poll will be reflected in both threads.

I'd like your feedback on the table of contents/navigation menu that we have mainly on RoadTest Reviews, but also on the Project Articles that we have recently introduced for Project14.

From a tablet, laptop or desktop computer, the navigation currently renders like this:

image

It is automatically generated by using header tags in the content, respecting H2 to higher numbers for sub-sections, headings should always go in the order from H1 to a higher number resulting in smaller headings for sub-sections. H1 is usually preferred for the title of the content and is automatically on the page.

The headings are also highlighted in bold when you scroll down the page, and the navigation persists. Though this can cause a couple of issues, such as the navigation taking up screen real-estate, and it also nudges the content over to the side of the page rather than using the full width.

On a mobile phone or narrow device, however, the navigation looks like this:

imageimage

On mobile, the navigation should be 'sticky' and remain at the top of the screen, particularly if you scroll 'far' down or up, and it auto switches to which heading section you're in.

What's the Question?

Should we make the desktop experience the same or similar to mobile? Here are the options:

In this poll, I am using the word 'static' to mean that you can scroll down the page, or up the page, and you can scroll away from it. You will no longer see it when you navigate away by browsing the rest of the content on that page.

I am using the term 'floating' to mean that it stays with you, it 'floats' on top of content, or perhaps next to it, and travels with you when you scroll the page, you do not browse away from it.

I thought I would add a 'bottom of the content, static, but a drop-down' because there are sites such as Guru3D where this is exactly what it's like. Nothing overly fancy, and it doesn't detract from reading the content first, which is mostly what you're hear to do when you land on the page. Here's an example: https://www.guru3d.com/review/xfx-radeon-rx-5700-xt-thicc-iii-ultra-review 

image

Though on their site you then have to scroll for the options, but I like how it shows the sub headings:

image

Let me know by voting and leaving a comment

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 2 years ago +2
    Leave like is on PC screen. No TOC on mobile (even no sticky if possible) - where the widget takes a decent chunk of prime readable text area. I don't know how many have a mobile phone with a screen…
  • michaelkellett
    michaelkellett over 2 years ago +2
    I voted to remove the navigation but (based on the Thermoflagger RoadTest) which looks like this on my screen: Half the screen is wasted with static or semi-static content. I'd lose the right hand…
  • jc2048
    jc2048 over 2 years ago +2
    I voted for "Remove the navigation, tell us why below". A table of contents serves a purpose in a book with hundreds of pages. Particularly in a technical textbook that may not be read in a linear manner…
  • electronicbiker
    electronicbiker over 2 years ago in reply to phoenixcomm

    I'm having difficulty understanding why this debate is taking place at all. Most commenters are saying that the text is too small, others say that a great deal of scrolling is required, that the width should be adjustable, etc. It's a classic case of not being able to please everybody all the time, and that's it, end of story. The comments above suggest that many commenters are either happy with what they've been presented with, or just don't care.

    Some simple answers - 1: If the font is too small then get a device with a larger screen or plug in a larger external VDU. 2: If the layout is not to your taste then try a different document covering the same subject. 3: If 2 is not possible then try a different package but this time insist on seeing it in use before buying. 4: If you have trouble with the colours used, try adjusting the colours displayed by your VDU, these asjustments are usually found in 'Settings' or a sub-menu therein.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<