Member's Forum What're you up to this weekend?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 55 replies
  • Subscribers 628 subscribers
  • Views 4838 views
  • Users 0 members are here
  • weekend plans
Related

What're you up to this weekend?

cstanton
cstanton over 2 years ago

I'm going to tinker with different soundcards I have, USB and PCI to see which is better at storing and playing audio from old vinyl records that I have.

What do/don't you have planned?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 2 years ago

    Not intended for audio, but using audio op-amps!

    I'm trying to build an amplifier  KiCad 8: Working with Circuit Simulations!  for measuring low-voltage signals. Basically a better iteration of Viewing Noise with a Measurement Amplifier benefiting from the mistakes learned. For instance, I found the very low-frequency response not very useful. 10 Hz is ok. 

    I found 100 Hz low-pass filter wasn't that useful. Also, the switchable gain of 100 and 200 isn't that helpful either. A fixed gain of 100 would be fine.

    I don't think BNC are needed, smaller SMA is more convenient. Replacing batteries is annoying, so a rechargeable battery would be better.

     I think I want switchable low-pass filters at 10k, 100k and 1 MHz. And switchable DC or AC input (10 Hz as mentioned).

    Additional ideas welcome. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 2 years ago

    Not intended for audio, but using audio op-amps!

    I'm trying to build an amplifier  KiCad 8: Working with Circuit Simulations!  for measuring low-voltage signals. Basically a better iteration of Viewing Noise with a Measurement Amplifier benefiting from the mistakes learned. For instance, I found the very low-frequency response not very useful. 10 Hz is ok. 

    I found 100 Hz low-pass filter wasn't that useful. Also, the switchable gain of 100 and 200 isn't that helpful either. A fixed gain of 100 would be fine.

    I don't think BNC are needed, smaller SMA is more convenient. Replacing batteries is annoying, so a rechargeable battery would be better.

     I think I want switchable low-pass filters at 10k, 100k and 1 MHz. And switchable DC or AC input (10 Hz as mentioned).

    Additional ideas welcome. 

    • Cancel
    • Vote Up +3 Vote Down