Products
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
Member's Forum AXOR speed control model mcs060
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 626 subscribers
  • Views 653 views
  • Users 0 members are here
Related

AXOR speed control model mcs060

acdc90
acdc90 over 1 year ago

Hello i have been repairing this unit after aluminium swaf got into and died.

https://www.axorindustries.com/en/products/microspeed-mcs-microspeed-plus-mcsplus/

i have not looked for circuits as usualy wont get them 

after replaceing several smd transisters diodes and resisters and caps.

i now have the OK led on and output voltages at 0v,

about to set up with input and output 

when i noticed the voltage on the opamps is rather high and opamps are getting warm  after only minutes

LM393,TLO72,

With total 32v across dual rails   + and - 16v

data sheet says max 36v 

this PCB has on board supply using UC3842 

the output does not change between 24 to 60 v input to board

Has anyone fixed one of these. ?

does anyone have a circuit,     ?

should i be worried about rail voltage ?

  • Sign in to reply
  • Cancel
  • acdc90
    acdc90 over 1 year ago in reply to anniel747

    I set the dual rails only onto a external psu at 15.5v

    + was 80ma 

    - was 100ma

    no obvious shorts around ics 

    i have not put a scope on it yet

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to acdc90
    [deleted]
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • acdc90
    acdc90 over 1 year ago

    at 24v it was only drawing 130ma total.

    if one had a short that would heat up quickly compared to others 

    as yet have not measured on each rail

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bidrohini
    bidrohini over 1 year ago

    Check the current draw on the ±16V rails to see if it's higher than expected. A damaged OPAMP may cause the heating.