Member's Forum What are your Tips for an Organized Workbench? [Ask e14 - Join, Share & Win Competition] - Winner Announcement
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 143 replies
  • Subscribers 628 subscribers
  • Views 16008 views
  • Users 0 members are here
  • competition
  • organisation
  • question of the month
  • give away
  • arduino
  • workbench
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

What are your Tips for an Organized Workbench? [Ask e14 - Join, Share & Win Competition] - Winner Announcement

e14phil
e14phil over 1 year ago

Calling all makers, engineers, and tinkerers! If your workbench is a masterpiece of order or even a chaotic haven with hidden gems of organisation, we want to hear from YOU!
Join the element14 Community today and take part in our latest “Join, Share & Win” challenge.

imageimageimage
Photo Credits: obones michaelkellett Jan Cumps 

Got a Tidy Workbench? Turn Your Organizing Skills into a Prize!

Calling all makers, engineers, and tinkerers! If your workbench is a masterpiece of order or even a chaotic haven with hidden gems of organization, we want to hear from YOU!
Join the element14 Community today and take part in our latest “Join, Share & Win” challenge.

It’s simple:
1. Register (or Login) for FREE
2. Answer this question by adding a reply / commenting:

What are your top tips for keeping your workbench organised?


3. Be in with a chance to WIN!

We’re celebrating the clever tricks, custom setups, and unique habits that help keep your workspace clean and efficient. Whether it’s colour-coded storage, custom tool racks, or a clever labelling system, we want your insight!

Here’s what you could win:

image

Arduino Uno R4 Minima

General Terms
What: Win 1 of 3 Arduino UNO R4 Minima
How: Sign up  or Sign in and Comment your best Workbench Organisation Tips below. 
When: Before September 30th 2025. 
Anything else: Full terms are below, but we must be able to ship to the address in your account. 

Entries close September 30th, 2025, so don’t wait!
Get organised, get inspired, and get rewarded with the element14 Community.


September Competition [Now Closed] 

The judging panel of E14Alice JoRatcliffe and my self have selected our winners in no particular order. 

Please congratulate:

 rsc 

 ipv1 

 kmikemoo 


Alice will be reaching out to you all to get your prizes via Direct message. 

Congratulations, and this months competition begins today! 
What was your biggest project Disaster? [Ask e14 - Join, Share & Win Competition] October 2025 



Terms & Conditions
 imagePDF

  • Cancel
Parents
  • colporteur
    colporteur over 1 year ago

    If you work bench is primarily for electronic builds and repair, my tip would be to start by defining your power requirements. Construct, assemble, install your setup to provide reliable access to all the power types you will need.

    Think about it. You’ll constantly require power. One AC outlet designed to hold two connections but alternating ten connections is a formula for frustration.

    Ensure access to the power is convenient to use. Nothing like continually having to move stuff around to get power only increases frustration. Better yet, let’s drag a few extension cords into the mix.

    The design should include power cables to make connections. Build or buy solid power connection cables. I suggest a three, minimum. People use cables so often that they break. Intermittent cable or repairing the one and only cable while trying to test is a frustration factor times 10.

    Not sure of your power requirement. Sit at a bench and mock up a project or think of repairing something. “I need to plug this into power” typically finds its way into a project. Wouldn’t it be nice if that power were accessible, convenient and reliable?

    image

    The image is a quick connect cable I use for bread boarding power. The 2.5 inch barrel connector comes from a power supply. It can be plugged into devices (no need for wall warts) or plugged into the extension cable that has north & south 2.5mm pins for use on a bread board. The pin arrangement allows the cable to lay flat coming from one end of the board, when plugged into either the north or south power rails on bread board. The set of pins pointing up become a convenient connection point to power other devices from that rail.

    When connect to bread board I secure the pin end it with some electrical tape to ensure it doesn't escape. I have a few of these cables so they tend to stay with a bread board for future use. Got a 2.5 spacing terminal. The pin end fits nicely into the screw terminal also.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • colporteur
    colporteur over 1 year ago

    If you work bench is primarily for electronic builds and repair, my tip would be to start by defining your power requirements. Construct, assemble, install your setup to provide reliable access to all the power types you will need.

    Think about it. You’ll constantly require power. One AC outlet designed to hold two connections but alternating ten connections is a formula for frustration.

    Ensure access to the power is convenient to use. Nothing like continually having to move stuff around to get power only increases frustration. Better yet, let’s drag a few extension cords into the mix.

    The design should include power cables to make connections. Build or buy solid power connection cables. I suggest a three, minimum. People use cables so often that they break. Intermittent cable or repairing the one and only cable while trying to test is a frustration factor times 10.

    Not sure of your power requirement. Sit at a bench and mock up a project or think of repairing something. “I need to plug this into power” typically finds its way into a project. Wouldn’t it be nice if that power were accessible, convenient and reliable?

    image

    The image is a quick connect cable I use for bread boarding power. The 2.5 inch barrel connector comes from a power supply. It can be plugged into devices (no need for wall warts) or plugged into the extension cable that has north & south 2.5mm pins for use on a bread board. The pin arrangement allows the cable to lay flat coming from one end of the board, when plugged into either the north or south power rails on bread board. The set of pins pointing up become a convenient connection point to power other devices from that rail.

    When connect to bread board I secure the pin end it with some electrical tape to ensure it doesn't escape. I have a few of these cables so they tend to stay with a bread board for future use. Got a 2.5 spacing terminal. The pin end fits nicely into the screw terminal also.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to colporteur
    colporteur said:
    to start by defining your power requirements.

    Got that covered Slight smile