• Products and Partners
    Products and Partners
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
Member's Forum NZ Earthquake
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 632 subscribers
  • Views 2892 views
  • Users 0 members are here
Related

NZ Earthquake

mcb1
mcb1 over 9 years ago

Guys/Gals

Just a quick update on the major Earthquake that struck NZ north of Christchurch just after midnight.

 

They have decided that there was two quakes and they are still deciding if it was along the Hope faultline which runs SW to NE and forms the hills that are between the Southern Alps and the east coast.

It would seem that this triggered many others right up the North Island so the effects were felt widespread.

 

 

I'm in Chch and was up at the time. It went on for 2-3 mins which is much longer than the previous ones.

The closest place is Kaikoura and it has caused some damage to houses, but has currently cut the road link that goes up the east coast (State Highway 1), and damaged other roads that could form an alternative route.

 

There was a Tsuanami warning issued, but got downgraded to a coastal warning.

Unfortunately these warnings end up much less than predicted, so if we actually get a real one, then I'm afraid many will ignore it.

 

 

For those that haven't experienced Earthquakes, they can be very disturbing to some people.

There is often little/no warning and while it might be a little bit of shaking at first, you have no idea how long it will last, or if it will get worse.

 

 

NZ sits on the junction of two plates and one is going under the other. The movement is constant, but various bits get stuck and then suddenly release as the stress overcomes the friction.

This release often results in extra loading on another part and triggers an aftershock which can be almost as large.

So far there have been 50 or more aftershocks in and around the area, so you get no rest from them.

GeoNet - Quakes

As you can imagine you lose power, your house gets trashed and you get no rest, so it's quite stressful in the affected are.

 

 

The christchurch event in 2010 had around 14,000 aftershocks varying down to only just detectable without instruments.

So this will last for some days and it may trigger more events.

 

 

 

If you have friends and relatives in NZ, do try to make contact but appreciate that cellphone systems get overloaded and texts are the best way to contact them.

 

 

Cheers

Mark

  • Sign in to reply
  • Cancel
Parents
  • COMPACT
    COMPACT over 9 years ago

    That Paua photo is amazing!

     

    Paua is indigenous black abalone and is sold in NZ "Fush & Chup" shops as deep fried fritters. (Yum! I should pop on over to have some along with some Terakihi.)

    The inside lining of the shells are made into colourful jewellery commonly for Tikis and other souvenirs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to COMPACT

    Correct.

    You win the prize of as many Paua as you can legally collect.

     

    Paua and Crayfish (think Rock Lobster) are a staple fishery source in Kaikoura, and it attracts people from up and down the east coast to pop into the water to collect a feed. Without breeding stck the fishery will die.

    Thankfully the local fisherman have been actively removing them and placing them back on the rocks that are covered at low tide.

     

    This is a delicate operation as they are basically a very large muscle and any nick will kill them.

    They slither along the rocks so dropping them into the water and landing shell side down is also a death sentence.

     

    Along with paua they have also been rescuing fish stuck in pools and the odd crayfish which aren't used to being up on 'land'.

    image

     

    I also found these images taken further up the coast.

    image

       Look closely at the horizontal and vertical displacement where the driveway used to go past the house.!

     

      image image

    You can see that from this point (about 30km north of kaikoura) back toward kaikoura, the land and seabed has risen 2m.

     

      image

    That isn't Helicopter window distortion, it the same piece of displacement.

     

    Credit goes to the photographers and NBR list them on their post.

    https://www.facebook.com/NBROnline/?hc_ref=NEWSFEED

     

    and these guys

    https://www.facebook.com/NelsonMarlboroughRescueHelicopter/

     

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 9 years ago in reply to mcb1

    Wow, that's a huge movement all in one shot.

     

    Bummer for the folks in the first pic that they built their house right over the fault line!

     

    Are you guys doing well? Did you have a lot of fixing and cleanup to do?

     

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 9 years ago in reply to mcb1

    Wow, that's a huge movement all in one shot.

     

    Bummer for the folks in the first pic that they built their house right over the fault line!

     

    Are you guys doing well? Did you have a lot of fixing and cleanup to do?

     

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 9 years ago in reply to ntewinkel

    It's not sand.

    It is a very fine powder like material and sets like concrete.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 9 years ago in reply to mcb1

    Wow, there's a business opportunity there in cleaning up the sand and then selling it for sandboxes image

     

    I think our local engineers were limited by budget. I suspect they may have just duct-taped it to higher ground image

     

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to ntewinkel

    I heard second hand that the seabed shift at Kaikoura was 3m, not the 2m that it appeared.

     

    Liquifaction is the biggest problem with anywhere that might have been created as the result of filling on top of water, swamp or other areas that previously had water.

    In Chch there was something like 500,000 tons of a very fine material (like cement) brought up by the water from underneath.

     

    Sometimes it has a large hole and other times it looks like mini volcanoes.

       Image result for liquefactionimage

     

     

    it's built right beside the river

    During the shaking, the land will try to flatten out, and many properties near rivers, streams or other cuts in the surface tended to migrate that way.

     

    There is a plan that large columns of stone dug many metres down can be used to prevent the surface heading toward the river.

    I'd hope your engineers look at some of these solutions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 9 years ago in reply to mcb1

    The effects here are mild shaking, and little or no actual damage.

    That's good to hear image

     

    I guess it makes sense - we get the occasional quake near Vancouver Island and we barely feel it when it's that same sort of distance.

     

    ...predicted to lift the west coast by 8m

    That's a huge shift! The pictures of the 2 meter shift are already impressive enough.

    We also have ongoing worries about "the big one" (Cascadia Subduction Zone, I think) that's supposed to do some nasty things. Not sure if my island will sink or rise in that case... I might end up with waterfront property if is sinks! image

     

    Lots of discussion about liquefaction here too - I think we are learning from what's happening with you guys in NZ there.

    The theatre here had some seismic upgrades done to deal with the possibility of liquefaction - it's built right beside the river. Lots of sand in this area too.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to ntewinkel

    Are you guys doing well? Did you have a lot of fixing and cleanup to do?

    Where are in Chch, which is about 150km south of Kaikoura.

    The effects here are mild shaking, and little or no actual damage.

    It does trigger emotions in some people that experienced issues in the Chch quakes, as you don't know how big or how long it will last.

     

    Ever since I've been alive they talk about the Alpine Fault (which formed the Southern Alps) going off, and that generates 8.2 - 8.5 quakes and is predicted to lift the west coast by 8m. Hence once you know where they originate, there is some relief... until the next very large aftershock.

     

    There has been some damage due to liquifaction ( Liquefaction information  ) in Wellington as some out it is built on the seabed which rose in the 1829 quake.

    I found this https://koordinates.com/layer/4068-wellington-region-liquefaction-potential/ which shows the potential effects.

     

    Now bear in mind Wellington didn't get hit, it was some distance form the initial quake but closer to the aftershocks and in the line of the faultlines for that area.

     

    Cheers

    Mark