Personal Blogs
  • Community Hub
  • More
Personal Blogs
Andy Clark's Blog Azure Sphere Secure IOT - I2C Compass
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 23 Nov 2018 11:46 PM Date Created
  • Views 4182 views
  • Likes 10 likes
  • Comments 17 comments
  • azure sphere kit
  • azure sphere
  • microsoft
  • iot
  • microsoft azure
Related
Recommended

Azure Sphere Secure IOT - I2C Compass

Workshopshed
Workshopshed
23 Nov 2018

My experiments with U-Center and the GPS module had shown that the direction indication was not very reliable. Following a link in Kevin Saye's post, I discovered a command that should tell the orientation. But my device did not seem to be generating that.

image

http://aprs.gids.nl/nmea/#hdt

 

Reading a bit further, I realised that the compass feature was provided by a  HMC5883HMC5883 connected over I2C on a second connector. So I soldered a green wire onto the SCL connector and a blue wire to the SDA. I did a test with a sample from instructables and an Arduino Uno (using 2x10k resistors pulled up to the 3.3v line) and got some readings from the sensor. Checking the HMC5883 datasheet later 2K2 resistors were recommended so I'll reduce my values if there are any issues.


imageimage

I realised from looking at this code that there is a magnetic deviation for compasses and really my project should compensate for that based on the current position. Perhaps another Azure Function is the best approach for that as it allows for adjustments over time.

 

So a bit of a problem with connecting the I2C to the Azure Sphere, the MS team have yet to support I2C in their SDK. I'd come across chips before that did not support I2C and knew that the protocol could be implemented in software with a technique called “bitbanging” i.e. you toggle a GPIO to have the desired behaviour. AlaskaResearchCubeSat had a great example bitbang I2C which looked straight forward to port.

 

I2C Hardware

As mentioned the MT3620 does support I2C, it has three comms modules that can be configured for UART, SPI or I2C. However this is not yet available via the API so I needed to look at the GPIO. For the board to be able to communicate with I2C it needs to be able send and receive on two pins. I did think about using 4 pins wired in pairs but it does not seem that is necessary.

 

The I2C protocol works by having pull up resistors and each of the devices pulls down the line to signal a zero. The output is left floating when the MCU indicates "high", that means that other devices could pull that line low still. The Azure Sphere seems to support this with the open_drain setting for GPIO_OpenAsOutput.

 

image

It also supports reading the pin whilst in this state so hence we can implement a software/bitbanged I2C.

 

Porting to Azure Sphere

My first pass at porting the Alaska bitbang version is as follows:

 

i2cbb.h

#pragma once


//I2CBus
typedef struct {
GPIO_Id scl;
int sclFd;
GPIO_Id sda;
int sdaFd;
} i2cbus_t;


//Function prototypes
void i2c_bb_setup(i2cbus_t* bus);
short i2c_bb_tx(i2cbus_t* bus, unsigned char addr, const unsigned char *dat, unsigned short len);
short i2c_bb_rx(i2cbus_t* bus, unsigned char addr, unsigned char *dest, unsigned short len);

 

i2cbb.c

#include <applibs/gpio.h>
#include <applibs/log.h>
#include <stdbool.h>
#include <errno.h>
#include <string.h>
#include <time.h>
#include "i2cbb.h"


#define BIT0 1


//setup bit bang I2C pins
void i2c_bb_setup(i2cbus_t* bus) {
    //set pins as outputs opendrain
    bus->sclFd = GPIO_OpenAsOutput(bus->scl, GPIO_OutputMode_OpenDrain, GPIO_Value_High);
    bus->sdaFd = GPIO_OpenAsOutput(bus->sda, GPIO_OutputMode_OpenDrain, GPIO_Value_High);
}


//wait for 1/2 of I2C clock period
void i2c_bb_hc(void) {
    const struct timespec clockhalftime = { 0, 50000 };
    //wait for 0.05ms
    nanosleep(&clockhalftime, NULL);
}


int setSDA(i2cbus_t* bus, GPIO_Value_Type val) {
    int result = GPIO_SetValue(bus->sdaFd, val);
    if (result != 0) {
        Log_Debug("ERROR: Could not set SDA output value: %s (%d).\n", strerror(errno), errno);
        return -1;
    }
    return 0;
}


int setSCL(i2cbus_t* bus, GPIO_Value_Type val) {
    int result = GPIO_SetValue(bus->sclFd, val);
    if (result != 0) {
        Log_Debug("ERROR: Could not set SCL output value: %s (%d).\n", strerror(errno), errno);
        return -1;
    }
    return 0;
}


unsigned char getSDA(i2cbus_t* bus) {
    GPIO_Value_Type val;
    int result = GPIO_GetValue(bus->sdaFd, &val);
    if (result != 0) {
        Log_Debug("ERROR: Could not read SDA value: %s (%d).\n", strerror(errno), errno);
    }
    return val == GPIO_Value_High ? 1 : 0;
}


void i2c_bb_start(i2cbus_t* bus) {
    //wait for 1/2 clock first
    i2c_bb_hc();
    //pull SDA low
    setSDA(bus, GPIO_Value_Low);
    //wait for 1/2 clock for end of start
    i2c_bb_hc();
}


void i2c_bb_stop(i2cbus_t* bus) {
    //pull SDA low
    setSDA(bus, GPIO_Value_Low);
    //wait for 1/2 clock for end of start
    i2c_bb_hc();
    //float SCL
    setSCL(bus, GPIO_Value_High);
    //wait for 1/2 clock
    i2c_bb_hc();
    //float SDA
    setSDA(bus, GPIO_Value_High);
    //wait for 1/2 clock
    i2c_bb_hc();
}


//send value over I2C return 1 if slave ACKed
short i2c_bb_tx_byte(i2cbus_t* bus, unsigned char val) {
    int i;
    //shift out bits
    for (i = 0;i < 8;i++) {
        //pull SCL low
        setSCL(bus, GPIO_Value_Low);
        //check bit
        if (val & 0x80) {
            //float SDA
            setSDA(bus, GPIO_Value_High);
        }
        else {
            //pull SDA low
            setSDA(bus, GPIO_Value_Low);
        }
        //shift
        val <<= 1;
        //wait for 1/2 clock
        i2c_bb_hc();
        //float SCL
        setSCL(bus, GPIO_Value_High);
        //wait for 1/2 clock
        i2c_bb_hc();
    }
    //check ack bit
    //pull SCL low
    setSCL(bus, GPIO_Value_Low);
    //float SDA
    setSDA(bus, GPIO_Value_High);
    //wait for 1/2 clock
    i2c_bb_hc();
    //float SCL
    setSCL(bus, GPIO_Value_High);
    //wait for 1/2 clock
    i2c_bb_hc();
    //sample SDA
    val = getSDA(bus);
    //pull SCL low
    setSCL(bus, GPIO_Value_Low);
    //return sampled value
    return !val;
}
//send value over I2C return 1 if slave ACKed
unsigned char i2c_bb_rx_byte(i2cbus_t* bus, unsigned short ack) {
    unsigned char val;
    int i;
    //shift out bits
    for (i = 0;i < 8;i++) {
        //pull SCL low
        setSCL(bus, GPIO_Value_Low);
        //wait for 1/2 clock
        i2c_bb_hc();
        //float SCL
        setSCL(bus, GPIO_Value_High);
        //wait for 1/2 clock
        i2c_bb_hc();


        //shift value to make room
        val <<= 1;


        //sample data
        unsigned char readbit;
        readbit = getSDA(bus);


        if (readbit == GPIO_Value_High) {
            val |= 1;
        }
    }


    //check ack bit
    //pull SCL low
    setSCL(bus, GPIO_Value_Low);
    //check if we are ACKing this byte
    if (ack) {
        //pull SDA low for ACK
        setSDA(bus, GPIO_Value_Low);
    }
    else {
        //float SDA for NACK
        setSDA(bus, GPIO_Value_High);
    }
    //wait for 1/2 clock
    i2c_bb_hc();
    //float SCL
    setSCL(bus, GPIO_Value_High);
    //wait for 1/2 clock
    i2c_bb_hc();
    //pull SCL low
    setSCL(bus, GPIO_Value_Low);
    //float SDA
    setSDA(bus, GPIO_Value_High);
    //return value
    return val;
}


short i2c_bb_tx(i2cbus_t* bus, unsigned char addr, const unsigned char *dat, unsigned short len) {
    short ack;
    int i;
    //send start
    i2c_bb_start(bus);
    //send address with W bit
    ack = i2c_bb_tx_byte(bus, (addr << 1));
    //send data bytes
    for (i = 0;i < len && ack;i++) {
        //transmit next byte
        ack = i2c_bb_tx_byte(bus, dat[i]);
    }
    //transmit stop
    i2c_bb_stop(bus);
    //return if slave NACKed
    return ack;
}


short i2c_bb_rx(i2cbus_t* bus, unsigned char addr, unsigned char *dest, unsigned short len) {
    int i;
    //send start
    i2c_bb_start(bus);
    //send address with R bit
    if (!i2c_bb_tx_byte(bus, (addr << 1) | BIT0)) {
        //got NACK return error
        return 0;
    }
    //receive data bytes
    for (i = 0;i < len;i++) {
        //receive next byte
        dest[i] = i2c_bb_rx_byte(bus, i == len - 1);
    }
    //transmit stop
    i2c_bb_stop(bus);
    //return if slave NACKed
    return 1;
}


This still needs testing but it does compile, the identification registers seem good candidates for the read testing as they have fixed values. As is common with most I2C devices the "read" register is selected by sending a single byte with no data.

"To move the address pointer to a random register location, first issue a “write” to that register location with no data byte following the command. For example, to move the address pointer to register 10, send 0x3C 0x0A."

image

From Honeywell HMC5883L datasheet.

 

Note that the output is in the form of a vector so that needs converting to a bearing using the X and Y values and Arctan function. The AdaFruit library used by the Instructables article has a good example of that. I'll like wrap the call to the compass up with a separate function so you don't need to see the low level I2C functionality. I quite like the AdaFruit universal sensor approach but that seems a bit overkill to copy here.

 

Unfortunately I've got a work trip coming up next week so there will be a pause in the project. Knowing my luck the SDK team will have enabled the I2C functionality before I've had a chance to finish this port.

 

Further reference

Embedded System I2C Tutorial - Embedded Systems Learning Academy

https://courses.engr.illinois.edu/ece437/fa2018/ref/I2C_Serial_Protocol_Tutorial.pdf

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 7 years ago in reply to Workshopshed +3
    I programmed the Azure Sphere to write to the same configuration registers I'd seen on the arduino sample and managed to get a snapshot. The thing I noticed was that the code was sending a NAK after the…
  • DAB
    DAB over 7 years ago +2
    Nice update. I know how it is when work interferes with fun. DAB
  • Workshopshed
    Workshopshed over 7 years ago in reply to shabaz +2
    Cheers, Shabaz, actually from the desktop, I know that the USB ground is connected to the probe ground on the Picoscope but both devices are coming from the same computer so the ground should be ok...…
Parents
  • Workshopshed
    Workshopshed over 7 years ago

    I tried to use the PicoScope 2204A to decode the I2C protocol but the scope keeps overloading my USB bus. I was hoping that using a powered hub would solve my problems with the picoscope but it appears not, I did manage to get one trace which reflected what I was getting back in my debug window and the address for read and write seemed good but that got lost before I could snapshot it.

     

    So I added some LEDs to the data lines and a push switch from the SDA line to GND. I stepped through the code using the switch to behave as the remote, cross referencing against these two links. And the code does seem to be valid.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 7 years ago

    I tried to use the PicoScope 2204A to decode the I2C protocol but the scope keeps overloading my USB bus. I was hoping that using a powered hub would solve my problems with the picoscope but it appears not, I did manage to get one trace which reflected what I was getting back in my debug window and the address for read and write seemed good but that got lost before I could snapshot it.

     

    So I added some LEDs to the data lines and a push switch from the SDA line to GND. I stepped through the code using the switch to behave as the remote, cross referencing against these two links. And the code does seem to be valid.