Personal Blogs
  • Community Hub
  • More
Personal Blogs
Andy Clark's Blog Dragonboard 410c - OpenCV
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 20 May 2016 10:41 PM Date Created
  • Views 933 views
  • Likes 7 likes
  • Comments 1 comment
  • opencv
  • dragonboard 410c
Related
Recommended

Dragonboard 410c - OpenCV

Workshopshed
Workshopshed
20 May 2016

I've put the code for the project on Github as it's now starting to get interesting.

 

Testing on something simpler

So that I knew that OpenCV was working correctly I created a simple test script.

 

import numpy as np
import cv2
print cv2.__version__

 

I also decided to do my testing and development on a Windows laptop with a lot more power than the Dragonboard. This will be particularly important when it comes to the number crunching of a new classifier.

I had a few false starts on getting OpenCV working on my laptop. I downloaded and installed the 3.1 version of OpenCV but then used the wrong version of the Python extensions, once I'd picked the right version to go with OpenCV3.1 and Python 2.7 (opencv_python-3.1.0-cp27-cp27m-win32.whl) things started working correctly. I also found that I needed to copy the classifier XML files into my project folder. I modified an example file so that it ran without creating a window.

 

# A simple test file for OpenCV

import numpy as np
import cv2
import datetime


def detect(img_color):
    face_cascade = cv2.CascadeClassifier('haarcascade_frontalface_default.xml')
    eye_cascade = cv2.CascadeClassifier('haarcascade_eye.xml')
    detected = 0
    gray = cv2.cvtColor(img_color, cv2.COLOR_BGR2GRAY)

    # Now we find the faces in the image. If faces are found, it returns the positions of detected faces as Rect(x,y,w,h).
    # Once we get these locations, we can create a ROI for the face and apply eye detection on this ROI (since eyes are always on the face !!! ).
    faces = face_cascade.detectMultiScale(gray)
    for (x, y, w, h) in faces:
        cv2.rectangle(img_color, (x, y), (x + w, y + h), (255, 0, 0), 2)
        roi_gray = gray[y:y + h, x:x + w]
        roi_color = img_color[y:y + h, x:x + w]
        eyes = eye_cascade.detectMultiScale(roi_gray)
        if len(eyes) > 0:
            detected = detected + 1
        for (ex, ey, ew, eh) in eyes:
            cv2.rectangle(roi_color, (ex, ey), (ex + ew, ey + eh), (0, 255, 0), 2)

    print(str(detected) + " people")
    return detected

img = cv2.imread('TestPicture.JPG')

if detect(img) > 0:
    newFileName = "TestOutput" + datetime.datetime.now().isoformat().replace(":","") + ".jpg"
    cv2.imwrite(newFileName, img);

 

The code reads a test file and then passes that to the detect function. The detect function creates two classifiers, one for faces and one for eyes based on the example XML provided with OpenCV. It grayscales the image for faster processing and then detects faces, for each face found it draws a rectangle and the checks for eyes. If it detects eyes on the face then it's a hit and we have found a person.

 

I tested my classifier with some astronauts and it detected three of them although interestingly spotted a face on one of the crumpled sleeves. On my laptop it takes about 1s to load and process the (615x425) pixel file.

image

The same script on the Dragonboard takes 0.6s to run.

 

Getting Webcam images

Capturing from the webcam with OpenCV is very simple. Most of the tutorials assume you want to display video output but these can be simplified to capture a single frame. In this example we capture a single frame from the camera and then save it to the disk. In the finished version that frame would be passed on the classifer.

 

import cv2
import datetime

cap = cv2.VideoCapture(0)
# Capture single frame
ret, frame = cap.read()
cap.release()

if ret:
    newFileName = "CaptureOutput" + datetime.datetime.now().isoformat().replace(":", "") + ".jpg"
    cv2.imwrite(newFileName, frame)
else:
    print "Capture failed"

 

When I tested this with the dragonboard I received the following error:

 

VIDEOIO ERROR: V4L2: Pixel format of incoming image is unsupported by OpenCV
Capture failed

 

There seemed to be some anicdotal evidence to fix this but they did not seem to work for me so I swapped the script out with one that called the command line "streamer" app instead.

 

That also caused me some trouble with the parameters not getting passed to the streamer app correctly, an streamer in turn complaining that the format could not be determined. After some experimentation, the following approach worked and the file could be opened by OpenCV.

 

import cv2
import datetime
from subprocess import call
capture = "CaptureInput" + datetime.datetime.now().isoformat().replace(":", "") + ".jpeg"
cmdline = "streamer -c /dev/video0 -b 32 -f jpeg -o " + capture
call(cmdline, shell=True)
img = cv2.imread(capture)
gray = cv2.cvtColor(img, cv2.COLOR_BGR2GRAY)
newFileName = "CaptureOutput" + datetime.datetime.now().isoformat().replace(":", "") + ".jpg"
cv2.imwrite(newFileName, gray)

Training a classifier

I followed this tutorial to create my classifier xml data, althought I had to drop the featureType parameter as that caused it to crash on my system. The training application is very hungry for memory and used about 2.5GB on my system for image sizes of 50 x 50. It ran one of my CPUs at between 50% and 100%. When I repeated the test with a 100 x 100 image the memory usage shot upto 8GB, although it should be possible to control this with the buffer size settings. However, I reverted to the 50 x 50 and increased the number of cycles of training as that is apparently what gives the quality results rather than the size. The training programme does seem to crash rather than report sensible errors, it also crashed for me when I put in really large image sizes. After 30 minutes I had my first prototype classifier.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

opencv_createsamples.exe -info Dragons.info -num 90 -w 50 -h 50 -vec Dragons.vec

Info file name: Dragons.info
Img file name: (NULL)
Vec file name: Dragons.vec
BG  file name: (NULL)
Num: 90
BG color: 0
BG threshold: 80
Invert: FALSE
Max intensity deviation: 40
Max x angle: 1.1
Max y angle: 1.1
Max z angle: 0.5
Show samples: FALSE
Width: 50
Height: 50
Create training samples from images collection...
Done. Created 90 samples

opencv_traincascade.exe" -data data -vec Dragons.vec -bg Negative.info -numPos 89 -numNeg 765 -numStages 5 -w 50 -h 50

PARAMETERS:
cascadeDirName: data
vecFileName: Dragons.vec
bgFileName: Negative.info
numPos: 89
numNeg: 765
numStages: 5
precalcValBufSize[Mb] : 1024
precalcIdxBufSize[Mb] : 1024
acceptanceRatioBreakValue : -1
stageType: BOOST
featureType: HAAR
sampleWidth: 50
sampleHeight: 50
boostType: GAB
minHitRate: 0.995
maxFalseAlarmRate: 0.5
weightTrimRate: 0.95
maxDepth: 1
maxWeakCount: 100
mode: BASIC

===== TRAINING 0-stage =====
<BEGIN
POS count : consumed   89 : 89
NEG count : acceptanceRatio    765 : 1
Precalculation time: 9.468
+----+---------+---------+
|  N |    HR   |    FA   |
+----+---------+---------+
|   1|        1|        1|
+----+---------+---------+
|   2|        1|        1|
+----+---------+---------+
|   3|        1|        1|
+----+---------+---------+
|   4|        1| 0.330719|
+----+---------+---------+
END>
Training until now has taken 0 days 0 hours 12 minutes 54 seconds.

===== TRAINING 1-stage =====
<BEGIN
POS count : consumed   89 : 89
NEG count : acceptanceRatio    765 : 0.407783
Precalculation time: 9.62
+----+---------+---------+
|  N |    HR   |    FA   |
+----+---------+---------+
|   1|        1|        1|
+----+---------+---------+
|   2|        1|        1|
+----+---------+---------+
|   3|        1| 0.426144|
+----+---------+---------+
END>
Training until now has taken 0 days 0 hours 22 minutes 45 seconds.

===== TRAINING 2-stage =====
<BEGIN
POS count : consumed   89 : 89
NEG count : acceptanceRatio    765 : 0.26127
Precalculation time: 9.143
+----+---------+---------+
|  N |    HR   |    FA   |
+----+---------+---------+
|   1|        1|        1|
+----+---------+---------+
|   2|        1|        1|
+----+---------+---------+
|   3|        1| 0.488889|
+----+---------+---------+
END>
Training until now has taken 0 days 0 hours 32 minutes 18 seconds.

 

Testing

My initial testing provided too many false positives so I found a 1000 more negative images and added them to the training, I also set the maxFalseAlarmRate to a smaller value and set my training going again.

image

This time the training took a lot longer, nearly 15hrs later the classifier was trained and it worked a whole lot better than my first version.

image

I think the next task is to look at hooking some proper hardware to the Dragonboard using the level shifters.

Reference

Getting Started with Videos — OpenCV-Python Tutorials 1 documentation

Coding Robin Train Your Own OpenCV Haar Classifier

OpenCV Tutorial: Training your own detector (video)

Tutorial: OpenCV haartraining (Rapid Object Detection With A Cascade of Boosted Classifiers Based on Haar-like Features)…

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Yes the "self" learning algorithms take a lot of time and options before they get reasonably reliable. I have seen a number of approaches where they use the geometry of eye placement and nose/mouth relationships…
Parents
  • DAB
    DAB over 10 years ago

    Yes the "self" learning algorithms take a lot of time and options before they get reasonably reliable.

     

    I have seen a number of approaches where they use the geometry of eye placement and nose/mouth relationships to quickly narrow the search areas.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 10 years ago

    Yes the "self" learning algorithms take a lot of time and options before they get reasonably reliable.

     

    I have seen a number of approaches where they use the geometry of eye placement and nose/mouth relationships to quickly narrow the search areas.

     

    DAB